usbh1 sometimes not working in imx6dl!

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

usbh1 sometimes not working in imx6dl!

515件の閲覧回数
adarsh1997
Contributor III

Hi,
we are using imx6dl-sabresd custom design board. We are using HUB as a HS device. Most of the time if we connect pendrive it is detected and data transfer also working fine but sometimes after inserting and reinserting Pendrive is not detected.AT the time of pendrive not detected if we reboot the board  pendrive is detected.
If anyone found this issue please help.
We are using linux 5.4. (yocto zeus)

Here are my dtsi entry:

reg_usb_h1_vbus: regulator-usb-h1-vbus {
compatible = "regulator-fixed";
regulator-name = "usb_h1_vbus";
regulator-min-microvolt = <5000000>;
regulator-max-microvolt = <5000000>;
gpio = <&gpio1 0 GPIO_ACTIVE_HIGH>;
enable-active-high;
vin-supply = <&swbst_reg>;

&usbh1 {
vbus-supply = <&reg_usb_h1_vbus>;
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_usbh1>;
status = "okay";
};

pinctrl_usbh1: usbh1grp {
fsl,pins = <
MX6QDL_PAD_GPIO_0__GPIO1_IO00      0x1b0b0
MX6QDL_PAD_EIM_D30__USB_H1_OC    0x1b0b0
>;
};

 

 

Note:We are not getting any error logs(dmesg logs) at the time of pendrive not detecting.

0 件の賞賛
返信
1 返信

501件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Adarsh

 

reason may be weak or noisy signals, so device is not detected sometimes.

One can try to check usb signals quality running tests described in

i.MX 6 Series USB Certification Guide

 

Best regards
igor

0 件の賞賛
返信