usbh1 sometimes not working in imx6dl!

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

usbh1 sometimes not working in imx6dl!

514 Views
adarsh1997
Contributor III

Hi,
we are using imx6dl-sabresd custom design board. We are using HUB as a HS device. Most of the time if we connect pendrive it is detected and data transfer also working fine but sometimes after inserting and reinserting Pendrive is not detected.AT the time of pendrive not detected if we reboot the board  pendrive is detected.
If anyone found this issue please help.
We are using linux 5.4. (yocto zeus)

Here are my dtsi entry:

reg_usb_h1_vbus: regulator-usb-h1-vbus {
compatible = "regulator-fixed";
regulator-name = "usb_h1_vbus";
regulator-min-microvolt = <5000000>;
regulator-max-microvolt = <5000000>;
gpio = <&gpio1 0 GPIO_ACTIVE_HIGH>;
enable-active-high;
vin-supply = <&swbst_reg>;

&usbh1 {
vbus-supply = <&reg_usb_h1_vbus>;
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_usbh1>;
status = "okay";
};

pinctrl_usbh1: usbh1grp {
fsl,pins = <
MX6QDL_PAD_GPIO_0__GPIO1_IO00      0x1b0b0
MX6QDL_PAD_EIM_D30__USB_H1_OC    0x1b0b0
>;
};

 

 

Note:We are not getting any error logs(dmesg logs) at the time of pendrive not detecting.

0 Kudos
Reply
1 Reply

500 Views
igorpadykov
NXP Employee
NXP Employee

Hi Adarsh

 

reason may be weak or noisy signals, so device is not detected sometimes.

One can try to check usb signals quality running tests described in

i.MX 6 Series USB Certification Guide

 

Best regards
igor

0 Kudos
Reply