usb3.0 fail on i.mx8mq

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

usb3.0 fail on i.mx8mq

1,767 次查看
wenfu
Contributor III

Hello,

Hardware:customer board with i.mx8mq SOC

Software: linux 5.4.24 nxp release

We use USB3.0 host port to connect with a USB3.0 device. USB disconnect randomly during the communication preocess. Sometime it happens after several minutes and sometimes several hours.

But our application is very strict on stability.

Here are some kernal log when fail happens:

Oct 13 12:08:28 embest-imx8m kernel: [ 150.530630] random: 7 urandom warning(s) missed due to ratelimiting
Oct 13 17:22:00 embest-imx8m kernel: [18963.130717] usb 1-1: USB disconnect, device number 2
Oct 13 17:22:00 embest-imx8m kernel: [18963.692704] usb 1-1: new high-speed USB device number 3 using xhci-hcd

or:

Sep 29 22:57:45 embest-imx8m kernel: [13530.551441] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 22:57:56 embest-imx8m kernel: [13541.231021] cdc_acm 2-1:1.1: failed to set dtr/rts
Sep 29 22:57:56 embest-imx8m kernel: [13541.235951] xhci-hcd xhci-hcd.4.auto: WARN Set TR Deq Ptr cmd failed due to incorrect slot or ep state.
Sep 29 22:57:56 embest-imx8m kernel: [13541.468610] usb 2-1: reset SuperSpeed Gen 1 USB device number 92 using xhci-hcd
Sep 29 22:57:56 embest-imx8m kernel: [13541.556548] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 22:57:56 embest-imx8m kernel: [13541.820939] usb 2-1: reset SuperSpeed Gen 1 USB device number 92 using xhci-hcd
Sep 29 22:57:56 embest-imx8m kernel: [13541.904009] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 22:57:58 embest-imx8m kernel: [13543.068612] usb 2-1: reset SuperSpeed Gen 1 USB device number 92 using xhci-hcd
Sep 29 22:57:58 embest-imx8m kernel: [13543.156243] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 22:57:58 embest-imx8m kernel: [13543.388343] usb 2-1: reset SuperSpeed Gen 1 USB device number 92 using xhci-hcd
Sep 29 22:57:58 embest-imx8m kernel: [13543.442567] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 22:58:03 embest-imx8m kernel: [13548.689398] cdc_acm 2-1:1.1: failed to set dtr/rts
Sep 29 22:58:03 embest-imx8m kernel: [13548.694339] xhci-hcd xhci-hcd.4.auto: WARN Set TR Deq Ptr cmd failed due to incorrect slot or ep state.
Sep 29 22:58:03 embest-imx8m kernel: [13548.924901] usb 2-1: reset SuperSpeed Gen 1 USB device number 92 using xhci-hcd
Sep 29 22:58:03 embest-imx8m kernel: [13548.950137] usb 2-1: device descriptor read/8, error -71
Sep 29 22:58:04 embest-imx8m kernel: [13549.062527] usb 2-1: reset SuperSpeed Gen 1 USB device number 92 using xhci-hcd
Sep 29 22:58:04 embest-imx8m kernel: [13549.374513] usb 2-1: USB disconnect, device number 92
Sep 29 22:58:04 embest-imx8m kernel: [13549.509292] usb 2-1: new SuperSpeed Gen 1 USB device number 93 using xhci-hcd
Sep 29 22:58:04 embest-imx8m kernel: [13549.654630] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 22:58:07 embest-imx8m kernel: [13552.956659] usb 2-1: reset SuperSpeed Gen 1 USB device number 93 using xhci-hcd
Sep 29 22:58:08 embest-imx8m kernel: [13553.043358] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 22:58:08 embest-imx8m kernel: [13553.308394] usb 2-1: reset SuperSpeed Gen 1 USB device number 93 using xhci-hcd
Sep 29 22:58:08 embest-imx8m kernel: [13553.360923] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 22:58:16 embest-imx8m kernel: [13561.268560] cdc_acm 2-1:1.1: failed to set dtr/rts
Sep 29 22:58:16 embest-imx8m kernel: [13561.273836] xhci-hcd xhci-hcd.4.auto: WARN Set TR Deq Ptr cmd failed due to incorrect slot or ep state.
Sep 29 22:58:16 embest-imx8m kernel: [13561.500238] usb 2-1: Device not responding to setup address.
Sep 29 22:58:16 embest-imx8m kernel: [13561.714574] usb 2-1: Device not responding to setup address.
Sep 29 22:58:16 embest-imx8m kernel: [13561.927023] usb 2-1: device not accepting address 93, error -71
Sep 29 22:58:17 embest-imx8m kernel: [13562.690858] usb 2-1: USB disconnect, device number 93
Sep 29 22:58:18 embest-imx8m kernel: [13563.579125] usb 2-1: new SuperSpeed Gen 1 USB device number 94 using xhci-hcd
Sep 29 22:58:18 embest-imx8m kernel: [13563.736472] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 22:58:25 embest-imx8m kernel: [13570.160303] cdc_acm 2-1:1.1: failed to set dtr/rts
Sep 29 22:58:25 embest-imx8m kernel: [13570.165227] xhci-hcd xhci-hcd.4.auto: WARN Set TR Deq Ptr cmd failed due to incorrect slot or ep state.
Sep 29 22:58:25 embest-imx8m kernel: [13570.396427] usb 2-1: reset SuperSpeed Gen 1 USB device number 94 using xhci-hcd
Sep 29 22:58:25 embest-imx8m kernel: [13570.465915] usb 2-1: can't restore configuration #1 (error=-71)
Sep 29 22:58:25 embest-imx8m kernel: [13570.650514] usb 2-1: USB disconnect, device number 94
Sep 29 22:58:25 embest-imx8m kernel: [13570.811170] usb 2-1: new SuperSpeed Gen 1 USB device number 95 using xhci-hcd
Sep 29 22:58:26 embest-imx8m kernel: [13570.965652] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 22:58:29 embest-imx8m kernel: [13574.004987] cdc_acm 2-1:1.1: failed to set dtr/rts
Sep 29 22:58:29 embest-imx8m kernel: [13574.009914] xhci-hcd xhci-hcd.4.auto: WARN Set TR Deq Ptr cmd failed due to incorrect slot or ep state.
Sep 29 22:58:29 embest-imx8m kernel: [13574.236786] usb 2-1: reset SuperSpeed Gen 1 USB device number 95 using xhci-hcd
Sep 29 22:58:29 embest-imx8m kernel: [13574.299849] usb 2-1: can't restore configuration #1 (error=-71)
Sep 29 22:58:29 embest-imx8m kernel: [13574.481965] usb 2-1: USB disconnect, device number 95
Sep 29 22:58:29 embest-imx8m kernel: [13574.620113] usb 2-1: new SuperSpeed Gen 1 USB device number 96 using xhci-hcd
Sep 29 22:58:29 embest-imx8m kernel: [13574.775187] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 22:58:35 embest-imx8m kernel: [13580.506966] cdc_acm 2-1:1.1: failed to set dtr/rts
Sep 29 22:58:35 embest-imx8m kernel: [13580.511899] xhci-hcd xhci-hcd.4.auto: WARN Set TR Deq Ptr cmd failed due to incorrect slot or ep state.
Sep 29 22:58:35 embest-imx8m kernel: [13580.733378] usb 2-1: reset SuperSpeed Gen 1 USB device number 96 using xhci-hcd
Sep 29 22:58:35 embest-imx8m kernel: [13580.758145] usb 2-1: device descriptor read/8, error -71
Sep 29 22:58:35 embest-imx8m kernel: [13580.870520] usb 2-1: reset SuperSpeed Gen 1 USB device number 96 using xhci-hcd
Sep 29 22:58:36 embest-imx8m kernel: [13581.182535] usb 2-1: USB disconnect, device number 96
Sep 29 22:58:36 embest-imx8m kernel: [13581.316906] usb 2-1: new SuperSpeed Gen 1 USB device number 97 using xhci-hcd
Sep 29 22:58:36 embest-imx8m kernel: [13581.468254] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 22:58:46 embest-imx8m kernel: [13591.740339] usb 2-1: reset SuperSpeed Gen 1 USB device number 97 using xhci-hcd
Sep 29 22:58:46 embest-imx8m kernel: [13591.796646] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 22:58:47 embest-imx8m kernel: [13592.060810] usb 2-1: reset SuperSpeed Gen 1 USB device number 97 using xhci-hcd
Sep 29 22:58:47 embest-imx8m kernel: [13592.148790] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 22:58:58 embest-imx8m kernel: [13603.013938] cdc_acm 2-1:1.1: failed to set dtr/rts
Sep 29 22:58:58 embest-imx8m kernel: [13603.018878] xhci-hcd xhci-hcd.4.auto: WARN Set TR Deq Ptr cmd failed due to incorrect slot or ep state.
Sep 29 22:58:58 embest-imx8m kernel: [13603.228292] usb 2-1: reset SuperSpeed Gen 1 USB device number 97 using xhci-hcd
Sep 29 22:58:58 embest-imx8m kernel: [13603.254216] usb 2-1: device descriptor read/8, error -71
Sep 29 22:58:58 embest-imx8m kernel: [13603.366541] usb 2-1: reset SuperSpeed Gen 1 USB device number 97 using xhci-hcd
Sep 29 22:58:58 embest-imx8m kernel: [13603.678516] usb 2-1: USB disconnect, device number 97
Sep 29 22:58:58 embest-imx8m kernel: [13603.811127] usb 2-1: new SuperSpeed Gen 1 USB device number 98 using xhci-hcd
Sep 29 22:58:58 embest-imx8m kernel: [13603.957570] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 22:59:02 embest-imx8m kernel: [13607.334560] cdc_acm 2-1:1.1: failed to set dtr/rts
Sep 29 22:59:02 embest-imx8m kernel: [13607.339483] xhci-hcd xhci-hcd.4.auto: WARN Set TR Deq Ptr cmd failed due to incorrect slot or ep state.
Sep 29 22:59:02 embest-imx8m kernel: [13607.548333] usb 2-1: reset SuperSpeed Gen 1 USB device number 98 using xhci-hcd
Sep 29 22:59:02 embest-imx8m kernel: [13607.635805] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 22:59:02 embest-imx8m kernel: [13607.868474] usb 2-1: reset SuperSpeed Gen 1 USB device number 98 using xhci-hcd
Sep 29 22:59:02 embest-imx8m kernel: [13607.956393] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 22:59:13 embest-imx8m kernel: [13618.588294] usb 2-1: reset SuperSpeed Gen 1 USB device number 98 using xhci-hcd
Sep 29 22:59:13 embest-imx8m kernel: [13618.614148] usb 2-1: device descriptor read/8, error -71
Sep 29 22:59:13 embest-imx8m kernel: [13618.726550] usb 2-1: reset SuperSpeed Gen 1 USB device number 98 using xhci-hcd
Sep 29 22:59:14 embest-imx8m kernel: [13619.038534] usb 2-1: USB disconnect, device number 98
Sep 29 22:59:14 embest-imx8m kernel: [13619.171172] usb 2-1: new SuperSpeed Gen 1 USB device number 99 using xhci-hcd
Sep 29 22:59:14 embest-imx8m kernel: [13619.319415] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 22:59:22 embest-imx8m kernel: [13626.992873] cdc_acm 2-1:1.1: failed to set dtr/rts
Sep 29 22:59:22 embest-imx8m kernel: [13626.997814] xhci-hcd xhci-hcd.4.auto: WARN Set TR Deq Ptr cmd failed due to incorrect slot or ep state.
Sep 29 22:59:22 embest-imx8m kernel: [13627.228630] usb 2-1: reset SuperSpeed Gen 1 USB device number 99 using xhci-hcd
Sep 29 22:59:22 embest-imx8m kernel: [13627.285827] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 22:59:22 embest-imx8m kernel: [13627.548336] usb 2-1: reset SuperSpeed Gen 1 USB device number 99 using xhci-hcd
Sep 29 22:59:22 embest-imx8m kernel: [13627.634380] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 22:59:33 embest-imx8m kernel: [13638.405673] cdc_acm 2-1:1.1: failed to set dtr/rts
Sep 29 22:59:33 embest-imx8m kernel: [13638.410602] xhci-hcd xhci-hcd.4.auto: WARN Set TR Deq Ptr cmd failed due to incorrect slot or ep state.
Sep 29 22:59:33 embest-imx8m kernel: [13638.620536] usb 2-1: reset SuperSpeed Gen 1 USB device number 99 using xhci-hcd
Sep 29 22:59:33 embest-imx8m kernel: [13638.707571] alloc_contig_range: [44148, 4414d) PFNs busy
Sep 29 22:59:33 embest-imx8m kernel: [13638.714977] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 22:59:34 embest-imx8m kernel: [13638.972347] usb 2-1: reset SuperSpeed Gen 1 USB device number 99 using xhci-hcd
Sep 29 22:59:34 embest-imx8m kernel: [13639.054897] alloc_contig_range: [44148, 4414d) PFNs busy
Sep 29 22:59:34 embest-imx8m kernel: [13639.061523] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 22:59:36 embest-imx8m kernel: [13641.186182] cdc_acm 2-1:1.1: failed to set dtr/rts
Sep 29 22:59:36 embest-imx8m kernel: [13641.191110] xhci-hcd xhci-hcd.4.auto: WARN Set TR Deq Ptr cmd failed due to incorrect slot or ep state.
Sep 29 22:59:36 embest-imx8m kernel: [13641.404729] usb 2-1: reset SuperSpeed Gen 1 USB device number 99 using xhci-hcd
Sep 29 22:59:36 embest-imx8m kernel: [13641.478334] usb 2-1: can't restore configuration #1 (error=-71)
Sep 29 22:59:36 embest-imx8m kernel: [13641.661966] usb 2-1: USB disconnect, device number 99
Sep 29 22:59:36 embest-imx8m kernel: [13641.819166] usb 2-1: new SuperSpeed Gen 1 USB device number 100 using xhci-hcd
Sep 29 22:59:37 embest-imx8m kernel: [13641.974999] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 22:59:40 embest-imx8m kernel: [13645.550392] cdc_acm 2-1:1.1: failed to set dtr/rts
Sep 29 22:59:40 embest-imx8m kernel: [13645.555649] xhci-hcd xhci-hcd.4.auto: WARN Set TR Deq Ptr cmd failed due to incorrect slot or ep state.
Sep 29 22:59:40 embest-imx8m kernel: [13645.788630] usb 2-1: reset SuperSpeed Gen 1 USB device number 100 using xhci-hcd
Sep 29 22:59:40 embest-imx8m kernel: [13645.843703] alloc_contig_range: [44148, 4414d) PFNs busy
Sep 29 22:59:40 embest-imx8m kernel: [13645.850324] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 22:59:41 embest-imx8m kernel: [13646.076490] usb 2-1: reset SuperSpeed Gen 1 USB device number 100 using xhci-hcd
Sep 29 22:59:41 embest-imx8m kernel: [13646.161782] alloc_contig_range: [44148, 4414d) PFNs busy
Sep 29 22:59:41 embest-imx8m kernel: [13646.168379] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 22:59:48 embest-imx8m kernel: [13653.673174] cdc_acm 2-1:1.1: failed to set dtr/rts
Sep 29 22:59:48 embest-imx8m kernel: [13653.678110] xhci-hcd xhci-hcd.4.auto: WARN Set TR Deq Ptr cmd failed due to incorrect slot or ep state.
Sep 29 22:59:48 embest-imx8m kernel: [13653.884568] usb 2-1: reset SuperSpeed Gen 1 USB device number 100 using xhci-hcd
Sep 29 22:59:49 embest-imx8m kernel: [13653.971871] alloc_contig_range: [44148, 4414d) PFNs busy
Sep 29 22:59:49 embest-imx8m kernel: [13653.979285] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 22:59:49 embest-imx8m kernel: [13654.235898] usb 2-1: reset SuperSpeed Gen 1 USB device number 100 using xhci-hcd
Sep 29 22:59:49 embest-imx8m kernel: [13654.324395] alloc_contig_range: [44148, 4414d) PFNs busy
Sep 29 22:59:49 embest-imx8m kernel: [13654.331813] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 22:59:51 embest-imx8m kernel: [13656.060931] cdc_acm 2-1:1.1: failed to set dtr/rts
Sep 29 22:59:51 embest-imx8m kernel: [13656.065846] xhci-hcd xhci-hcd.4.auto: WARN Set TR Deq Ptr cmd failed due to incorrect slot or ep state.
Sep 29 22:59:51 embest-imx8m kernel: [13656.284337] usb 2-1: reset SuperSpeed Gen 1 USB device number 100 using xhci-hcd
Sep 29 22:59:51 embest-imx8m kernel: [13656.337913] alloc_contig_range: [44148, 4414d) PFNs busy
Sep 29 22:59:51 embest-imx8m kernel: [13656.344495] alloc_contig_range: [44150, 44155) PFNs busy
Sep 29 22:59:51 embest-imx8m kernel: [13656.352767] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 22:59:51 embest-imx8m kernel: [13656.604397] usb 2-1: reset SuperSpeed Gen 1 USB device number 100 using xhci-hcd
Sep 29 22:59:51 embest-imx8m kernel: [13656.654889] alloc_contig_range: [44148, 4414d) PFNs busy
Sep 29 22:59:51 embest-imx8m kernel: [13656.660988] alloc_contig_range: [44150, 44155) PFNs busy
Sep 29 22:59:51 embest-imx8m kernel: [13656.667617] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 22:59:58 embest-imx8m kernel: [13663.562904] cdc_acm 2-1:1.1: failed to set dtr/rts
Sep 29 22:59:58 embest-imx8m kernel: [13663.567825] xhci-hcd xhci-hcd.4.auto: WARN Set TR Deq Ptr cmd failed due to incorrect slot or ep state.
Sep 29 22:59:58 embest-imx8m kernel: [13663.804701] usb 2-1: reset SuperSpeed Gen 1 USB device number 100 using xhci-hcd
Sep 29 22:59:58 embest-imx8m kernel: [13663.848141] usb 2-1: device firmware changed
Sep 29 22:59:59 embest-imx8m kernel: [13664.030526] usb 2-1: USB disconnect, device number 100
Sep 29 22:59:59 embest-imx8m kernel: [13664.168264] usb 2-1: new SuperSpeed Gen 1 USB device number 101 using xhci-hcd
Sep 29 22:59:59 embest-imx8m kernel: [13664.312279] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:00:01 embest-imx8m kernel: [13665.990755] cdc_acm 2-1:1.1: failed to set dtr/rts
Sep 29 23:00:01 embest-imx8m kernel: [13665.995689] xhci-hcd xhci-hcd.4.auto: WARN Set TR Deq Ptr cmd failed due to incorrect slot or ep state.
Sep 29 23:00:01 embest-imx8m kernel: [13666.236197] usb 2-1: reset SuperSpeed Gen 1 USB device number 101 using xhci-hcd
Sep 29 23:00:01 embest-imx8m kernel: [13666.299826] usb 2-1: can't restore configuration #1 (error=-71)
Sep 29 23:00:01 embest-imx8m kernel: [13666.481966] usb 2-1: USB disconnect, device number 101
Sep 29 23:00:01 embest-imx8m kernel: [13666.619187] usb 2-1: new SuperSpeed Gen 1 USB device number 102 using xhci-hcd
Sep 29 23:00:01 embest-imx8m kernel: [13666.776183] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:00:03 embest-imx8m kernel: [13668.301069] cdc_acm 2-1:1.1: failed to set dtr/rts
Sep 29 23:00:03 embest-imx8m kernel: [13668.306197] cdc_acm 2-1:1.1: failed to set dtr/rts
Sep 29 23:00:03 embest-imx8m kernel: [13668.518805] usb 2-1: Device not responding to setup address.
Sep 29 23:00:03 embest-imx8m kernel: [13668.730014] usb 2-1: Device not responding to setup address.
Sep 29 23:00:03 embest-imx8m kernel: [13668.942538] usb 2-1: device not accepting address 102, error -71
Sep 29 23:00:04 embest-imx8m kernel: [13669.706843] usb 2-1: USB disconnect, device number 102
Sep 29 23:00:05 embest-imx8m kernel: [13670.597197] usb 2-1: new SuperSpeed Gen 1 USB device number 103 using xhci-hcd
Sep 29 23:00:05 embest-imx8m kernel: [13670.742417] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:00:17 embest-imx8m kernel: [13682.076838] cdc_acm 2-1:1.1: failed to set dtr/rts
Sep 29 23:00:17 embest-imx8m kernel: [13682.081780] xhci-hcd xhci-hcd.4.auto: WARN Set TR Deq Ptr cmd failed due to incorrect slot or ep state.
Sep 29 23:00:17 embest-imx8m kernel: [13682.300235] usb 2-1: Device not responding to setup address.
Sep 29 23:00:17 embest-imx8m kernel: [13682.514591] usb 2-1: Device not responding to setup address.
Sep 29 23:00:17 embest-imx8m kernel: [13682.726510] usb 2-1: device not accepting address 103, error -71
Sep 29 23:00:18 embest-imx8m kernel: [13683.490845] usb 2-1: USB disconnect, device number 103
Sep 29 23:00:19 embest-imx8m kernel: [13684.379515] usb 2-1: new SuperSpeed Gen 1 USB device number 104 using xhci-hcd
Sep 29 23:00:19 embest-imx8m kernel: [13684.535241] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:00:21 embest-imx8m kernel: [13686.465612] cdc_acm 2-1:1.1: failed to set dtr/rts
Sep 29 23:00:21 embest-imx8m kernel: [13686.470570] xhci-hcd xhci-hcd.4.auto: WARN Set TR Deq Ptr cmd failed due to incorrect slot or ep state.
Sep 29 23:00:21 embest-imx8m kernel: [13686.684812] usb 2-1: reset SuperSpeed Gen 1 USB device number 104 using xhci-hcd
Sep 29 23:00:21 embest-imx8m kernel: [13686.727679] usb 2-1: can't restore configuration #1 (error=-71)
Sep 29 23:00:21 embest-imx8m kernel: [13686.910511] usb 2-1: USB disconnect, device number 104
Sep 29 23:00:22 embest-imx8m kernel: [13687.068070] usb 2-1: new SuperSpeed Gen 1 USB device number 105 using xhci-hcd
Sep 29 23:00:22 embest-imx8m kernel: [13687.223732] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:00:33 embest-imx8m kernel: [13698.921524] cdc_acm 2-1:1.1: failed to set dtr/rts
Sep 29 23:00:33 embest-imx8m kernel: [13698.926445] xhci-hcd xhci-hcd.4.auto: WARN Set TR Deq Ptr cmd failed due to incorrect slot or ep state.
Sep 29 23:00:34 embest-imx8m kernel: [13699.132936] usb 2-1: reset SuperSpeed Gen 1 USB device number 105 using xhci-hcd
Sep 29 23:00:34 embest-imx8m kernel: [13699.187356] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:00:34 embest-imx8m kernel: [13699.452511] usb 2-1: reset SuperSpeed Gen 1 USB device number 105 using xhci-hcd
Sep 29 23:00:34 embest-imx8m kernel: [13699.514709] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:00:35 embest-imx8m kernel: [13699.965141] usb 2-1: reset SuperSpeed Gen 1 USB device number 105 using xhci-hcd
Sep 29 23:00:35 embest-imx8m kernel: [13700.051586] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:00:35 embest-imx8m kernel: [13700.284417] usb 2-1: reset SuperSpeed Gen 1 USB device number 105 using xhci-hcd
Sep 29 23:00:35 embest-imx8m kernel: [13700.372352] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:00:42 embest-imx8m kernel: [13707.311263] cdc_acm 2-1:1.1: failed to set dtr/rts
Sep 29 23:00:42 embest-imx8m kernel: [13707.316200] xhci-hcd xhci-hcd.4.auto: WARN Set TR Deq Ptr cmd failed due to incorrect slot or ep state.
Sep 29 23:00:42 embest-imx8m kernel: [13707.548293] usb 2-1: reset SuperSpeed Gen 1 USB device number 105 using xhci-hcd
Sep 29 23:00:42 embest-imx8m kernel: [13707.636559] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:00:42 embest-imx8m kernel: [13707.868331] usb 2-1: reset SuperSpeed Gen 1 USB device number 105 using xhci-hcd
Sep 29 23:00:42 embest-imx8m kernel: [13707.953127] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:00:44 embest-imx8m kernel: [13709.956556] cdc_acm 2-1:1.1: failed to set dtr/rts
Sep 29 23:00:44 embest-imx8m kernel: [13709.961489] xhci-hcd xhci-hcd.4.auto: WARN Set TR Deq Ptr cmd failed due to incorrect slot or ep state.
Sep 29 23:00:45 embest-imx8m kernel: [13710.173125] usb 2-1: reset SuperSpeed Gen 1 USB device number 105 using xhci-hcd
Sep 29 23:00:45 embest-imx8m kernel: [13710.247683] usb 2-1: can't restore configuration #1 (error=-71)
Sep 29 23:00:45 embest-imx8m kernel: [13710.430532] usb 2-1: USB disconnect, device number 105
Sep 29 23:00:45 embest-imx8m kernel: [13710.587129] usb 2-1: new SuperSpeed Gen 1 USB device number 106 using xhci-hcd
Sep 29 23:00:45 embest-imx8m kernel: [13710.745700] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:00:52 embest-imx8m kernel: [13717.690057] cdc_acm 2-1:1.1: failed to set dtr/rts
Sep 29 23:00:52 embest-imx8m kernel: [13717.694988] xhci-hcd xhci-hcd.4.auto: WARN Set TR Deq Ptr cmd failed due to incorrect slot or ep state.
Sep 29 23:00:52 embest-imx8m kernel: [13717.918459] usb 2-1: Device not responding to setup address.
Sep 29 23:00:53 embest-imx8m kernel: [13718.130574] usb 2-1: Device not responding to setup address.
Sep 29 23:00:53 embest-imx8m kernel: [13718.343010] usb 2-1: device not accepting address 106, error -71
Sep 29 23:00:54 embest-imx8m kernel: [13719.106868] usb 2-1: USB disconnect, device number 106
Sep 29 23:00:55 embest-imx8m kernel: [13719.997752] usb 2-1: new SuperSpeed Gen 1 USB device number 107 using xhci-hcd
Sep 29 23:00:55 embest-imx8m kernel: [13720.152554] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:00:58 embest-imx8m kernel: [13723.241044] cdc_acm 2-1:1.1: failed to set dtr/rts
Sep 29 23:00:58 embest-imx8m kernel: [13723.246039] xhci-hcd xhci-hcd.4.auto: WARN Set TR Deq Ptr cmd failed due to incorrect slot or ep state.
Sep 29 23:00:58 embest-imx8m kernel: [13723.451767] usb 2-1: reset SuperSpeed Gen 1 USB device number 107 using xhci-hcd
Sep 29 23:00:58 embest-imx8m kernel: [13723.508250] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:00:58 embest-imx8m kernel: [13723.772525] usb 2-1: reset SuperSpeed Gen 1 USB device number 107 using xhci-hcd
Sep 29 23:00:58 embest-imx8m kernel: [13723.822257] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:01:11 embest-imx8m kernel: [13736.667859] cdc_acm 2-1:1.1: failed to set dtr/rts
Sep 29 23:01:11 embest-imx8m kernel: [13736.672803] xhci-hcd xhci-hcd.4.auto: WARN Set TR Deq Ptr cmd failed due to incorrect slot or ep state.
Sep 29 23:01:11 embest-imx8m kernel: [13736.892302] usb 2-1: reset SuperSpeed Gen 1 USB device number 107 using xhci-hcd
Sep 29 23:01:12 embest-imx8m kernel: [13736.978716] alloc_contig_range: [44148, 4414d) PFNs busy
Sep 29 23:01:12 embest-imx8m kernel: [13736.984809] alloc_contig_range: [44150, 44155) PFNs busy
Sep 29 23:01:12 embest-imx8m kernel: [13736.991437] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:01:12 embest-imx8m kernel: [13737.212787] usb 2-1: reset SuperSpeed Gen 1 USB device number 107 using xhci-hcd
Sep 29 23:01:12 embest-imx8m kernel: [13737.297680] alloc_contig_range: [44148, 4414d) PFNs busy
Sep 29 23:01:12 embest-imx8m kernel: [13737.304263] alloc_contig_range: [44150, 44155) PFNs busy
Sep 29 23:01:12 embest-imx8m kernel: [13737.311677] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:01:17 embest-imx8m kernel: [13742.474466] cdc_acm 2-1:1.1: failed to set dtr/rts
Sep 29 23:01:17 embest-imx8m kernel: [13742.479391] xhci-hcd xhci-hcd.4.auto: WARN Set TR Deq Ptr cmd failed due to incorrect slot or ep state.
Sep 29 23:01:17 embest-imx8m kernel: [13742.716369] usb 2-1: reset SuperSpeed Gen 1 USB device number 107 using xhci-hcd
Sep 29 23:01:17 embest-imx8m kernel: [13742.788635] usb 2-1: can't restore configuration #1 (error=-71)
Sep 29 23:01:18 embest-imx8m kernel: [13742.974537] usb 2-1: USB disconnect, device number 107
Sep 29 23:01:18 embest-imx8m kernel: [13743.131381] usb 2-1: new SuperSpeed Gen 1 USB device number 108 using xhci-hcd
Sep 29 23:01:18 embest-imx8m kernel: [13743.289555] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:01:22 embest-imx8m kernel: [13747.005022] usb 2-1: reset SuperSpeed Gen 1 USB device number 108 using xhci-hcd
Sep 29 23:01:22 embest-imx8m kernel: [13747.058774] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:01:22 embest-imx8m kernel: [13747.292555] usb 2-1: reset SuperSpeed Gen 1 USB device number 108 using xhci-hcd
Sep 29 23:01:22 embest-imx8m kernel: [13747.375352] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:01:25 embest-imx8m kernel: [13750.955419] cdc_acm 2-1:1.1: failed to set dtr/rts
Sep 29 23:01:25 embest-imx8m kernel: [13750.960366] xhci-hcd xhci-hcd.4.auto: WARN Set TR Deq Ptr cmd failed due to incorrect slot or ep state.
Sep 29 23:01:26 embest-imx8m kernel: [13751.196810] usb 2-1: reset SuperSpeed Gen 1 USB device number 108 using xhci-hcd
Sep 29 23:01:26 embest-imx8m kernel: [13751.252499] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:01:26 embest-imx8m kernel: [13751.484358] usb 2-1: reset SuperSpeed Gen 1 USB device number 108 using xhci-hcd
Sep 29 23:01:26 embest-imx8m kernel: [13751.571649] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:01:35 embest-imx8m kernel: [13760.893269] cdc_acm 2-1:1.1: failed to set dtr/rts
Sep 29 23:01:35 embest-imx8m kernel: [13760.898241] xhci-hcd xhci-hcd.4.auto: WARN Set TR Deq Ptr cmd failed due to incorrect slot or ep state.
Sep 29 23:01:36 embest-imx8m kernel: [13761.116621] usb 2-1: reset SuperSpeed Gen 1 USB device number 108 using xhci-hcd
Sep 29 23:01:36 embest-imx8m kernel: [13761.150410] usb 2-1: device descriptor read/8, error -71
Sep 29 23:01:36 embest-imx8m kernel: [13761.262517] usb 2-1: reset SuperSpeed Gen 1 USB device number 108 using xhci-hcd
Sep 29 23:01:36 embest-imx8m kernel: [13761.574533] usb 2-1: USB disconnect, device number 108
Sep 29 23:01:36 embest-imx8m kernel: [13761.713159] usb 2-1: new SuperSpeed Gen 1 USB device number 109 using xhci-hcd
Sep 29 23:01:36 embest-imx8m kernel: [13761.844961] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:01:43 embest-imx8m kernel: [13768.606208] cdc_acm 2-1:1.1: failed to set dtr/rts
Sep 29 23:01:43 embest-imx8m kernel: [13768.611135] xhci-hcd xhci-hcd.4.auto: WARN Set TR Deq Ptr cmd failed due to incorrect slot or ep state.
Sep 29 23:01:43 embest-imx8m kernel: [13768.828421] usb 2-1: reset SuperSpeed Gen 1 USB device number 109 using xhci-hcd
Sep 29 23:01:43 embest-imx8m kernel: [13768.880760] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:01:44 embest-imx8m kernel: [13769.148345] usb 2-1: reset SuperSpeed Gen 1 USB device number 109 using xhci-hcd
Sep 29 23:01:44 embest-imx8m kernel: [13769.235163] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:01:48 embest-imx8m kernel: [13773.415303] cdc_acm 2-1:1.1: failed to set dtr/rts
Sep 29 23:01:48 embest-imx8m kernel: [13773.420242] xhci-hcd xhci-hcd.4.auto: WARN Set TR Deq Ptr cmd failed due to incorrect slot or ep state.
Sep 29 23:01:48 embest-imx8m kernel: [13773.629099] usb 2-1: reset SuperSpeed Gen 1 USB device number 109 using xhci-hcd
Sep 29 23:01:48 embest-imx8m kernel: [13773.715737] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:01:48 embest-imx8m kernel: [13773.948500] usb 2-1: reset SuperSpeed Gen 1 USB device number 109 using xhci-hcd
Sep 29 23:01:49 embest-imx8m kernel: [13774.035688] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:01:51 embest-imx8m kernel: [13776.885247] cdc_acm 2-1:1.1: failed to set dtr/rts
Sep 29 23:01:51 embest-imx8m kernel: [13776.890191] xhci-hcd xhci-hcd.4.auto: WARN Set TR Deq Ptr cmd failed due to incorrect slot or ep state.
Sep 29 23:01:52 embest-imx8m kernel: [13777.116346] usb 2-1: reset SuperSpeed Gen 1 USB device number 109 using xhci-hcd
Sep 29 23:01:52 embest-imx8m kernel: [13777.189368] usb 2-1: can't restore configuration #1 (error=-71)
Sep 29 23:01:52 embest-imx8m kernel: [13777.374519] usb 2-1: USB disconnect, device number 109
Sep 29 23:01:52 embest-imx8m kernel: [13777.531988] usb 2-1: new SuperSpeed Gen 1 USB device number 110 using xhci-hcd
Sep 29 23:01:52 embest-imx8m kernel: [13777.688331] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:01:54 embest-imx8m kernel: [13779.132708] usb 2-1: reset SuperSpeed Gen 1 USB device number 110 using xhci-hcd
Sep 29 23:01:54 embest-imx8m kernel: [13779.199384] usb 2-1: can't restore configuration #1 (error=-71)
Sep 29 23:01:54 embest-imx8m kernel: [13779.382514] usb 2-1: USB disconnect, device number 110
Sep 29 23:01:54 embest-imx8m kernel: [13779.547136] usb 2-1: new SuperSpeed Gen 1 USB device number 111 using xhci-hcd
Sep 29 23:01:54 embest-imx8m kernel: [13779.704602] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:02:01 embest-imx8m kernel: [13786.715883] cdc_acm 2-1:1.1: failed to set dtr/rts
Sep 29 23:02:01 embest-imx8m kernel: [13786.720808] xhci-hcd xhci-hcd.4.auto: WARN Set TR Deq Ptr cmd failed due to incorrect slot or ep state.
Sep 29 23:02:01 embest-imx8m kernel: [13786.940615] usb 2-1: reset SuperSpeed Gen 1 USB device number 111 using xhci-hcd
Sep 29 23:02:02 embest-imx8m kernel: [13786.997922] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:02:02 embest-imx8m kernel: [13787.260854] usb 2-1: reset SuperSpeed Gen 1 USB device number 111 using xhci-hcd
Sep 29 23:02:02 embest-imx8m kernel: [13787.343569] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:02:04 embest-imx8m kernel: [13789.550530] cdc_acm 2-1:1.1: failed to set dtr/rts
Sep 29 23:02:04 embest-imx8m kernel: [13789.555464] xhci-hcd xhci-hcd.4.auto: WARN Set TR Deq Ptr cmd failed due to incorrect slot or ep state.
Sep 29 23:02:04 embest-imx8m kernel: [13789.788897] usb 2-1: reset SuperSpeed Gen 1 USB device number 111 using xhci-hcd
Sep 29 23:02:04 embest-imx8m kernel: [13789.845114] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:02:05 embest-imx8m kernel: [13790.076337] usb 2-1: reset SuperSpeed Gen 1 USB device number 111 using xhci-hcd
Sep 29 23:02:05 embest-imx8m kernel: [13790.163834] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:02:12 embest-imx8m kernel: [13797.851105] cdc_acm 2-1:1.1: failed to set dtr/rts
Sep 29 23:02:12 embest-imx8m kernel: [13797.856045] xhci-hcd xhci-hcd.4.auto: WARN Set TR Deq Ptr cmd failed due to incorrect slot or ep state.
Sep 29 23:02:13 embest-imx8m kernel: [13798.076831] usb 2-1: reset SuperSpeed Gen 1 USB device number 111 using xhci-hcd
Sep 29 23:02:13 embest-imx8m kernel: [13798.130251] alloc_contig_range: [44148, 4414d) PFNs busy
Sep 29 23:02:13 embest-imx8m kernel: [13798.136829] alloc_contig_range: [44150, 44155) PFNs busy
Sep 29 23:02:13 embest-imx8m kernel: [13798.144258] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:02:13 embest-imx8m kernel: [13798.364509] usb 2-1: reset SuperSpeed Gen 1 USB device number 111 using xhci-hcd
Sep 29 23:02:13 embest-imx8m kernel: [13798.451861] alloc_contig_range: [44148, 4414d) PFNs busy
Sep 29 23:02:13 embest-imx8m kernel: [13798.458017] alloc_contig_range: [44150, 44155) PFNs busy
Sep 29 23:02:13 embest-imx8m kernel: [13798.464691] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:02:22 embest-imx8m kernel: [13807.356292] usb 2-1: reset SuperSpeed Gen 1 USB device number 111 using xhci-hcd
Sep 29 23:02:22 embest-imx8m kernel: [13807.444550] alloc_contig_range: [44148, 4414d) PFNs busy
Sep 29 23:02:22 embest-imx8m kernel: [13807.451179] alloc_contig_range: [44150, 44155) PFNs busy
Sep 29 23:02:22 embest-imx8m kernel: [13807.458614] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:02:22 embest-imx8m kernel: [13807.676311] usb 2-1: reset SuperSpeed Gen 1 USB device number 111 using xhci-hcd
Sep 29 23:02:22 embest-imx8m kernel: [13807.729656] alloc_contig_range: [44148, 4414d) PFNs busy
Sep 29 23:02:22 embest-imx8m kernel: [13807.736236] alloc_contig_range: [44150, 44155) PFNs busy
Sep 29 23:02:22 embest-imx8m kernel: [13807.743684] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:02:28 embest-imx8m kernel: [13813.542465] cdc_acm 2-1:1.1: failed to set dtr/rts
Sep 29 23:02:28 embest-imx8m kernel: [13813.547387] xhci-hcd xhci-hcd.4.auto: WARN Set TR Deq Ptr cmd failed due to incorrect slot or ep state.
Sep 29 23:02:28 embest-imx8m kernel: [13813.756366] usb 2-1: reset SuperSpeed Gen 1 USB device number 111 using xhci-hcd
Sep 29 23:02:28 embest-imx8m kernel: [13813.843652] alloc_contig_range: [44148, 4414d) PFNs busy
Sep 29 23:02:28 embest-imx8m kernel: [13813.850318] alloc_contig_range: [44150, 44155) PFNs busy
Sep 29 23:02:28 embest-imx8m kernel: [13813.859102] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:02:29 embest-imx8m kernel: [13814.108324] usb 2-1: reset SuperSpeed Gen 1 USB device number 111 using xhci-hcd
Sep 29 23:02:29 embest-imx8m kernel: [13814.164208] alloc_contig_range: [44148, 4414d) PFNs busy
Sep 29 23:02:29 embest-imx8m kernel: [13814.170331] alloc_contig_range: [44150, 44155) PFNs busy
Sep 29 23:02:29 embest-imx8m kernel: [13814.177668] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:02:43 embest-imx8m kernel: [13828.719783] cdc_acm 2-1:1.1: failed to set dtr/rts
Sep 29 23:02:43 embest-imx8m kernel: [13828.724731] xhci-hcd xhci-hcd.4.auto: WARN Set TR Deq Ptr cmd failed due to incorrect slot or ep state.
Sep 29 23:02:43 embest-imx8m kernel: [13828.956912] usb 2-1: reset SuperSpeed Gen 1 USB device number 111 using xhci-hcd
Sep 29 23:02:44 embest-imx8m kernel: [13829.019874] usb 2-1: can't restore configuration #1 (error=-71)
Sep 29 23:02:44 embest-imx8m kernel: [13829.206522] usb 2-1: USB disconnect, device number 111
Sep 29 23:02:44 embest-imx8m kernel: [13829.373161] usb 2-1: new SuperSpeed Gen 1 USB device number 112 using xhci-hcd
Sep 29 23:02:44 embest-imx8m kernel: [13829.527623] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:02:49 embest-imx8m kernel: [13834.511359] cdc_acm 2-1:1.1: failed to set dtr/rts
Sep 29 23:02:49 embest-imx8m kernel: [13834.516360] xhci-hcd xhci-hcd.4.auto: WARN Set TR Deq Ptr cmd failed due to incorrect slot or ep state.
Sep 29 23:02:49 embest-imx8m kernel: [13834.748643] usb 2-1: reset SuperSpeed Gen 1 USB device number 112 using xhci-hcd
Sep 29 23:02:49 embest-imx8m kernel: [13834.811817] usb 2-1: can't restore configuration #1 (error=-71)
Sep 29 23:02:50 embest-imx8m kernel: [13834.994514] usb 2-1: USB disconnect, device number 112
Sep 29 23:02:50 embest-imx8m kernel: [13835.131180] usb 2-1: new SuperSpeed Gen 1 USB device number 113 using xhci-hcd
Sep 29 23:02:50 embest-imx8m kernel: [13835.284741] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:02:51 embest-imx8m kernel: [13836.860530] usb 2-1: reset SuperSpeed Gen 1 USB device number 113 using xhci-hcd
Sep 29 23:02:51 embest-imx8m kernel: [13836.947682] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:02:52 embest-imx8m kernel: [13837.180471] usb 2-1: reset SuperSpeed Gen 1 USB device number 113 using xhci-hcd
Sep 29 23:02:52 embest-imx8m kernel: [13837.267211] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:02:58 embest-imx8m kernel: [13843.792927] cdc_acm 2-1:1.1: failed to set dtr/rts
Sep 29 23:02:58 embest-imx8m kernel: [13843.797865] xhci-hcd xhci-hcd.4.auto: WARN Set TR Deq Ptr cmd failed due to incorrect slot or ep state.
Sep 29 23:02:59 embest-imx8m kernel: [13844.028333] usb 2-1: reset SuperSpeed Gen 1 USB device number 113 using xhci-hcd
Sep 29 23:02:59 embest-imx8m kernel: [13844.091856] usb 2-1: can't restore configuration #1 (error=-71)
Sep 29 23:02:59 embest-imx8m kernel: [13844.274522] usb 2-1: USB disconnect, device number 113
Sep 29 23:02:59 embest-imx8m kernel: [13844.411174] usb 2-1: new SuperSpeed Gen 1 USB device number 114 using xhci-hcd
Sep 29 23:02:59 embest-imx8m kernel: [13844.567745] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:03:02 embest-imx8m kernel: [13847.239782] cdc_acm 2-1:1.1: failed to set dtr/rts
Sep 29 23:03:02 embest-imx8m kernel: [13847.244730] xhci-hcd xhci-hcd.4.auto: WARN Set TR Deq Ptr cmd failed due to incorrect slot or ep state.
Sep 29 23:03:02 embest-imx8m kernel: [13847.485156] usb 2-1: reset SuperSpeed Gen 1 USB device number 114 using xhci-hcd
Sep 29 23:03:02 embest-imx8m kernel: [13847.547791] usb 2-1: can't restore configuration #1 (error=-19)
Sep 29 23:03:02 embest-imx8m kernel: [13847.730544] usb 2-1: USB disconnect, device number 114
Sep 29 23:03:02 embest-imx8m kernel: [13847.867170] usb 2-1: new SuperSpeed Gen 1 USB device number 115 using xhci-hcd
Sep 29 23:03:03 embest-imx8m kernel: [13848.023594] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:03:08 embest-imx8m kernel: [13853.436409] usb 2-1: reset SuperSpeed Gen 1 USB device number 115 using xhci-hcd
Sep 29 23:03:08 embest-imx8m kernel: [13853.490816] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:03:08 embest-imx8m kernel: [13853.692621] usb 2-1: reset SuperSpeed Gen 1 USB device number 115 using xhci-hcd
Sep 29 23:03:08 embest-imx8m kernel: [13853.780252] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:03:09 embest-imx8m kernel: [13854.525002] usb 2-1: reset SuperSpeed Gen 1 USB device number 115 using xhci-hcd
Sep 29 23:03:09 embest-imx8m kernel: [13854.612999] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:03:09 embest-imx8m kernel: [13854.844745] usb 2-1: reset SuperSpeed Gen 1 USB device number 115 using xhci-hcd
Sep 29 23:03:09 embest-imx8m kernel: [13854.930432] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:03:17 embest-imx8m kernel: [13862.163632] cdc_acm 2-1:1.1: failed to set dtr/rts
Sep 29 23:03:17 embest-imx8m kernel: [13862.168547] xhci-hcd xhci-hcd.4.auto: WARN Set TR Deq Ptr cmd failed due to incorrect slot or ep state.
Sep 29 23:03:17 embest-imx8m kernel: [13862.396846] usb 2-1: reset SuperSpeed Gen 1 USB device number 115 using xhci-hcd
Sep 29 23:03:17 embest-imx8m kernel: [13862.451878] alloc_contig_range: [44148, 4414d) PFNs busy
Sep 29 23:03:17 embest-imx8m kernel: [13862.458499] alloc_contig_range: [44150, 44155) PFNs busy
Sep 29 23:03:17 embest-imx8m kernel: [13862.465927] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:03:17 embest-imx8m kernel: [13862.780403] usb 2-1: reset SuperSpeed Gen 1 USB device number 115 using xhci-hcd
Sep 29 23:03:17 embest-imx8m kernel: [13862.866476] alloc_contig_range: [44148, 4414d) PFNs busy
Sep 29 23:03:17 embest-imx8m kernel: [13862.873058] alloc_contig_range: [44150, 44155) PFNs busy
Sep 29 23:03:17 embest-imx8m kernel: [13862.880510] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:03:27 embest-imx8m kernel: [13872.563378] cdc_acm 2-1:1.1: failed to set dtr/rts
Sep 29 23:03:27 embest-imx8m kernel: [13872.568295] xhci-hcd xhci-hcd.4.auto: WARN Set TR Deq Ptr cmd failed due to incorrect slot or ep state.
Sep 29 23:03:27 embest-imx8m kernel: [13872.796524] usb 2-1: reset SuperSpeed Gen 1 USB device number 115 using xhci-hcd
Sep 29 23:03:27 embest-imx8m kernel: [13872.861512] usb 2-1: can't restore configuration #1 (error=-71)
Sep 29 23:03:28 embest-imx8m kernel: [13873.046529] usb 2-1: USB disconnect, device number 115
Sep 29 23:03:28 embest-imx8m kernel: [13873.211181] usb 2-1: new SuperSpeed Gen 1 USB device number 116 using xhci-hcd
Sep 29 23:03:28 embest-imx8m kernel: [13873.336046] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:03:37 embest-imx8m kernel: [13881.991235] cdc_acm 2-1:1.1: failed to set dtr/rts
Sep 29 23:03:37 embest-imx8m kernel: [13881.996183] xhci-hcd xhci-hcd.4.auto: WARN Set TR Deq Ptr cmd failed due to incorrect slot or ep state.
Sep 29 23:03:37 embest-imx8m kernel: [13882.204356] usb 2-1: reset SuperSpeed Gen 1 USB device number 116 using xhci-hcd
Sep 29 23:03:37 embest-imx8m kernel: [13882.288812] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:03:37 embest-imx8m kernel: [13882.524587] usb 2-1: reset SuperSpeed Gen 1 USB device number 116 using xhci-hcd
Sep 29 23:03:37 embest-imx8m kernel: [13882.608797] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:03:38 embest-imx8m kernel: [13883.165004] usb 2-1: reset SuperSpeed Gen 1 USB device number 116 using xhci-hcd
Sep 29 23:03:38 embest-imx8m kernel: [13883.201273] usb 2-1: device descriptor read/8, error -71
Sep 29 23:03:38 embest-imx8m kernel: [13883.314541] usb 2-1: reset SuperSpeed Gen 1 USB device number 116 using xhci-hcd
Sep 29 23:03:38 embest-imx8m kernel: [13883.630512] usb 2-1: USB disconnect, device number 116
Sep 29 23:03:38 embest-imx8m kernel: [13883.768721] usb 2-1: new SuperSpeed Gen 1 USB device number 117 using xhci-hcd
Sep 29 23:03:38 embest-imx8m kernel: [13883.926413] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:03:43 embest-imx8m kernel: [13887.989234] cdc_acm 2-1:1.1: failed to set dtr/rts
Sep 29 23:03:43 embest-imx8m kernel: [13887.994162] xhci-hcd xhci-hcd.4.auto: WARN Set TR Deq Ptr cmd failed due to incorrect slot or ep state.
Sep 29 23:03:43 embest-imx8m kernel: [13888.220631] usb 2-1: reset SuperSpeed Gen 1 USB device number 117 using xhci-hcd
Sep 29 23:03:43 embest-imx8m kernel: [13888.262433] usb 2-1: unable to get BOS descriptor or descriptor too short
Sep 29 23:03:43 embest-imx8m kernel: [13888.269260] usb 2-1: device firmware changed
Sep 29 23:03:43 embest-imx8m kernel: [13888.449964] usb 2-1: USB disconnect, device number 117
Sep 29 23:03:43 embest-imx8m kernel: [13888.583161] usb 2-1: new SuperSpeed Gen 1 USB device number 118 using xhci-hcd
Sep 29 23:03:43 embest-imx8m kernel: [13888.729635] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:03:45 embest-imx8m kernel: [13890.844307] usb 2-1: reset SuperSpeed Gen 1 USB device number 118 using xhci-hcd
Sep 29 23:03:45 embest-imx8m kernel: [13890.907817] usb 2-1: can't restore configuration #1 (error=-71)
Sep 29 23:03:46 embest-imx8m kernel: [13891.090540] usb 2-1: USB disconnect, device number 118
Sep 29 23:03:46 embest-imx8m kernel: [13891.227147] usb 2-1: new SuperSpeed Gen 1 USB device number 119 using xhci-hcd
Sep 29 23:03:46 embest-imx8m kernel: [13891.381938] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:03:53 embest-imx8m kernel: [13898.563335] cdc_acm 2-1:1.1: failed to set dtr/rts
Sep 29 23:03:53 embest-imx8m kernel: [13898.568268] xhci-hcd xhci-hcd.4.auto: WARN Set TR Deq Ptr cmd failed due to incorrect slot or ep state.
Sep 29 23:03:53 embest-imx8m kernel: [13898.780341] usb 2-1: reset SuperSpeed Gen 1 USB device number 119 using xhci-hcd
Sep 29 23:03:53 embest-imx8m kernel: [13898.866879] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:03:54 embest-imx8m kernel: [13899.100477] usb 2-1: reset SuperSpeed Gen 1 USB device number 119 using xhci-hcd
Sep 29 23:03:54 embest-imx8m kernel: [13899.188221] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:04:06 embest-imx8m kernel: [13911.398974] cdc_acm 2-1:1.1: failed to set dtr/rts
Sep 29 23:04:06 embest-imx8m kernel: [13911.403916] xhci-hcd xhci-hcd.4.auto: WARN Set TR Deq Ptr cmd failed due to incorrect slot or ep state.
Sep 29 23:04:06 embest-imx8m kernel: [13911.612750] usb 2-1: reset SuperSpeed Gen 1 USB device number 119 using xhci-hcd
Sep 29 23:04:06 embest-imx8m kernel: [13911.667048] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:04:07 embest-imx8m kernel: [13911.964495] usb 2-1: reset SuperSpeed Gen 1 USB device number 119 using xhci-hcd
Sep 29 23:04:07 embest-imx8m kernel: [13912.019496] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:04:12 embest-imx8m kernel: [13917.707113] cdc_acm 2-1:1.1: failed to set dtr/rts
Sep 29 23:04:12 embest-imx8m kernel: [13917.712038] xhci-hcd xhci-hcd.4.auto: WARN Set TR Deq Ptr cmd failed due to incorrect slot or ep state.
Sep 29 23:04:12 embest-imx8m kernel: [13917.948595] usb 2-1: reset SuperSpeed Gen 1 USB device number 119 using xhci-hcd
Sep 29 23:04:13 embest-imx8m kernel: [13917.974174] usb 2-1: device descriptor read/8, error -71
Sep 29 23:04:13 embest-imx8m kernel: [13918.086534] usb 2-1: reset SuperSpeed Gen 1 USB device number 119 using xhci-hcd
Sep 29 23:04:13 embest-imx8m kernel: [13918.402519] usb 2-1: USB disconnect, device number 119
Sep 29 23:04:13 embest-imx8m kernel: [13918.539128] usb 2-1: new SuperSpeed Gen 1 USB device number 120 using xhci-hcd
Sep 29 23:04:13 embest-imx8m kernel: [13918.678569] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:04:17 embest-imx8m kernel: [13922.646447] cdc_acm 2-1:1.1: failed to set dtr/rts
Sep 29 23:04:17 embest-imx8m kernel: [13922.651373] xhci-hcd xhci-hcd.4.auto: WARN Set TR Deq Ptr cmd failed due to incorrect slot or ep state.
Sep 29 23:04:17 embest-imx8m kernel: [13922.876414] usb 2-1: reset SuperSpeed Gen 1 USB device number 120 using xhci-hcd
Sep 29 23:04:17 embest-imx8m kernel: [13922.964954] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:04:18 embest-imx8m kernel: [13923.196434] usb 2-1: reset SuperSpeed Gen 1 USB device number 120 using xhci-hcd
Sep 29 23:04:18 embest-imx8m kernel: [13923.281841] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:04:20 embest-imx8m kernel: [13925.825817] cdc_acm 2-1:1.1: failed to set dtr/rts
Sep 29 23:04:20 embest-imx8m kernel: [13925.831080] xhci-hcd xhci-hcd.4.auto: WARN Set TR Deq Ptr cmd failed due to incorrect slot or ep state.
Sep 29 23:04:21 embest-imx8m kernel: [13926.044747] usb 2-1: reset SuperSpeed Gen 1 USB device number 120 using xhci-hcd
Sep 29 23:04:21 embest-imx8m kernel: [13926.133518] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:04:21 embest-imx8m kernel: [13926.396493] usb 2-1: reset SuperSpeed Gen 1 USB device number 120 using xhci-hcd
Sep 29 23:04:21 embest-imx8m kernel: [13926.485557] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:04:22 embest-imx8m kernel: [13927.005044] usb 2-1: reset SuperSpeed Gen 1 USB device number 120 using xhci-hcd
Sep 29 23:04:22 embest-imx8m kernel: [13927.058578] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:04:22 embest-imx8m kernel: [13927.260305] usb 2-1: reset SuperSpeed Gen 1 USB device number 120 using xhci-hcd
Sep 29 23:04:22 embest-imx8m kernel: [13927.344003] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:04:32 embest-imx8m kernel: [13937.649425] cdc_acm 2-1:1.1: failed to set dtr/rts
Sep 29 23:04:32 embest-imx8m kernel: [13937.654374] xhci-hcd xhci-hcd.4.auto: WARN Set TR Deq Ptr cmd failed due to incorrect slot or ep state.
Sep 29 23:04:32 embest-imx8m kernel: [13937.884774] usb 2-1: reset SuperSpeed Gen 1 USB device number 120 using xhci-hcd
Sep 29 23:04:32 embest-imx8m kernel: [13937.947807] usb 2-1: can't restore configuration #1 (error=-19)
Sep 29 23:04:33 embest-imx8m kernel: [13938.130523] usb 2-1: USB disconnect, device number 120
Sep 29 23:04:33 embest-imx8m kernel: [13938.267163] usb 2-1: new SuperSpeed Gen 1 USB device number 121 using xhci-hcd
Sep 29 23:04:33 embest-imx8m kernel: [13938.424495] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:04:40 embest-imx8m kernel: [13945.948002] cdc_acm 2-1:1.1: failed to set dtr/rts
Sep 29 23:04:40 embest-imx8m kernel: [13945.952931] xhci-hcd xhci-hcd.4.auto: WARN Set TR Deq Ptr cmd failed due to incorrect slot or ep state.
Sep 29 23:04:41 embest-imx8m kernel: [13946.172569] usb 2-1: reset SuperSpeed Gen 1 USB device number 121 using xhci-hcd
Sep 29 23:04:41 embest-imx8m kernel: [13946.260478] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:04:41 embest-imx8m kernel: [13946.492524] usb 2-1: reset SuperSpeed Gen 1 USB device number 121 using xhci-hcd
Sep 29 23:04:41 embest-imx8m kernel: [13946.576516] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:04:50 embest-imx8m kernel: [13955.463006] cdc_acm 2-1:1.1: failed to set dtr/rts
Sep 29 23:04:50 embest-imx8m kernel: [13955.467931] xhci-hcd xhci-hcd.4.auto: WARN Set TR Deq Ptr cmd failed due to incorrect slot or ep state.
Sep 29 23:04:50 embest-imx8m kernel: [13955.676639] usb 2-1: reset SuperSpeed Gen 1 USB device number 121 using xhci-hcd
Sep 29 23:04:50 embest-imx8m kernel: [13955.759893] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:04:51 embest-imx8m kernel: [13956.028337] usb 2-1: reset SuperSpeed Gen 1 USB device number 121 using xhci-hcd
Sep 29 23:04:51 embest-imx8m kernel: [13956.117087] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:04:58 embest-imx8m kernel: [13963.416943] cdc_acm 2-1:1.1: failed to set dtr/rts
Sep 29 23:04:58 embest-imx8m kernel: [13963.421869] xhci-hcd xhci-hcd.4.auto: WARN Set TR Deq Ptr cmd failed due to incorrect slot or ep state.
Sep 29 23:04:58 embest-imx8m kernel: [13963.644646] usb 2-1: reset SuperSpeed Gen 1 USB device number 121 using xhci-hcd
Sep 29 23:04:58 embest-imx8m kernel: [13963.711022] usb 2-1: can't restore configuration #1 (error=-71)
Sep 29 23:04:58 embest-imx8m kernel: [13963.894512] usb 2-1: USB disconnect, device number 121
Sep 29 23:04:59 embest-imx8m kernel: [13964.059683] usb 2-1: new SuperSpeed Gen 1 USB device number 122 using xhci-hcd
Sep 29 23:04:59 embest-imx8m kernel: [13964.215280] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:05:02 embest-imx8m kernel: [13967.955987] cdc_acm 2-1:1.1: failed to set dtr/rts
Sep 29 23:05:02 embest-imx8m kernel: [13967.960933] xhci-hcd xhci-hcd.4.auto: WARN Set TR Deq Ptr cmd failed due to incorrect slot or ep state.
Sep 29 23:05:03 embest-imx8m kernel: [13968.188744] usb 2-1: reset SuperSpeed Gen 1 USB device number 122 using xhci-hcd
Sep 29 23:05:03 embest-imx8m kernel: [13968.239884] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:05:03 embest-imx8m kernel: [13968.508375] usb 2-1: reset SuperSpeed Gen 1 USB device number 122 using xhci-hcd
Sep 29 23:05:03 embest-imx8m kernel: [13968.595164] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:05:07 embest-imx8m kernel: [13972.572635] usb 2-1: reset SuperSpeed Gen 1 USB device number 122 using xhci-hcd
Sep 29 23:05:07 embest-imx8m kernel: [13972.635887] usb 2-1: can't restore configuration #1 (error=-71)
Sep 29 23:05:07 embest-imx8m kernel: [13972.817984] usb 2-1: USB disconnect, device number 122
Sep 29 23:05:07 embest-imx8m kernel: [13972.955176] usb 2-1: new SuperSpeed Gen 1 USB device number 123 using xhci-hcd
Sep 29 23:05:08 embest-imx8m kernel: [13973.110349] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:05:14 embest-imx8m kernel: [13979.604277] cdc_acm 2-1:1.1: failed to set dtr/rts
Sep 29 23:05:14 embest-imx8m kernel: [13979.609226] xhci-hcd xhci-hcd.4.auto: WARN Set TR Deq Ptr cmd failed due to incorrect slot or ep state.
Sep 29 23:05:14 embest-imx8m kernel: [13979.836339] usb 2-1: reset SuperSpeed Gen 1 USB device number 123 using xhci-hcd
Sep 29 23:05:14 embest-imx8m kernel: [13979.924154] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:05:15 embest-imx8m kernel: [13980.156574] usb 2-1: reset SuperSpeed Gen 1 USB device number 123 using xhci-hcd
Sep 29 23:05:15 embest-imx8m kernel: [13980.242858] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:05:15 embest-imx8m kernel: [13980.860738] usb 2-1: reset SuperSpeed Gen 1 USB device number 123 using xhci-hcd
Sep 29 23:05:15 embest-imx8m kernel: [13980.916146] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:05:16 embest-imx8m kernel: [13981.148415] usb 2-1: reset SuperSpeed Gen 1 USB device number 123 using xhci-hcd
Sep 29 23:05:16 embest-imx8m kernel: [13981.234911] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:05:22 embest-imx8m kernel: [13987.025102] cdc_acm 2-1:1.1: failed to set dtr/rts
Sep 29 23:05:22 embest-imx8m kernel: [13987.030065] xhci-hcd xhci-hcd.4.auto: WARN Set TR Deq Ptr cmd failed due to incorrect slot or ep state.
Sep 29 23:05:22 embest-imx8m kernel: [13987.260662] usb 2-1: reset SuperSpeed Gen 1 USB device number 123 using xhci-hcd
Sep 29 23:05:22 embest-imx8m kernel: [13987.331225] usb 2-1: can't restore configuration #1 (error=-71)
Sep 29 23:05:22 embest-imx8m kernel: [13987.514534] usb 2-1: USB disconnect, device number 123
Sep 29 23:05:22 embest-imx8m kernel: [13987.677253] usb 2-1: new SuperSpeed Gen 1 USB device number 124 using xhci-hcd
Sep 29 23:05:22 embest-imx8m kernel: [13987.831115] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:05:32 embest-imx8m kernel: [13997.618261] cdc_acm 2-1:1.1: failed to set dtr/rts
Sep 29 23:05:32 embest-imx8m kernel: [13997.623195] xhci-hcd xhci-hcd.4.auto: WARN Set TR Deq Ptr cmd failed due to incorrect slot or ep state.
Sep 29 23:05:32 embest-imx8m kernel: [13997.852394] usb 2-1: reset SuperSpeed Gen 1 USB device number 124 using xhci-hcd
Sep 29 23:05:32 embest-imx8m kernel: [13997.915829] usb 2-1: can't restore configuration #1 (error=-19)
Sep 29 23:05:33 embest-imx8m kernel: [13998.097966] usb 2-1: USB disconnect, device number 124
Sep 29 23:05:33 embest-imx8m kernel: [13998.235811] usb 2-1: new SuperSpeed Gen 1 USB device number 125 using xhci-hcd
Sep 29 23:05:33 embest-imx8m kernel: [13998.391492] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:05:35 embest-imx8m kernel: [14000.490990] cdc_acm 2-1:1.1: failed to set dtr/rts
Sep 29 23:05:35 embest-imx8m kernel: [14000.495942] xhci-hcd xhci-hcd.4.auto: WARN Set TR Deq Ptr cmd failed due to incorrect slot or ep state.
Sep 29 23:05:35 embest-imx8m kernel: [14000.732508] usb 2-1: reset SuperSpeed Gen 1 USB device number 125 using xhci-hcd
Sep 29 23:05:35 embest-imx8m kernel: [14000.802139] usb 2-1: can't restore configuration #1 (error=-71)
Sep 29 23:05:36 embest-imx8m kernel: [14000.986998] usb 2-1: USB disconnect, device number 125
Sep 29 23:05:36 embest-imx8m kernel: [14001.147140] usb 2-1: new SuperSpeed Gen 1 USB device number 126 using xhci-hcd
Sep 29 23:05:36 embest-imx8m kernel: [14001.307402] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:05:39 embest-imx8m kernel: [14004.572434] usb 2-1: reset SuperSpeed Gen 1 USB device number 126 using xhci-hcd
Sep 29 23:05:39 embest-imx8m kernel: [14004.640826] usb 2-1: can't restore configuration #1 (error=-71)
Sep 29 23:05:39 embest-imx8m kernel: [14004.826527] usb 2-1: USB disconnect, device number 126
Sep 29 23:05:40 embest-imx8m kernel: [14004.988188] usb 2-1: new SuperSpeed Gen 1 USB device number 127 using xhci-hcd
Sep 29 23:05:40 embest-imx8m kernel: [14005.143541] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:05:49 embest-imx8m kernel: [14014.620213] cdc_acm 2-1:1.1: failed to set dtr/rts
Sep 29 23:05:49 embest-imx8m kernel: [14014.625157] xhci-hcd xhci-hcd.4.auto: WARN Set TR Deq Ptr cmd failed due to incorrect slot or ep state.
Sep 29 23:05:49 embest-imx8m kernel: [14014.844540] usb 2-1: reset SuperSpeed Gen 1 USB device number 127 using xhci-hcd
Sep 29 23:05:49 embest-imx8m kernel: [14014.898998] alloc_contig_range: [44148, 4414d) PFNs busy
Sep 29 23:05:49 embest-imx8m kernel: [14014.905579] alloc_contig_range: [44150, 44155) PFNs busy
Sep 29 23:05:49 embest-imx8m kernel: [14014.912974] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:05:50 embest-imx8m kernel: [14015.131914] usb 2-1: reset SuperSpeed Gen 1 USB device number 127 using xhci-hcd
Sep 29 23:05:50 embest-imx8m kernel: [14015.183139] alloc_contig_range: [44148, 4414d) PFNs busy
Sep 29 23:05:50 embest-imx8m kernel: [14015.189236] alloc_contig_range: [44150, 44155) PFNs busy
Sep 29 23:05:50 embest-imx8m kernel: [14015.195870] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:05:50 embest-imx8m kernel: [14015.773013] usb 2-1: reset SuperSpeed Gen 1 USB device number 127 using xhci-hcd
Sep 29 23:05:50 embest-imx8m kernel: [14015.827316] alloc_contig_range: [44148, 4414d) PFNs busy
Sep 29 23:05:50 embest-imx8m kernel: [14015.833899] alloc_contig_range: [44150, 44155) PFNs busy
Sep 29 23:05:50 embest-imx8m kernel: [14015.841328] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:05:50 embest-imx8m kernel: [14015.847876] usb 2-1: USB disconnect, device number 127
Sep 29 23:05:51 embest-imx8m kernel: [14016.171142] usb 2-1: new SuperSpeed Gen 1 USB device number 2 using xhci-hcd
Sep 29 23:05:51 embest-imx8m kernel: [14016.311063] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:05:58 embest-imx8m kernel: [14023.791426] cdc_acm 2-1:1.1: failed to set dtr/rts
Sep 29 23:05:58 embest-imx8m kernel: [14023.796375] xhci-hcd xhci-hcd.4.auto: WARN Set TR Deq Ptr cmd failed due to incorrect slot or ep state.
Sep 29 23:05:59 embest-imx8m kernel: [14024.028688] usb 2-1: reset SuperSpeed Gen 1 USB device number 2 using xhci-hcd
Sep 29 23:05:59 embest-imx8m kernel: [14024.082653] alloc_contig_range: [44148, 4414d) PFNs busy
Sep 29 23:05:59 embest-imx8m kernel: [14024.089235] alloc_contig_range: [44150, 44155) PFNs busy
Sep 29 23:05:59 embest-imx8m kernel: [14024.096639] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:05:59 embest-imx8m kernel: [14024.316579] usb 2-1: reset SuperSpeed Gen 1 USB device number 2 using xhci-hcd
Sep 29 23:05:59 embest-imx8m kernel: [14024.366188] alloc_contig_range: [44148, 4414d) PFNs busy
Sep 29 23:05:59 embest-imx8m kernel: [14024.372284] alloc_contig_range: [44150, 44155) PFNs busy
Sep 29 23:05:59 embest-imx8m kernel: [14024.378923] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:06:08 embest-imx8m kernel: [14033.226793] cdc_acm 2-1:1.1: failed to set dtr/rts
Sep 29 23:06:08 embest-imx8m kernel: [14033.231714] xhci-hcd xhci-hcd.4.auto: WARN Set TR Deq Ptr cmd failed due to incorrect slot or ep state.
Sep 29 23:06:08 embest-imx8m kernel: [14033.468725] usb 2-1: reset SuperSpeed Gen 1 USB device number 2 using xhci-hcd
Sep 29 23:06:08 embest-imx8m kernel: [14033.512531] usb 2-1: device descriptor read/all, error -71
Sep 29 23:06:08 embest-imx8m kernel: [14033.715195] usb 2-1: reset SuperSpeed Gen 1 USB device number 2 using xhci-hcd
Sep 29 23:06:08 embest-imx8m kernel: [14033.779225] alloc_contig_range: [44148, 4414d) PFNs busy
Sep 29 23:06:08 embest-imx8m kernel: [14033.785808] alloc_contig_range: [44150, 44155) PFNs busy
Sep 29 23:06:08 embest-imx8m kernel: [14033.793230] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:06:19 embest-imx8m kernel: [14044.818418] cdc_acm 2-1:1.1: failed to set dtr/rts
Sep 29 23:06:19 embest-imx8m kernel: [14044.823350] xhci-hcd xhci-hcd.4.auto: WARN Set TR Deq Ptr cmd failed due to incorrect slot or ep state.
Sep 29 23:06:20 embest-imx8m kernel: [14045.052977] usb 2-1: reset SuperSpeed Gen 1 USB device number 2 using xhci-hcd
Sep 29 23:06:20 embest-imx8m kernel: [14045.123052] usb 2-1: can't restore configuration #1 (error=-71)
Sep 29 23:06:20 embest-imx8m kernel: [14045.306533] usb 2-1: USB disconnect, device number 2
Sep 29 23:06:20 embest-imx8m kernel: [14045.467765] usb 2-1: new SuperSpeed Gen 1 USB device number 3 using xhci-hcd
Sep 29 23:06:20 embest-imx8m kernel: [14045.592230] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:06:21 embest-imx8m kernel: [14046.300466] usb 2-1: reset SuperSpeed Gen 1 USB device number 3 using xhci-hcd
Sep 29 23:06:21 embest-imx8m kernel: [14046.363843] usb 2-1: can't restore configuration #1 (error=-71)
Sep 29 23:06:21 embest-imx8m kernel: [14046.546535] usb 2-1: USB disconnect, device number 3
Sep 29 23:06:21 embest-imx8m kernel: [14046.682904] usb 2-1: new SuperSpeed Gen 1 USB device number 4 using xhci-hcd
Sep 29 23:06:21 embest-imx8m kernel: [14046.839554] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:06:29 embest-imx8m kernel: [14054.244263] cdc_acm 2-1:1.1: failed to set dtr/rts
Sep 29 23:06:29 embest-imx8m kernel: [14054.249225] xhci-hcd xhci-hcd.4.auto: WARN Set TR Deq Ptr cmd failed due to incorrect slot or ep state.
Sep 29 23:06:29 embest-imx8m kernel: [14054.460449] usb 2-1: reset SuperSpeed Gen 1 USB device number 4 using xhci-hcd
Sep 29 23:06:29 embest-imx8m kernel: [14054.486160] usb 2-1: device descriptor read/8, error -71
Sep 29 23:06:29 embest-imx8m kernel: [14054.598537] usb 2-1: reset SuperSpeed Gen 1 USB device number 4 using xhci-hcd
Sep 29 23:06:29 embest-imx8m kernel: [14054.910521] usb 2-1: USB disconnect, device number 4
Sep 29 23:06:30 embest-imx8m kernel: [14055.045108] usb 2-1: new SuperSpeed Gen 1 USB device number 5 using xhci-hcd
Sep 29 23:06:30 embest-imx8m kernel: [14055.190775] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:06:37 embest-imx8m kernel: [14061.980360] usb 2-1: reset SuperSpeed Gen 1 USB device number 5 using xhci-hcd
Sep 29 23:06:37 embest-imx8m kernel: [14062.069036] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:06:37 embest-imx8m kernel: [14062.332627] usb 2-1: reset SuperSpeed Gen 1 USB device number 5 using xhci-hcd
Sep 29 23:06:37 embest-imx8m kernel: [14062.419841] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:06:47 embest-imx8m kernel: [14072.687129] cdc_acm 2-1:1.1: failed to set dtr/rts
Sep 29 23:06:47 embest-imx8m kernel: [14072.692054] xhci-hcd xhci-hcd.4.auto: WARN Set TR Deq Ptr cmd failed due to incorrect slot or ep state.
Sep 29 23:06:47 embest-imx8m kernel: [14072.924322] usb 2-1: reset SuperSpeed Gen 1 USB device number 5 using xhci-hcd
Sep 29 23:06:48 embest-imx8m kernel: [14072.987845] usb 2-1: can't restore configuration #1 (error=-71)
Sep 29 23:06:48 embest-imx8m kernel: [14073.170521] usb 2-1: USB disconnect, device number 5
Sep 29 23:06:48 embest-imx8m kernel: [14073.307451] usb 2-1: new SuperSpeed Gen 1 USB device number 6 using xhci-hcd
Sep 29 23:06:48 embest-imx8m kernel: [14073.459470] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:06:51 embest-imx8m kernel: [14076.028472] usb 2-1: reset SuperSpeed Gen 1 USB device number 6 using xhci-hcd
Sep 29 23:06:51 embest-imx8m kernel: [14076.091886] usb 2-1: can't restore configuration #1 (error=-71)
Sep 29 23:06:51 embest-imx8m kernel: [14076.278533] usb 2-1: USB disconnect, device number 6
Sep 29 23:06:51 embest-imx8m kernel: [14076.443183] usb 2-1: new SuperSpeed Gen 1 USB device number 7 using xhci-hcd
Sep 29 23:06:51 embest-imx8m kernel: [14076.600273] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:06:53 embest-imx8m kernel: [14078.171250] xhci-hcd xhci-hcd.4.auto: WARN: HC couldn't access mem fast enough for slot 1 ep 8
Sep 29 23:06:53 embest-imx8m kernel: [14078.195118] cdc_acm 2-1:1.1: failed to set dtr/rts
Sep 29 23:06:53 embest-imx8m kernel: [14078.200040] xhci-hcd xhci-hcd.4.auto: WARN Set TR Deq Ptr cmd failed due to incorrect slot or ep state.
Sep 29 23:06:53 embest-imx8m kernel: [14078.429189] usb 2-1: reset SuperSpeed Gen 1 USB device number 7 using xhci-hcd
Sep 29 23:06:53 embest-imx8m kernel: [14078.515814] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:06:53 embest-imx8m kernel: [14078.748772] usb 2-1: reset SuperSpeed Gen 1 USB device number 7 using xhci-hcd
Sep 29 23:06:53 embest-imx8m kernel: [14078.836356] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:07:05 embest-imx8m kernel: [14090.376456] cdc_acm 2-1:1.1: failed to set dtr/rts
Sep 29 23:07:05 embest-imx8m kernel: [14090.381398] xhci-hcd xhci-hcd.4.auto: WARN Set TR Deq Ptr cmd failed due to incorrect slot or ep state.
Sep 29 23:07:05 embest-imx8m kernel: [14090.592898] usb 2-1: Device not responding to setup address.
Sep 29 23:07:05 embest-imx8m kernel: [14090.806589] usb 2-1: Device not responding to setup address.
Sep 29 23:07:06 embest-imx8m kernel: [14091.018002] usb 2-1: device not accepting address 7, error -71
Sep 29 23:07:06 embest-imx8m kernel: [14091.782867] usb 2-1: USB disconnect, device number 7
Sep 29 23:07:07 embest-imx8m kernel: [14092.672386] usb 2-1: new SuperSpeed Gen 1 USB device number 8 using xhci-hcd
Sep 29 23:07:07 embest-imx8m kernel: [14092.827469] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:07:11 embest-imx8m kernel: [14096.622869] cdc_acm 2-1:1.1: failed to set dtr/rts
Sep 29 23:07:11 embest-imx8m kernel: [14096.627790] xhci-hcd xhci-hcd.4.auto: WARN Set TR Deq Ptr cmd failed due to incorrect slot or ep state.
Sep 29 23:07:11 embest-imx8m kernel: [14096.860406] usb 2-1: reset SuperSpeed Gen 1 USB device number 8 using xhci-hcd
Sep 29 23:07:11 embest-imx8m kernel: [14096.886134] usb 2-1: device descriptor read/8, error -71
Sep 29 23:07:12 embest-imx8m kernel: [14096.998514] usb 2-1: reset SuperSpeed Gen 1 USB device number 8 using xhci-hcd
Sep 29 23:07:12 embest-imx8m kernel: [14097.310535] usb 2-1: USB disconnect, device number 8
Sep 29 23:07:12 embest-imx8m kernel: [14097.443909] usb 2-1: new SuperSpeed Gen 1 USB device number 9 using xhci-hcd
Sep 29 23:07:12 embest-imx8m kernel: [14097.586641] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:07:23 embest-imx8m kernel: [14108.156308] usb 2-1: reset SuperSpeed Gen 1 USB device number 9 using xhci-hcd
Sep 29 23:07:23 embest-imx8m kernel: [14108.210308] alloc_contig_range: [44148, 4414d) PFNs busy
Sep 29 23:07:23 embest-imx8m kernel: [14108.216925] alloc_contig_range: [44150, 44155) PFNs busy
Sep 29 23:07:23 embest-imx8m kernel: [14108.224337] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:07:23 embest-imx8m kernel: [14108.444310] usb 2-1: reset SuperSpeed Gen 1 USB device number 9 using xhci-hcd
Sep 29 23:07:23 embest-imx8m kernel: [14108.498180] alloc_contig_range: [44148, 4414d) PFNs busy
Sep 29 23:07:23 embest-imx8m kernel: [14108.504761] alloc_contig_range: [44150, 44155) PFNs busy
Sep 29 23:07:23 embest-imx8m kernel: [14108.512175] cdc_acm 2-1:1.1: ttyACM0: USB ACM device
Sep 29 23:07:27 embest-imx8m kernel: [14112.351325] cdc_acm 2-1:1.1: failed to set dtr/rts
Sep 29 23:07:27 embest-imx8m kernel: [14112.356254] xhci-hcd xhci-hcd.4.auto: WARN Set TR Deq Ptr cmd failed due to incorrect slot or ep state.
Sep 29 23:07:27 embest-imx8m kernel: [14112.572497] usb 2-1: reset SuperSpeed Gen 1 USB device number 9 using xhci-hcd
Sep 29 23:07:27 embest-imx8m kernel: [14112.642403] usb 2-1: can't restore configuration #1 (error=-71)
Sep 29 23:07:27 embest-imx8m kernel: [14112.826535] usb 2-1: USB disconnect, device number 9
Sep 29 23:07:28 embest-imx8m kernel: [14112.987860] usb 2-1: new SuperSpeed Gen 1 USB device number 10 using xhci-hcd
Sep 29 23:07:28 embest-imx8m kernel: [14113.144528] cdc_acm 2-1:1.1: ttyACM0: USB ACM device

 

 

 

 

 

 

 

 

 

0 项奖励
6 回复数

1,760 次查看
igorpadykov
NXP Employee
NXP Employee

Hi wenfu

 

one can try patch provided on link

https://community.nxp.com/t5/i-MX-Processors/i-MX8M-USB3-0-HC-died-with-external-USB3-0-hub/m-p/9685...

 

Best regards
igor

0 项奖励

1,752 次查看
wenfu
Contributor III

thank you igorpadykov,

we have seen this issue in the communitytryed this patch before and we have tryed it. but the issue still exist.

I think this patch can solve issue with USB HUB, but my sinario has no HUB, the USB device was connected to i.mx8 directly.

 

 

 

 

 

 

0 项奖励

1,746 次查看
igorpadykov
NXP Employee
NXP Employee

Hi wenfu

 

also issue may be related to usb layout (high signal loss, noise), suggest to recheck it using
0 项奖励

1,733 次查看
wenfu
Contributor III

I don't think this is a hardware issue because we can use USB3.0 Disk normally.

0 项奖励

1,715 次查看
igorpadykov
NXP Employee
NXP Employee

one can try to reproduce issue on NXP i.MX8MK EVK reference board,

if it can not be reproduced, then seems this issue is related to custom board.

 

Best regards
igor

0 项奖励

1,673 次查看
wenfu
Contributor III

Hi igorpadykov,

 i.MX8MK EVK reference board is OK. We have tested it.

We have found some clue for the failue of USB3.0. When we run iperf to test the ethernet  throughput capacity, no matter there are USB transfer or not, and no matter what the devices is,U-disk or other usb3.0 devices, it will fiall. like the bellow kernel msg shows. So it seems ethernet cause USB3.0 fial. I konw EVK board is OK, and we have belief on i.mx8 platform, that's way we choose nxp. I just want you team to give some advices or guidance. The main difference between nxp EVK and our board is we use 2GB ddr4 and rohm pmic and EVK use 3GB lpddr4 and nxp pmic. Looking forward to you reply.

[ 1639.329793] usb 2-1: reset SuperSpeed Gen 1 USB device number 97 using xhci-hcd
[ 1639.629964] usb 2-1: reset SuperSpeed Gen 1 USB device number 97 using xhci-hcd
[ 1640.002084] usb 2-1: reset SuperSpeed Gen 1 USB device number 97 using xhci-hcd
[ 1640.137351] usb 2-1: reset SuperSpeed Gen 1 USB device number 97 using xhci-hcd

 

 

 

0 项奖励