usb host not working on imx7 based sabresd board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

usb host not working on imx7 based sabresd board

1,068 次查看
adnanali
Contributor III

I have build the images from yocto using meta-fsl-arm (jethro) layer for imx7dsabresd board. but the USB host is not working. I have cloned linux-imx from the freescale git repository and when I use zImage and dtb from imx_4.1.15_1.0.0_ga branch the USB's get detected. I want to know whether there is any known issue in kernel 3.14 for imx7 related to USB ?

 

dmesg for kernel 3.14 is attached.

Original Attachment has been moved to: dmesg.txt.zip

标签 (3)
0 项奖励
回复
2 回复数

629 次查看
falstaff
Senior Contributor I

We used 3.14.52 successfully with USB Host functionality on our Colibri iMX7S/D platform, without any specific changes to the USB drivers in the kernel itself. It might be related to device tree and/or regulator (e.g. vbus) control.

But I agree with jimmychan​, use 4.1.15 BSP, it is the future...

0 项奖励
回复

629 次查看
jimmychan
NXP TechSupport
NXP TechSupport

There are a lot of different between 3.14.52 and 4.1.15.

I would suggest you to use 4.1.15 BSP.

0 项奖励
回复