ubuntu won't start in Imx6q sdb board on hdmi monitor

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

ubuntu won't start in Imx6q sdb board on hdmi monitor

跳至解决方案
2,696 次查看
brinihamdi
Contributor II

hi

i have installed successfully ubuntu on the sdcard using mfgtool but i can't display ubuntu on my monitor hdmi because i don't have an LVDS

any solution for my problem please ?

i followed this tutorial in the attached file

标签 (2)
标记 (4)
0 项奖励
回复
1 解答
1,862 次查看
SergioSolis
NXP Employee
NXP Employee

Hello Brini,

Did you set the booting arguments to boot to HDMI?.  I'm attaching the linux user guide which has the necessary information to boot from HDMI. Chapter 7 shows the different configuration for HDMI.

Most probably this is the one you'll need:

setenv bootargs_mmc 'setenv bootargs ${bootargs} root=/dev/mmcblk0p1 rootwait rw video=mxcfb1:dev=ldb,LDB-XGA,if=RGB666 video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24 ip=none'

Let me know if it works.

在原帖中查看解决方案

0 项奖励
回复
5 回复数
1,863 次查看
SergioSolis
NXP Employee
NXP Employee

Hello Brini,

Did you set the booting arguments to boot to HDMI?.  I'm attaching the linux user guide which has the necessary information to boot from HDMI. Chapter 7 shows the different configuration for HDMI.

Most probably this is the one you'll need:

setenv bootargs_mmc 'setenv bootargs ${bootargs} root=/dev/mmcblk0p1 rootwait rw video=mxcfb1:dev=ldb,LDB-XGA,if=RGB666 video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24 ip=none'

Let me know if it works.

0 项奖励
回复
1,862 次查看
yuriychernyshov
Contributor I

Hi.

I have face the same problem also.

I use

SABRE for Automotive Infotainment Based on the i.MX 6 Series

What I do need is use it with HDMI video out put, but when I connect monitor via HDMI to the board I have no video signal, I read somewhere that it is a matter of the Boot Configuration DIP Switches panel, but there is no information about how to configure them.

Does anyone know how manage this issue?

0 项奖励
回复
1,862 次查看
brinihamdi
Contributor II

hi Yuriy

i succesfully installed ubuntu on the imx6 board  and before using mfgtool and downloading the image to the baod make sure that the dip swiches sw6 is set to 0000000 correspond to download mode after that while the downloading is finished reboot the with sdcard and with telnet software like Tera Term try to set bootarguments

0 项奖励
回复
1,862 次查看
brinihamdi
Contributor II

i have used Tera team while sending data to mfgtool and everything is ok but i can't understand when we put argument setenv bootargs_mmc 'setenv bootargs ${bootargs} root=/dev/mmcblk0p1 rootwait rw video=mxcfb1:dev=ldb,LDB-XGA,if=RGB666 video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24 ip=none'

0 项奖励
回复
1,862 次查看
brinihamdi
Contributor II

Thanks  for helping i appreciate that . i didn't set the booting arguments because i can't see arguments when the ubuntu boot after that i configurated the micro sd card the monitor stay blinking  . im using a hdmi adapter to a full hd lcd samsung monitor . is there any problem if i used a micro sd with it adapter instead of sd card in the imx6q board ?

0 项奖励
回复