Hi All,
I have imx6 solo h/w with SLC nand of size 256 MB.I made ubifs filesystem and flashed it in SLC nand.
Now kernel should take filesystem from SLC nand.
I have configured the kernel for required settings and UBIFS is found but could not boot completely from that..
Logs:
nand: device found, Manufacturer ID: 0x2c, Chip ID: 0xaa
nand: Micron MT29F2G08ABBEAH4
nand: 256MiB, SLC, page size: 2048, OOB size: 64
gpmi-nand 112000.gpmi-nand: enable the asynchronous EDO mode 4
Scanning device for bad blocks
Bad eraseblock 100 at 0x000000c80000
Bad eraseblock 101 at 0x000000ca0000
1 ofpart partitions found on MTD device gpmi-nand
Creating 1 MTD partitions on "gpmi-nand":
0x000000020000-0x000000820000 : "root"
UBI: attaching mtd0 to ubi0
UBI: scanning is finished
UBI: attached mtd0 (name "gpmi-nand", size 256 MiB) to ubi0
UBI: PEB size: 131072 bytes (128 KiB), LEB size: 126976 bytes
UBI: min./max. I/O unit sizes: 2048/2048, sub-page size 2048
UBI: VID header offset: 2048 (aligned 2048), data offset: 4096
UBI: good PEBs: 2046, bad PEBs: 2, corrupted PEBs: 0
UBI: user volume: 1, internal volumes: 1, max. volumes count: 128
UBI: max/mean erase counter: 2/1, WL threshold: 4096, image sequence number: 1743731081
UBI: available PEBs: 0, total reserved PEBs: 2046, PEBs reserved for bad PEB handling: 38
UBI: background thread "ubi_bgt0d" started, PID 65
snvs_rtc 20cc034.snvs-rtc-lp: setting system clock to 1970-01-01 00:00:01 UTC (1)
ALSA device list:
No soundcards found.
VFS: Cannot open root device "ubi0:root" or unknown-block(0,0): error -2
Please append a correct "root=" boot option; here are the available partitions:
b300 7684096 mmcblk0 driver: mmcblk
b301 504 mmcblk0p1 1a000003-01
b302 512 mmcblk0p2 1a000003-02
b303 10240 mmcblk0p3 1a000003-03
b304 1 mmcblk0p4
b305 1016 mmcblk0p5 1a000003-05
b306 24568 mmcblk0p6 1a000003-06
b307 2058232 mmcblk0p7 1a000003-07
b308 5588984 mmcblk0p8 1a000003-08
b330 128 mmcblk0rpmb (driver?)
b320 2048 mmcblk0boot1 (driver?)
b310 2048 mmcblk0boot0 (driver?)
Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(0,0)
CPU: 0 PID: 1 Comm: swapper Not tainted 3.10.17 #975
[<80013b70>] (unwind_backtrace+0x0/0x104) from [<80011e60>] (show_stack+0x20/0x24)
[<80011e60>] (show_stack+0x20/0x24) from [<8051deb4>] (dump_stack+0x20/0x28)
[<8051deb4>] (dump_stack+0x20/0x28) from [<8051b978>] (panic+0x8c/0x1dc)
[<8051b978>] (panic+0x8c/0x1dc) from [<80754fb0>] (mount_block_root+0x214/0x2d4)
[<80754fb0>] (mount_block_root+0x214/0x2d4) from [<8075525c>] (prepare_namespace+0x94/0x1c0)
[<8075525c>] (prepare_namespace+0x94/0x1c0) from [<80754be8>] (kernel_init_freeable+0x174/0x1b8)
[<80754be8>] (kernel_init_freeable+0x174/0x1b8) from [<80519960>] (kernel_init+0x1
cat /proc/partition is not listing the mtdblock. Is this the problem??
root@imx6solosabreauto:~# cat /proc/partitions
major minor #blocks name
179 0 7684096 mmcblk0
179 1 504 mmcblk0p1
179 2 512 mmcblk0p2
179 3 10240 mmcblk0p3
179 4 1 mmcblk0p4
179 5 1016 mmcblk0p5
179 6 24568 mmcblk0p6
179 7 2058232 mmcblk0p7
179 8 5588984 mmcblk0p8
179 48 128 mmcblk0rpmb
179 32 2048 mmcblk0boot1
179 16 2048 mmcblk0boot0
cat /proc/mtd is listing the mtd device.
root@imx6solosabreauto:~# cat /proc/mtd
dev: size erasesize name
mtd0: 00800000 00020000 "root"
root@imx6solosabreauto:~#
I created this partition in dtsi file under gpmi node.
partition@4 {
label = "root";
reg = <0x00020000 0x00800000>;
};
};
Let me know what i am missing for making the kernel to take UBIFS from SLC Nand.
Hi kiruthika
for NAND boot please look at attached Linux Guide
sect.8.3 Run the Image from NAND. NAND si supported in
Sabre AI boards, examples : imx6qdl-sabreauto.dtsi,imx6dl-sabreauto.dts.
For NAND programming it is recommended to use MFG Tool on below link
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi igor,
I went through the attached document and for information, we have customized uboot and my uboot is not aware of SLC nand at all.
So mtdparts is unknown. Only kernel is aware of this SLC NAND and I have UBIFS In SLC NAND and kernel to take UBIFS from SLC NAND.
Any clues on how to add partition in kernel and cat /proc/partition to show /dev/mtdblock0??
Hi igor,
Thanks for your reference.
I have partitioned SLC nand
gpmi: gpmi-nand@00112000 {
compatible = "fsl,imx6q-gpmi-nand";
#address-cells = <1>;
#size-cells = <1>;
reg = <0x00112000 0x2000>, <0x00114000 0x2000>;
reg-names = "gpmi-nand", "bch";
interrupts = <0 15 0x04>;
interrupt-names = "bch";
clocks = <&clks 152>, <&clks 153>, <&clks 151>,
<&clks 150>, <&clks 149>;
clock-names = "gpmi_io", "gpmi_apb", "gpmi_bch",
"gpmi_bch_apb", "per1_bch";
dmas = <&dma_apbh 0>;
dma-names = "rx-tx";
status = "okay";
partition@0 {
label = "rootfs";
reg = <0x000010 0x00800000>;
};
partition@1 {
label = "persistent";
reg = <0x00800000 0x00900000>;
};
};
Kernel command line options for MTD includes
CONFIG_MTD=y
CONFIG_MTD_CMDLINE_PARTS=y
CONFIG_MTD_OF_PARTS=y
CONFIG_MTD_BLKDEVS=y
CONFIG_MTD_BLOCK=y
root@imx6solosabreauto:~# cat /proc/partitions
major minor #blocks name
31 0 262144 mtdblock0
mtdblock0 and mtdblock1 is expected but its not shown.
May i know what else i need to do for making the partitions in DTS file to be visible in cat /proc/partitions