Hai.,.,
Thanks for the response.
Yes you are correct, after changing to mmc 1:1 it was loading into RAM successfully , Now if I give go command its throwing a data abort error and also board is getting Reset. Any Idea what could be the issue,
I am running standalone program without modifying single line
Here is the log
=>
=> fatload mmc 1:2 0x12000000 hello_world.bin
578 bytes read in 13 ms (43 KiB/s)
=>
=> go 0x12000000
## Starting application at 0x12000000 ...
data abort
pc : [<12000008>] lr : [<4ff683d7>]
reloc pc : [<d989b008>] lr : [<178033d7>]
sp : 4f564d48 ip : 0000001c fp : 00000002
r10: 4ffc436c r9 : 4f564ea8 r8 : 4f567938
r7 : 4ff683ad r6 : 00000002 r5 : 12000000 r4 : 4f56793c
r3 : 12000000 r2 : 4f56793c r1 : 4f56793c r0 : 00000001
Flags: nzCv IRQs off FIQs off Mode SVC_32
Code: e4df8df7 cedfb73f 41f0e92d 46084605 (2400460e)
Resetting CPU ...
resetting ...
U-Boot SPL 2018.07-rc2-dirty (Aug 24 2018 - 10:03:53 +0530)
Trying to boot from MMC1
U-Boot 2018.07-rc2-dirty (Aug 24 2018 - 10:03:53 +0530)
CPU: Freescale i.MX6Q rev1.2 996 MHz (running at 792 MHz)
CPU: Automotive temperature grade (-40C to 125C) at 48C
Reset cause: WDOG
Board: MX6-SabreSD
I2C: ready
DRAM: 1 GiB
PMIC: PFUZE100 ID=0x10
MMC: FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2
Loading Environment from MMC... *** Warning - bad CRC, using default environment
Failed (-5)
PCI: pcie phy link never came up
No panel detected: default to Hannstar-XGA
Display: Hannstar-XGA (1024x768)
In: serial
Out: serial
Err: serial
Net: FEC [PRIME]
Press SPACE to abort autoboot in 2 seconds
=>
CTRL-A Z for help | 115200 8N1 | NOR | Minicom 2.7 | VT102 | Offline | ttyUSB0
Thank you.
Regards
Karthik