the imax8 support max raw sensor ? raw 10 bit or raw 16bit?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

the imax8 support max raw sensor ? raw 10 bit or raw 16bit?

1,532件の閲覧回数
gavin-luo
Contributor I

imax8 support max raw sensor bits? 16bit  or 10 bit

0 件の賞賛
1 返信

550件の閲覧回数
art
NXP Employee
NXP Employee

The i.MX8 series processors do not support parallel camera interface, they only support MIPI-CSI2 interface. On this interface, they support all RAW data formats up to RAW16. The i.MX8M and i.MX8X series processors only support up to RAW14 data formats.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛