tCKELCK issue on mscale_ddr_tool of IMX8M EVK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

tCKELCK issue on mscale_ddr_tool of IMX8M EVK

885件の閲覧回数
mikesu
Contributor I

Topic :  tCKELCK issue on mscale_ddr_tool of IMX8M EVK .

When I run mscale_ddr_tool on imx8m EVK and found out that

1. some lpddr4 can't pass mscale_ddr_test stress test by version 2.1 but pass version beta.

    This failure would happen at hot temperature only. All samples could pass at room temperature.

2.  After comparing btween V2.1 and beta version , we found out that

     a. V2.1 (V1.1 are the same) : CKE toggle 2 times at the beginning of stress test

         While CKE  toggle, its tCKELCK is 0ns and against its specification.

         Even we changed setup value of tCKELCK of ds file, tCKELCK still kept 0ns

     b. V beta: CKE always keep high within stress test

3. Please see the attached file for the detailed waveforms and information

Request : could you fix up this tCKELCK issue of mscale_ddr_tool?

ラベル(1)
3 返答(返信)

689件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  The issue will be fixed in the next release.

Regards,

Yuri.

0 件の賞賛

689件の閲覧回数
oliver_chen
NXP Employee
NXP Employee

Hi YuriMuhin_ng‌,

This issue is only happened in DDR tool stress test function, not in timing parameters, generated code and uboot/Linux. Customer can use current DDR tool in their projects without any problems.

B.R

Oliver

689件の閲覧回数
oliver_chen
NXP Employee
NXP Employee

Hi,

Now I'm working with customers to find the root cause.

B.R

Oliver