supported USB Camera moules for i.MX7D / Android N7.1.2_2.0.0

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

supported USB Camera moules for i.MX7D / Android N7.1.2_2.0.0

766件の閲覧回数
eric_kang
Contributor II

Dear All,

I'm finding the USB Camera module for i.MX7D / Android N7.1.2_2.0.0.

I confirmed the below USB Cameras were supported in i.MX7D / Android N7.1.2_2.0.0.

Logitech C250 / C920 / E3500

But those cameras couldn't apply to our boards, because the cameras are a stand-alone USB type Camera, not module.

So we have to find the module type USB Camera.

Please tell me if you know the camera module.

Best Regards,
Eric.

ラベル(3)
0 件の賞賛
1 返信

403件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Eric

I have internal confirmation that usb camera is not supported on MX7D.

The release note will be updated.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛