srktool - number of fuses per word

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

srktool - number of fuses per word

677件の閲覧回数
antonio_santagi
Contributor IV

Hello, 

I am using imX8M mini.

when launching srktool  , what setting should I choose for the number of fuses per word ? 8 fuses per word or 32 fuses per word ?

-f, --fuse_format <format>:
Optional, Data format of the SRK efuse binary file. The
format may be selected by setting <format> to either:
- 0: 8 fuses per word, ex: 00 00 00 0a 00 00 00 01 ...
- 1 (default): 32 fuses per word, ex: 0a 01 ff 8e

thank you

ラベル(2)
タグ(3)
2 返答(返信)

593件の閲覧回数
Yuri
NXP Employee
NXP Employee

 

Hello,

 

   default  value for -f parameter  - 1 (default): 32 fuses per word  is usually used.

 

       $ ../linux64/bin/srktool -h 4 -t SRK_1_2_3_4_table.bin -e SRK_1_2_3_4_fuse.bin -d

       sha256 -c SRK1_sha256_2048_65537_v3_ca_crt.pem,

       SRK2_sha256_2048_65537_v3_ca_crt.pem,

       SRK3_sha256_2048_65537_v 3_ca_crt.pem,

       SRK4_sha256_2048_65537_v3_ca_crt.pem

 

Have a great day,

Yuri.

 

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

 

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

593件の閲覧回数
antonio_santagi
Contributor IV

Ok, I will use 32 fuses per word then, thank you.