sources for GLES Demos on imx6Q

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

sources for GLES Demos on imx6Q

2,989件の閲覧回数
spre
Contributor II

Hello,

we try to learn more about how to use GLES 2.0 on imx6q.

For that reason, we'd like to have the sources for the GLES 2.0 Demos.

The package gpu-viv-src tries to get the sources from

http://bitshrine.org/gpp/gpu-viv-src-12.09.01.tar.gz:

but there they are not available any more.

Also Google doesn't have any hits on those search criteria.

Can you please provide the sources?

regards,

Sascha

ラベル(1)
タグ(4)
10 返答(返信)

1,695件の閲覧回数
andre_silva
NXP Employee
NXP Employee

The i.MX6 GPU demos will be released with the i.MX6 GPU SDK next month (I think)

0 件の賞賛

1,695件の閲覧回数
weizhuang
Contributor I

Has this i.MX6 GPU demo been releases?

Ive got my application running on X11 (Oneiric), but I want to remove X11 dependence. My application only uses XOpenDisplay and XCreateWindow, can I replace them with EGL functions? 

0 件の賞賛

1,695件の閲覧回数
andre_silva
NXP Employee
NXP Employee

Yes, you will just need to change these functions in the initialization code, you can get some samples here: github.com/andreluizeng

1,695件の閲覧回数
yuanlu
Contributor I

I ask you who this “gpu-viv-src-12.09.01.tar.gz” file?

I imx6 on develop opengles program。

please help me?

0 件の賞賛

1,695件の閲覧回数
andre_silva
NXP Employee
NXP Employee

this tarball is meant to contains the GPU driver source code not the demos, and as this code is proprietary is not available for downloading, there is this blog: www.imxcv.blogspot.com that has some gpu demos with source code (www.github.com/andreluizeng) that you could give it a try. I´m going to check where is the correctly repository with the gpu demos available to imx6 with source code and you know.

0 件の賞賛

1,695件の閲覧回数
spre
Contributor II

Hello yuanlu

as mentioned above, I didn't get information where to get the sources from.

regards,

Sascha

yuanlu lu https://community.freescale.com/people/yuanlu created the

discussion

"sources for GLES Demos on imx6Q"

To view the discussion, visit:

https://community.freescale.com/message/310959#310959

>

0 件の賞賛

1,695件の閲覧回数
daiane_angolini
NXP Employee
NXP Employee

You're able to find this package inside 12.09.01 BSP tarball.

That one that installs the LTIB. You can take the file and open it.

Please, let me know if it works for you

0 件の賞賛

1,695件の閲覧回数
spre
Contributor II

Hello Daiane,

thanks for that. But we tried that. The package does not contain the sources, but the link to the above mentioned website, to fetch the sources from there. But they are not available there any more.

0 件の賞賛

1,695件の閲覧回数
daiane_angolini
NXP Employee
NXP Employee

do you mean, under:

L3.0.35_12.09.01_GA_source/pkgs/gpu-viv-bin-mx6q-12.09.01.tar.gz?

I can see the file. But I got the tarball a lot of time ago, I´m not sure it there is any modification.

0 件の賞賛

1,695件の閲覧回数
spre
Contributor II

Hi,

no I meant gpu-viv-src-12.09.01.tar.gz

But anyway, we have been able write our own hw supported app and compare it.

So we already reached the goal.

Thanks for your help.

regards,

Sascha