Hello everybody, im new in the community,
i need any help : im testing (sw) the CAAM module on the SABRE i.MX6Dual Lite.
how can i set the different mode of the AESA. and also test the other Accelerators (DESA, AFHA, MDHA).
Thank
First, please let me know if the examples of the Platform SDK were used ?
Re: En/Decryption of data on iMX6 board
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
hey Yuri,
please how do i test the AES _CBC mode.
im using the exemple code this directory:
D:\IMX6SDK\iMX6_Platform_SDK\sdk\drivers\caam..... and i can run well the caam_test for AES_ECB.
But when i change the initialyzation line of caam_internal.h : #define ENCRYPT_DESC4 0x8210020D in order to use the AES_CBC mode unfortunately it does not change these value in the Mode register and does not give out the expected CBC_cipher_test values
Thank you for your answe
Hello,
Thank you for your post, however please consider moving it to the right community place (e.g. i.MX Community ) to get it visible for active members.
For details please see general advice Where to post a Discussion?
Thank you for using Freescale Community.