serial can communication from pc to i.mx8qm

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

serial can communication from pc to i.mx8qm

651 Views
aksh9354
Contributor I
hello I am using serial can communication with the host pc through can USB in the above scenario every time I need to update the USB port in the host PC after board reboot otherwise can bus is going in off state but if again run the command sudo slcand -o -s6 -t hw -S 3000000 /dev/ttyUSB0 that time it is working i already right down one script for bringing can interface up in host pc but every time after board boot up i need to rerun it any solution for this
0 Kudos
3 Replies

636 Views
aksh9354
Contributor I

it is required to reinitialize the serial communication every time when we reboot the i.mx board ?????

0 Kudos

630 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Yes, it does.

 

0 Kudos

643 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello aksh9354,

If you reset the usb you will have to initialize the serial communication.

Regards

 

0 Kudos