sabrelite on Linux 4.14.78 (GA)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

sabrelite on Linux 4.14.78 (GA)

515 次查看
pawel_kopalko
Contributor II

Hi I have boundary devieces flavoured sabrelite board. Linux worked fine on 4.9.98_ga now on 4.14.78 it doesn't (no sign of life after Starting Kernel... ).

4.14.78 kernel requires to enable optee in config, otherwise the smp won't compile, thus the kernel wouldn't compile otherwise. Does it mean that now there are more adaptations required, ie. configuring u-boot optee aware etc, have optee os in the flash/sd. Or this should not matter at all? (the release docs for 4.14.78 state that for the NXP's boards it is always built).

Regards

标签 (2)
标记 (2)
0 项奖励
1 回复

416 次查看
gusarambula
NXP TechSupport
NXP TechSupport

Hello Pawel Kopalko,

The SabreLite board is supported by Boundary Devices so I would recommend contacting them for more information.

The Community BSP does support this board but with default kernel 4.1.15. (More information on the link below)

http://freescale.github.io/doc/release-notes/2.4/

This being said, I would recommend looking at the i.MX BSP Porting Guide, which has a chapter on configuring Optee, which may be of help.  This document is part of the 4.14.78 BSP documentation bundle.

Regards,

0 项奖励