run yocto imx 4.x kernel on mx53 quick start board.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

run yocto imx 4.x kernel on mx53 quick start board.

574件の閲覧回数
wenmingfeng
Contributor III

Hi forks,

I bitbake from yocto master branch for my mx53 quick start board. with 4.6.0-rc7-fslc+g9be3cdc, it can run and login as root. But no gpu driver and display. Even with the core-image-x11 there is no diplay on my VGA display. How can I got the graphics and display working on the latest kernel. The 2.6.35.3 is the one currently supporting all gui/graphics and gstreamer functions. Does someone know a high kernel which can support gstreamer 1.0 on mx53 or a method to do so?

Thanks!

Wenming

ラベル(4)
0 件の賞賛
1 返信

356件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Wenming Feng,

The following thread contains useful information:

https://community.nxp.com/thread/316272 

If you would like to use the GPU you would need to stick to the 2.6.35 kernel, but you should be able to use X11 on newer kernels, just most likely not 4.x.

Regards,

0 件の賞賛