Hello, I built the fsl-image-qt5-validation-imx for the IMX8M Quad using the fsl-wayland distro. I am running a QT application in my imx8 and when trying to enter text into a LineEdit I get "qt.qpa.wayland: xkbcommon not available on this build, not performing key mapping"
Would anyone know how to fix this?
Sorry to reopen the ticket. But I think we can add an answer for whoever ends up here in the future.
I have the same issue, also had `libxkbcommon` into the image under `/usr/lib/` and kept having the same error.
The problem was basically on Yocto build, I missed configuring the qtbase `PACKAGECONFIG` variable to enable the xkbcommon option.
To do that, you add a new layer, create a `qtbase_%.bbappend` file and add:
`PACKAGECONFIG:append:<machinename> = " xkbcommon"`
NOTE: If you don't add the <machinename> you will have failures because other packages won't have the -native extension.
NOTE2: make sure to do that in a clean build (or clean all qt packages), other `ptest` will fail complaining that a configuration was changed, and it doesn't know why.
Hello rthomas,
You need to add that library to yocto build, but xkbcommon still required without X11. Our build does not support X11, just Wayland and nullWindow (EGLFS). It used to work through xkbcommon-evdev only.
Regards