ptn5110 device tree configuration?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ptn5110 device tree configuration?

3,770 Views
amodamatya
Fresh Out Contributor

We have been using imx8qxp processors which has support for USB Power delivery.
In imx8x-mek.dtsi , I can see that there is a node for ptn5110 device. We would want the device to be able to provide 5V, 12V and 15V with 3A current. 

I have changed the source pdos to the values that I have mentioned above in this way, is this a correct implementation? How does the voltage switching in kernel happen? Do I have to write down some properties for the vbus-supply to switch the voltage?

ptn5110@50 {
compatible = "nxp,ptn5110";
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_typec>;
reg = <0x50>;
interrupt-parent = <&lsio_gpio1>;
interrupts = <3 IRQ_TYPE_LEVEL_LOW>;
status = "okay";

usb_con: connector {
compatible = "usb-c-connector";
label = "USB-C";
data-role = "dual";
power-role = "source";
source-pdos = <PDO_FIXED(5000, 3000, PDO_FIXED_USB_COMM)
PDO_FIXED(12000, 3000, PDO_FIXED_USB_COMM)
PDO_FIXED(15000, 3000, PDO_FIXED_USB_COMM)>;

ports {
#address-cells = <1>;
#size-cells = <0>;

port@1 {
reg = <1>;
usb_con_ss: endpoint {
remote-endpoint = <&usb3_data_ss>;
};
};
};
};
};
0 Kudos
Reply
2 Replies

3,754 Views
IvanRuiz
NXP Employee
NXP Employee

Hello,

 

I believe this configuration involves SW and HW but need to check internally. In the meantime, could you please share your schematics in order to check the HW part?

 

Thank you.

 

BR,

Ivan.

0 Kudos
Reply

3,737 Views
amodamatya
Fresh Out Contributor

Hello, thank you for your response and also sorry for the late reply as I am only working as a part time.
We found out, where in the kernel we have to supply the regulator voltage, here
 https://elixir.bootlin.com/linux/latest/source/drivers/usb/typec/tcpm/tcpm.c#L3861,
so we got some idea to move ahead, we will seek your help, if there is any confusions ahead..

0 Kudos
Reply