pinmux tool export

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

pinmux tool export

693件の閲覧回数
inmaku
Contributor III

Hi All,

In order to document the pinmuxing of the iMX6, I'd like to Export the tables. Unfortunately, the Export to .csv leaves off the first row (peripheral/Signal). When exporting to .rtf or .txt, it misses the Signal Notes. Both columns are important for my documentation. For now, I do make Screen shots anmd paste them into my word document - a pretty inefficient way!

Is there another way of doing this Kind or did somebody write a tool to do the pinmuxing like in teh oldder iMX processors, where the pinmux actually was an Excel sheet?

Thanks in advance,

Ingo

ラベル(1)
タグ(2)
0 件の賞賛
1 返信

524件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

The exported information on the IOMUX does changes from format to format. Unfortunately there is not an option that will include all the information you need but I would recommend working from the version closest to your needs (which seems to be the rtf file format) and manually adding the Signal Notes which should be relatively easier since there is usually less information in these columns.

0 件の賞賛