pan profile on bluez5

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

pan profile on bluez5

1,129 Views
sergio_dorazio
Contributor IV

Hi,

have anyone any example how enable PAN profile on Bluez5 ?

I have bluetooth module and it work well with hciconfig, sdptool, bletoothctl utilitys. I never found an example with enabling PAN profile. Have anyone any examples or weblink ?

Sergio.

0 Kudos
4 Replies

1,012 Views
sergio_dorazio
Contributor IV

Ok thanks

0 Kudos

1,012 Views
sergio_dorazio
Contributor IV

Hi Igor,

thank you , but your links cannot help me.

I need to configure PAN profile in my linux on IMX6 microprocessor. The Bluez version is 5.49.

I am following some examples found in internet but nothing work well.

I think, in my kernel linux it isn't necessary set a lot of file or script. For example I have /etc/bluetooth/network.conf file where I can configure bluetooth network. Is it for configure PAN profile ?

Have you an example how I can use and configure bluetooth how lan interface (Pan profile) ?

Am I the first softwareman that need this type of configuration with IMX6ULL EVK ?

Regards

Sergio

0 Kudos

1,012 Views
igorpadykov
NXP Employee
NXP Employee

Hi Sergio

Bluez is not nxp software, may be suggested to post issue to murata support portal :

wireless.murata.com/eng/products/rf-modules-1/wi-fi-bluetooth-for-freescale-i-mx.html

Best regards
igor

0 Kudos

1,012 Views
igorpadykov
NXP Employee
NXP Employee

Hi Sergio

as this is not imx specific question it may be posted on

dedicated wifi/bluetooth forum, like

BCM4343W Bluetooth 4.2 support | Cypress Developer Community 

BlueZ - i.MX6+1DX (Buildroot) | Cypress Developer Community 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos