package compatible of FBGA624 and LFBGA624

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

package compatible of FBGA624 and LFBGA624

928件の閲覧回数
zhitao_zhang
Contributor I

hi, Dear

when I was investigating the imx6 series CPU, one article note that, I.MX6 solo to i.mx 6dualplus series are pin-to- pin and power compatible.

but I found that  there are two package FBGA624 and LFBGA624 . There is minor difference of both package, My question is that , can the two package be soldered compatible?

pastedImage_1.png

ラベル(3)
0 件の賞賛
返信
1 返信

876件の閲覧回数
mrudangshelat1
Senior Contributor II

Hi,

There is a difference in package thickness. Please refer below URL

FBGA624: SOT1643-1 

https://www.nxp.com/docs/en/package-information/SOT1643-1.pdf 

LFBGA624: SOT1642-1 

https://www.nxp.com/docs/en/package-information/98ASA00329D.pdf 

Mrudang

0 件の賞賛
返信