overcurrent protection of PMU of i.MX28

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

overcurrent protection of PMU of i.MX28

Jump to solution
461 Views
yuuki
Senior Contributor II

Dear all,

I have a question about PMU of i.MX28.

When DC-DC is powered by Battery input, does Battery input pin have overcurrent protection function?

Does DCDC converter(output) have overcurrent protection function?

Best Regards,

Yuuki

Labels (1)
0 Kudos
1 Solution
379 Views
igorpadykov
NXP Employee
NXP Employee

Hi Yuuki

there is no overcurrent protection function on

Battery input and DCDC converter outputs.

Best regards

igor
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
380 Views
igorpadykov
NXP Employee
NXP Employee

Hi Yuuki

there is no overcurrent protection function on

Battery input and DCDC converter outputs.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos