ov5640/ov5642 drivers for imx6ulevk board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ov5640/ov5642 drivers for imx6ulevk board

1,165件の閲覧回数
brucelee
Contributor I

I have bought a imx6ulevk development board, and I want to use ov5640/ov5642 camera with auto focus, but I found the bsp(4.1.15) support ov5640 only and the the driver does not support auto focus function, where can I get the ov5642 and ov5640 drivers which support auto focus and can work on imx6ulevk board?

ラベル(1)
0 件の賞賛
3 返答(返信)

695件の閲覧回数
brucelee
Contributor I

I have checked this docs, but the ov5640_mipi.c in drivers/media/platform/mxc/capture is not for imx6ul, it for imx6qdl, the imx6ul use the driver in drivers/media/platform/mxc/subdev, and i found it's very different between this two drivers files...

0 件の賞賛

695件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

ov5640 usage with i.MX6UL is described on

https://community.freescale.com/thread/386695 

unfortunately I am not aware of auto focus support for i.MX6UL,

seems you will have to implement it youself or apply for help to

NXP Professional Services:

http://www.nxp.com/support/nxp-professional-services:PROFESSIONAL-SERVICE

Best regards
igor

0 件の賞賛

695件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi bruce

please check

https://community.nxp.com/thread/430065

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛