Hi Guys,
i'm trying to create a c application which will change brightness value of ov5640.
i have modified the following things:
1-> i have added support for brightness in ioctl_s_ctrl in ov5640_mipi.c
pr_debug("In ov5640:ioctl_s_ctrl %d\n", vc->id);
switch (vc->id) {
case V4L2_CID_BRIGHTNESS:
pr_debug("GB : %s in V4L2_CID_BRIGHTNESS\n",__FUNCTION__);
ov5640_brightness(vc->value); //--> this function hold sitch case for different brightness levels.
2-> in c application i'm opening /dev/video1
struct v4l2_control control;
control.value = seek;//-> seek is range say -4 to +4 from user input.
with help of ioctl(fd,VIDIOC_S_CTRL,&control)
well so far so good.
i have added some debug statement also at regular interval in probe, s_ctrl and g_ctrl also.
but when i'm trying to run application and try to set ctrl value it is not changing. i have checked kernel log also it is not displaying debug statement also.
any help very useful.
regards,
Ganesh
Hi Guys,
Update to my question, now it is working fine but i have on more issue. well after setting brightness value i'm trying to read but brightness value is not updating. i'm using VIDIOC_G_CTRL
control.id = V4L2_CID_BRIGHTNESS;
ioctl(fd,VIDIOC_G_CTRL,&control)
printf("Current value of brightness level is %d\n",control.value);
but the value is zero.
Hi,
Are you modifying the ov5640_data structure when setting the brightness?
As I see the value must be set in the below function.
static int ioctl_s_ctrl(struct v4l2_int_device *s, struct v4l2_control *vc)
{
int retval = 0;
pr_debug("In ov5640:ioctl_s_ctrl %d\n",
vc->id);
switch (vc->id) {
case V4L2_CID_BRIGHTNESS:
break;
case V4L2_CID_CONTRAST:
break;
case V4L2_CID_SATURATION:
break;
case V4L2_CID_HUE:
break;
case V4L2_CID_AUTO_WHITE_BALANCE:
break;
case V4L2_CID_DO_WHITE_BALANCE:
break;
case V4L2_CID_RED_BALANCE:
break;
case V4L2_CID_BLUE_BALANCE:
break;
case V4L2_CID_GAMMA:
break;
case V4L2_CID_EXPOSURE:
break;
case V4L2_CID_AUTOGAIN:
break;
case V4L2_CID_GAIN:
break;
case V4L2_CID_HFLIP:
break;
case V4L2_CID_VFLIP:
break;
default:
retval = -EPERM;
break;
}
return retval;
}
And it is returned in this one:
static int ioctl_g_ctrl(struct v4l2_int_device *s, struct v4l2_control *vc)
{
int ret = 0;
switch (vc->id) {
case V4L2_CID_BRIGHTNESS:
vc->value = ov5640_data.brightness;
break;
case V4L2_CID_HUE:
vc->value = ov5640_data.hue;
break;
case V4L2_CID_CONTRAST:
vc->value = ov5640_data.contrast;
break;
case V4L2_CID_SATURATION:
vc->value = ov5640_data.saturation;
break;
case V4L2_CID_RED_BALANCE:
vc->value = ov5640_data.red;
break;
case V4L2_CID_BLUE_BALANCE:
vc->value = ov5640_data.blue;
break;
case V4L2_CID_EXPOSURE:
vc->value = ov5640_data.ae_mode;
break;
default:
ret = -EINVAL;
}
return ret;
}
As you may notice in the code the ov5640_data.brightness is not modified.
Best Regards,
Alejandro
Hi alejandrolozano yes what you said is correct.
static int ioctl_s_ctrl(struct v4l2_int_device *s, struct v4l2_control *vc)
{
int retval = 0;
pr_debug("In ov5640:ioctl_s_ctrl %d\n",
vc->id);
switch (vc->id) {
case V4L2_CID_BRIGHTNESS: ov5640_brightness(vc->value);
break;
ov5640_brightness(vc->value); -----> it's a function which has switch case statement with different brightness level which can be selected by vc->value from ioctl_s_ctrl by calling ov5640_brightness().
this i have got i'm able to set the values but while i'm trying to read using ioctl_g_ctrl for V4L2_CID_BRIGHTNESS i'm trying to read brightness value but i'm getting '0'. please check my follow up post with my original question.
Hi alejandrolozano,
i already did that i given my return value like this ov5640.brightness = ov5640_read_reg(0x5587,&value). when i'm reading the register the outcome is zero. i just want to read brightness value.