otg device mode issue for imx535 QSB ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

otg device mode issue for imx535 QSB ?

ソリューションへジャンプ
1,742件の閲覧回数
venkateshp
Contributor I

Hi,

    I was used IMx53 development kit and USB OTG DEVICE issue is their.How to configure OTG in device mode  and let me know the OTG Id pin is connected to External  5V or Ground,otherwise Otg id pin connecd to Both Ext 5V or Ground which one is DEVICE MOD.

thanks,

Venkat

ラベル(3)
0 件の賞賛
1 解決策
953件の閲覧回数
Henry_p
NXP Employee
NXP Employee

You don't need to connect ID pin to 5V or ground for device function. Just keep it floating.

You can find more details in USB On-The-Go - Wikipedia, the free encyclopedia

元の投稿で解決策を見る

0 件の賞賛
2 返答(返信)
953件の閲覧回数
venkatesh_pvsm
Contributor II

Hi ,

  Still Devcice mode was not detected in i.MX53 QSB Board, How to solve this issue.

Thanks By,

Venkat.

0 件の賞賛
954件の閲覧回数
Henry_p
NXP Employee
NXP Employee

You don't need to connect ID pin to 5V or ground for device function. Just keep it floating.

You can find more details in USB On-The-Go - Wikipedia, the free encyclopedia

0 件の賞賛