optee porting for imx6solo

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

optee porting for imx6solo

617 Views
hailiu
Contributor IV

dear exports,

I am porting optee to imx6solo processor, I have three questions here.

1. in imx6.h, there are the following code:

#if defined(CFG_MX6QP) || defined(CFG_MX6Q) || defined(CFG_MX6DL) || \
defined(CFG_MX6D)
#define TZASC2_BASE 0x21D4000
#define TZASC2_SIZE 0x4000
#endif

I see in the i.MX6solo/6duallite reference manual that there are two TZASCs, do I need to add the following line:

#elif defined(CFG_MX6S)
#define TRUSTZONE_OCRAM_START 0x918000

before the line #else to the following code?

#if defined(CFG_MX6QP) || defined(CFG_MX6Q) || defined(CFG_MX6DL) || \
defined(CFG_MX6D)||(CFG_MX6S) because there are two TZASCs?

2. For 6solo, there are only 128k OSCRAM,  do I need to modify the following code:

if defined(CFG_MX6UL) || defined(CFG_MX6ULL)
/* 128K OCRAM */
#define TRUSTZONE_OCRAM_START 0x918000
#elif defined(CFG_MX6DL)
#define TRUSTZONE_OCRAM_START 0x918000
#elif defined(CFG_MX6QP)
#define TRUSTZONE_OCRAM_START 0x938000
#elif defined(CFG_MX6SX)
#define TRUSTZONE_OCRAM_START 0x8f8000
#elif defined(CFG_MX6SL)
#define TRUSTZONE_OCRAM_START 0x918000
#elif defined(CFG_MX6SLL)
#define TRUSTZONE_OCRAM_START 0x918000
#else
/* 256K OCRAM */
#define TRUSTZONE_OCRAM_START 0x938000
#endif

3. in driver/tzc380.c, do I need to add ||IS_ENABLED(CFG_MX6S) to the following line?

if (IS_ENABLED(CFG_MX6Q) || IS_ENABLED(CFG_MX6D) ||
IS_ENABLED(CFG_MX6DL))

4. Do I need to add $(call force,CFG_TZC380,y) to the following code in conf.mk?

else ifneq (,$(filter $(PLATFORM_FLAVOR),$(mx6s-flavorlist)))
$(call force,CFG_MX6,y)
$(call force,CFG_MX6S,y)
$(call force,CFG_TEE_CORE_NB_CORE,1)

 

thank you all!

Hai

Tags (1)
0 Kudos
Reply
2 Replies

593 Views
hailiu
Contributor IV

I found the problem, when compiling OP-TEE, the first character in MACHINE is dropped. for an example,  imx6solosabresd is changed to mx6solosabresd. so to support the imx6solosabresd board, use mx6solosabresd instead of imx6solosabresd in conf.mk

0 Kudos
Reply

604 Views
igorpadykov
NXP Employee
NXP Employee

Hi Hai

 

one can look at   i.MX Porting Guide​   Chapter 5   Configuring OP-TEE

 

Best regards
igor

0 Kudos
Reply