nxp S32V232 emmc performance

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

nxp S32V232 emmc performance

966 Views
tom3
Contributor I


Hi, nxp

We find problems during product development and leave inquiries.
The ap I use is s32v232. This ap supports up to emmc 4.41.

In emmc ddr52 mode, the bus width max is known to be 104MB/s. But the results of our testing are as follows:

//////////////////////////////////////////////////////////////////////////////////////////////////////////////

/ # hdparm -t /dev/mmcblk0

/dev/mmcblk0:
Timing buffered disk reads: 85 MB in 3.03 seconds = 28715 kB/s
/ # [ 196.353005] random: crng init done

//////////////////////////////////////////////////////////////////////////////////////////////////////////////

/ # dd if=/testfile of=/dev/mmcblk0p3 bs=1M count=300
300+0 records in
300+0 records out
314572800 bytes (300.0MB) copied, 11.514134 seconds, 26.1MB/s
/ #

//////////////////////////////////////////////////////////////////////////////////////////////////////////////

As above, the read/write performance of emmc is only 26~28MB.

I don't think this is a matter of emmc performance. Because, emmc supports 280MB to read in hs400 mode.

So we are thinking that there is a problem with the AP's emmc controller.

I don't know how to attach the photo, so I leave a link.
In the link, I captured the waveform of emmc.

Red    : cmd
Yellow: clock
Blue   : data0

If you look closely at the clock part, you can see that it operates at 52mhz and then at a slower speed. This occurs periodically, and an interver occurs every two clocks.

The reason for the slow read/write performance is a situation where there is a suspected problem with the clock control.
Please review whether there is a problem with the waveform.
And what should we expect of emmc's max performance in s32v232 ap?

 

0 Kudos
Reply
0 Replies