hi, everyone
I have a sabresd i.MX6 board.
But it isn't work on NFS.
I attach uboot env and boot log.
How can I fix this error?
Sending DHCP requests ., OK
IP-Config: Got DHCP answer from 0.0.0.0, my address is 192.168.0.65
IP-Config: Complete:
device=eth0, addr=192.168.0.65, mask=255.255.255.0, gw=192.168.0.1,
host=192.168.0.65, domain=, nis-domain=(none),
bootserver=0.0.0.0, rootserver=0.0.0.0, rootpath=
VFS: Cannot open root device "nfs" or unknown-block(0,255)
Please append a correct "root=" boot option; here are the available partitions:
1f00 1024 mtdblock0 (driver?)
1f01 3072 mtdblock1 (driver?)
b300 7757824 mmcblk0 driver: mmcblk
b301 7747584 mmcblk0p1 00000000-0000-0000-0000-000000000000
b310 2048 mmcblk0boot1 (driver?)
b308 2048 mmcblk0boot0 (driver?)
Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(0,255)
...
Original Attachment has been moved to: uboot_env.txt.zip
Original Attachment has been moved to: boot_log.txt.zip
解決済! 解決策の投稿を見る。
Add rootwait to bootargs_nfs and it should be OK (if NFS server is set up properly).
how to add rootwait
U-Boot > setenv bootargs_nfs ‘setenv bootargs ${bootargs} root=/dev/nfs
ip=dhcp nfsroot=${serverip}:${nfsroot} fec_mac=00:04:9F:00:EA:D7’
to this...
thanks Vladan,
I sovled it add NFS server features at LTIB Setting.