mx6u linux-4.1.15 RS485驱动

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

mx6u linux-4.1.15 RS485驱动

2,292 Views
小辉哥
Contributor III

imx6u linux4.1.15 RS485驱动,我使用uart3接一个485收发器MC34901,这个方向控制RS485EN是使用UART3_RTS_B,pastedImage_0.png

dts我也做了修改:

pastedImage_1.png

但是重新烧写后,不能正常工作?请给我点建议。

Labels (3)
0 Kudos
Reply
3 Replies

1,717 Views
igorpadykov
NXP Employee
NXP Employee

Hi

please look at

IMX6u rs485驱动

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,717 Views
小辉哥
Contributor III

Hi igor,

那个链接也是我发的提问,我可能发了两次这个提问,没有答案呀。

0 Kudos
Reply

977 Views
adamhuang
Contributor III

**bleep**, embarrassed!

0 Kudos
Reply