platform: mx6d , uboot-2015-04-r0
rmii + lan8720a (The sch is OK, because rmii (lan8720a) in linux3.14.52 is ok)
List what I have done .
mx6sabresd.c
1,PINs config
static iomux_v3_cfg_t const enet_pads[] = {
MX6_PAD_ENET_MDIO__ENET_MDIO | MUX_PAD_CTRL(ENET_PAD_CTRL),
MX6_PAD_ENET_MDC__ENET_MDC | MUX_PAD_CTRL(ENET_PAD_CTRL),
MX6_PAD_ENET_CRS_DV__ENET_RX_EN | MUX_PAD_CTRL(ENET_PAD_CTRL),
MX6_PAD_ENET_RX_ER__ENET_RX_ER | MUX_PAD_CTRL(ENET_PAD_CTRL),
MX6_PAD_ENET_TX_EN__ENET_TX_EN | MUX_PAD_CTRL(ENET_PAD_CTRL),
MX6_PAD_ENET_RXD0__ENET_RX_DATA0 | MUX_PAD_CTRL(ENET_PAD_CTRL),
MX6_PAD_ENET_RXD1__ENET_RX_DATA1 | MUX_PAD_CTRL(ENET_PAD_CTRL),
MX6_PAD_ENET_TXD0__ENET_TX_DATA0 | MUX_PAD_CTRL(ENET_PAD_CTRL),
MX6_PAD_ENET_TXD1__ENET_TX_DATA1 | MUX_PAD_CTRL(ENET_PAD_CTRL),
MX6_PAD_GPIO_16__ENET_REF_CLK | MUX_PAD_CTRL(ENET_PAD_CTRL),
MX6_PAD_EIM_D21__GPIO3_IO21 | MUX_PAD_CTRL(NO_PAD_CTRL),
};
2,PIN IOMUX and PHY reset
static void setup_iomux_enet(void)
{
imx_iomux_v3_setup_multiple_pads(enet_pads, ARRAY_SIZE(enet_pads));
// Reset lan8720 PHY
gpio_direction_output(IMX_GPIO_NR(3, 21) , 1);
udelay(150);
gpio_set_value(IMX_GPIO_NR(3, 21), 0);
udelay(200);
gpio_set_value(IMX_GPIO_NR(3, 21), 1);
udelay(100);
}
3,clk 50MHz , and run it in board_init()
static int setup_fec(void)
{
struct iomuxc_base_regs *iomuxc_regs =
(struct iomuxc_base_regs *)IOMUXC_BASE_ADDR;
int ret;
/* set gpr1[21] to select anatop clock */
clrsetbits_le32(&iomuxc_regs->gpr[1], IOMUXC_GPR1_ENET_CLK_SEL_MASK, 1
<< 21);
ret = enable_fec_anatop_clock(0, ENET_50MHZ);
if (ret)
return ret;
return 0;
}
mx6sabre-common.h
4,RMII CONFIGs
#define CONFIG_CMD_PING
#define CONFIG_CMD_DHCP
#define CONFIG_CMD_MII
#define CONFIG_CMD_NET
#define CONFIG_FEC_MXC
#define CONFIG_MII
#define IMX_FEC_BASE ENET_BASE_ADDR
#define CONFIG_FEC_XCV_TYPE RMII
#define CONFIG_ETHPRIME "FEC"
#define CONFIG_FEC_MXC_PHYADDR 0
#define CONFIG_PHYLIB
#define CONFIG_PHY_SMSC
5,now ,what we got
a , clk 50MHz is OK ,we can test it .
b, log as below: (ip is the same 192.168.0.x )
U-Boot 2015.04-imx_v2015.04_3.14.52_1.1.0_ga+g6cf684a (May 10 2016 - 16:42:24)
CPU: Freescale i.MX6D rev1.2 at 792 MHz
CPU: Temperature 36 C
Reset cause: POR
Board: MX6-SabreSD
I2C: ready
DRAM: 1 GiB
MMC: FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2
No panel detected: default to Hannstar-XGA
Display: Hannstar-XGA (1024x768)
In: serial
Out: serial
Err: serial
switch to partitions #0, OK
mmc2(part 0) is current device
Net: FEC [PRIME]
Normal Boot
Hit any key to stop autoboot: 0
=>
=>
=> ping 192.168.0.1
Using FEC device
error frame: 0x4ef46dc0 0x00000804
error frame: 0x4ef47400 0x00000804
error frame: 0x4ef47a40 0x00000804
error frame: 0x4f24ba40 0x00000884
error frame: 0x4f24c080 0x00000804
ARP Retry count exceeded; starting again
error frame: 0x4ef46dc0 0x00000804
error frame: 0x4ef47400 0x00000804
error frame: 0x4ef47a40 0x00000804
error frame: 0x4f24ba40 0x00000804
error frame: 0x4f24c080 0x00000884
ARP Retry count exceeded; starting again
we found the same problem :
http://bbs.21ic.com/icview-727812-1-1.html
It really have a patch about rmii of uboot ?
WHO CAN help me ?@BiyongSUN
Hi,
in the attachment a patch for our board with the processor i.MX6 DUAL, PHY lan8720a, u-boot release 4.1.15_1.1.0_ga (U-Boot 2015.04), only minimum necessary is enabled.
U-Boot 2015.04 (May 17 2016 - 12:32:03)
CPU: Freescale i.MX6D rev1.5 at 792 MHz
CPU: Temperature 35 C
Reset cause: POR
Board: SK-iMX6-SODIMM
DRAM: 1 GiB
MMC: FSL_SDHC: 0, FSL_SDHC: 1
*** Warning - bad CRC, using default environment
Net: FEC
Normal Boot
Hit any key to stop autoboot: 0
u-boot > printenv ipaddr
ipaddr=192.168.0.136
u-boot > printenv ethaddr
ethaddr=00:1f:f2:00:00:00
u-boot > ping 192.168.0.2
Using FEC device
host 192.168.0.2 is alive
I haven't noticed - the ping works without problems, but problems appear when using tftp
u-boot > tftp zImage
Using FEC device
TFTP from server 192.168.0.2; our IP address is 192.168.0.136
Filename 'zImage'.
Load address: 0x12000000
Loading: #################################################################
###########################error frame: 0x4f58d5c0 0x00000804
######################################
################################error frame: 0x4f58c300 0x00000804
###error frame: 0x4f597840 0x00000804
##############################
#################################################################
#################################################################
#################################################################
##############error frame: 0x4f587e40 0x00000804
###################################################
############error frame: 0x4f583c80 0x00000804
##################################error frame: 0x4f58d5c0 0x00000804
###error frame: 0x4f59aa40 0x00000804
######error frame: 0x4f597e80 0x00000804
##########
##########################error frame: 0x4f591440 0x00000804
###############error frame: 0x4f599140 0x00000804
Hi li chao,
we don't use mx6sabresd, the board-file is in the enclosed patch
possibly you are interested in initialization of ethernet there
#define ENET_PAD_CTRL (PAD_CTL_PUS_100K_UP | PAD_CTL_SPEED_MED | \
PAD_CTL_DSE_40ohm | PAD_CTL_HYS)
#define ETH_PHY_RESET | IMX_GPIO_NR(1, 23) |
#ifdef CONFIG_FEC_MXC
static iomux_v3_cfg_t const enet_pads[] = {
MX6_PAD_GPIO_16__ENET_REF_CLK | MUX_PAD_CTRL(ENET_PAD_CTRL),
MX6_PAD_ENET_MDIO__ENET_MDIO | MUX_PAD_CTRL(ENET_PAD_CTRL),
MX6_PAD_ENET_MDC__ENET_MDC | MUX_PAD_CTRL(ENET_PAD_CTRL),
MX6_PAD_ENET_CRS_DV__ENET_RX_EN | MUX_PAD_CTRL(ENET_PAD_CTRL),
MX6_PAD_ENET_RX_ER__ENET_RX_ER | MUX_PAD_CTRL(ENET_PAD_CTRL),
MX6_PAD_ENET_TX_EN__ENET_TX_EN | MUX_PAD_CTRL(ENET_PAD_CTRL),
MX6_PAD_ENET_RXD0__ENET_RX_DATA0 | MUX_PAD_CTRL(ENET_PAD_CTRL),
MX6_PAD_ENET_RXD1__ENET_RX_DATA1 | MUX_PAD_CTRL(ENET_PAD_CTRL),
MX6_PAD_ENET_TXD0__ENET_TX_DATA0 | MUX_PAD_CTRL(ENET_PAD_CTRL),
MX6_PAD_ENET_TXD1__ENET_TX_DATA1 | MUX_PAD_CTRL(ENET_PAD_CTRL),
/* PHY Reset */
MX6_PAD_ENET_REF_CLK__GPIO1_IO23 | MUX_PAD_CTRL(NO_PAD_CTRL),
};
static void setup_iomux_enet(void)
{
imx_iomux_v3_setup_multiple_pads(enet_pads, ARRAY_SIZE(enet_pads));
/* Reset PHY */
gpio_direction_output(ETH_PHY_RESET, 0);
udelay(500);
gpio_set_value(ETH_PHY_RESET, 1);
}
int board_eth_init(bd_t *bis)
{
int ret = 0;
struct iomuxc *const iomuxc_regs = (struct iomuxc *)IOMUXC_BASE_ADDR;
ret = enable_fec_anatop_clock(0, ENET_50MHZ);
if (ret)
return ret;
/* set gpr1[ENET_CLK_SEL] */
setbits_le32(&iomuxc_regs->gpr[1], IOMUXC_GPR1_ENET_CLK_SEL_MASK);
setup_iomux_enet();
ret = cpu_eth_init(bis);
if (ret)
printf("FEC MXC: %s:failed\n", __func__);
return ret;
}
#endif /* CONFIG_FEC_MXC */
Hi,
I needed to add a special setup just after reset.
In phy_reset() I added a soft reset MODE[2:0] = 111
phy_write(phydev, devad, MII_DCOUNTER, 0x60E1
--
Marco Cavallini | KOAN sas | Bergamo - Italia
embedded and real-time software engineering
Thanks!
I think mac address is OK !
=> pri ethaddr
ethaddr=FA:E8:79:7A:B4:B8
it is the same mac in linux , rmii is ok in linux.
=> pri ipaddr
ipaddr=192.168.0.171
=> pri gw_ip
gw_ip=192.168.0.1
=> pri netmask
netmask=255.255.255.0