Hi,
I have an eclipse project which I'm building for x86 and for i.mx53 .
The code is loading firmware through the UART2 or UART3 at 115200 bps to a modem chip and and making alive checks (custom board) .
The code works for x86 and fails for mx53 .
I observed the uart Tx pins with a port monitor SW and realised that some piece of the sent packet is missing or repeated .
I thought its an alignment problem but the sendbuffer is aligned to four bytes :
} __attribute__((aligned(4),packed)) str_fwbuf;
Any comment?
yektaayduk,
.....did you ever get Rx working on UART2 and 3? If so can you point the way! :smileyhappy:
I applied "ENGR00252150 Fix MX53 IOMUX setup for all UARTs" . Uarts are working now.
Below is the link of the engineering patch:
Thanks. I had stumbled across the incorrect iomux definitions a few weeks ago. .didn't think it useful to post "found it!".
Greatly appreciate your follow through though - THANKS anyway!
Uart-2 and Uart-3 Tx Rx are OK.
I applied "ENGR00252150 Fix MX53 IOMUX setup for all UARTs" patch .
Settings in serial.h :
UART2_UCR4_CTSTL 16
UART2_DMA_ENABLE 0
UART3_UCR4_CTSTL 16
UART3_DMA_ENABLE 0
Which board are you using? Which BSP are you using?
Thank you jimmychan
İts a custom board , BSP version is L2.6.35_11.09.01 .
We have found that the problem is somewhere else :
The port monitor I was using is somehow effected from the activation order of boards. When I first activate CPU board then reset the modem board and then activate the port monitor there are no missing bytes at the beginning .
So I think mx53 has no missing bytes problem.
But if so why is the modem not receiving 8K firmware bytes and replay to alive checks?
Our CPU board was controlling the modem boards . We saw that an fpga which is not implemented fully yet was helding the modem in a reset state so that modem doesnt replay.Now FPGA has inactivated the reset line by default and we are observing uart data from modem with the oscilloscope.
We have still a problem:
Now the modem replay should be received by mx53 UART ,but it doesnt get anything within the timeout window .
I'm using UART2 and UART3 for modem communications.The same project when compiled with x86 and run on PC works without any problem.
QUESTIONS :
In /linux/arch/arm/mx5/serial.h all the uarts are configured differently.DMA is enabled for some for some not ,some of them are using interrupts some of them not. I dont have use the CTS ,RTS pins so from the flow control viewUART2_UCR4_CTSTL -1 should be correct .
Are these default values and changed somewhere else according to the board configuration or should we change them only in serial.h if we want en- disable dma ,irq ?
How can I enable the receive part of UART2 or UART3 ( I have to check that the replay coming from modem reaches to UART2 receive pin ,still ).
Should I apply the changes mentioned in forum MX53 UART2(3) not working at Oct 28, 2011 ?
Should I use the imx_2.6.35_maintain BSP ? How to get the patches to upgrade my BSP to imx_2.6.35_maintain BSP?
Please try MX53 UART2(3) not working first.
Hi,
MX53 UART2(3) not working is irrelevant for my case because my pins for uart-2 & -3 are as below:
#define _MX53_PAD_PATA_DMARQ__UART2_TXD_MUX | IOMUX_PAD(0x5F8, 0x278, 3, 0x0, 0, 0) |
#define _MX53_PAD_PATA_BUFFER_EN__UART2_RXD_MUX IOMUX_PAD(0x5FC, 0x27C, 3, 0x880, 3, 0)
#define _MX53_PAD_PATA_CS_1__UART3_RXD_MUX | IOMUX_PAD(0x620, 0x2A0, 4, 0x888, 3, 0) |
#define _MX53_PAD_PATA_CS_0__UART3_TXD_MUX | IOMUX_PAD(0x61C, 0x29C, 4, 0x0, 0, 0) |
These settings are also used in mx53_ard.c and mx53_smd.c (for uart2) ,in mx53_ard.c for uart3 .
Did anybody having these boards successfully use the uart2 uart3 ?
ttymxc1 ,ttymxc2,ttymxc3,ttymxc4 seems to receive data with the test code.
I think this is an internal loopback without driving the device pins.
So its a kind of IOMUX problem?
root@freescale /unit_tests$ ./mxc_uart_test.out /dev/ttymxc1
Test: MXC UART!
Usage: mxc_uart_test <UART device name, opens UART2 if no dev name is specified>
/dev/ttymxc1 opened
Attributes set
Test: IOCTL Set
Data Written= Test
Data Read back= Test
root@freescale /unit_tests$ ./mxc_uart_test.out /dev/ttymxc2
Test: MXC UART!
Usage: mxc_uart_test <UART device name, opens UART2 if no dev name is specified>
/dev/ttymxc2 opened
Attributes set
Test: IOCTL Set
Data Written= Test
Data Read back= Test
root@freescale /unit_tests$ ./mxc_uart_test.out /dev/ttymxc3
Test: MXC UART!
Usage: mxc_uart_test <UART device name, opens UART2 if no dev name is specified>
/dev/ttymxc3 opened
Attributes set
Test: IOCTL Set
Data Written= Test
Data Read back= Test
root@freescale /unit_tests$ ./mxc_uart_test.out /dev/ttymxc4
Test: MXC UART!
Usage: mxc_uart_test <UART device name, opens UART2 if no dev name is specified>
/dev/ttymxc4 opened
Attributes set
Test: IOCTL Set
Data Written= Test
Data Read back= Test
root@freescale /unit_tests$
Check to see if you have the Daisy Chain setting correct for the UART RXD:
IOMUXC_UART3_IPP_UART_RXD_MUX_SELECT_INPUT
This setting tells the IOMUX which pin to use for RXD.
Brett