mmc1: Timeout waiting for hardware interrupt

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

mmc1: Timeout waiting for hardware interrupt

2,744 Views
lvguangzhao
Contributor I

Our product develop is base on I.MX6 SOLOLITE+ BSP L3.0.35_4.1.0, I have a wifi module bcm43241, connect to slot sd2, sdio sometimes occur "mmc1:Timeout waiting for hardware interrupt" when in process of "mmc_add_host", reboot 100 times happen about 2 times,After track mmc driver, we found that there is no irq generate when host prepare sending command, we have tried cut down the sdio interface in wifi module side, problem still happen, only adjust the boot sequence of sdio and mipi lcm can fix this issue, which means let sdio init first , lcm init later, So anyone can help explain why?

pastedImage_1.png

0 Kudos
1 Reply

1,043 Views
igorpadykov
NXP Employee
NXP Employee

Hi lv

bcm43241 is not supported on official L3.0.35_4.1.0, may be recommended to apply

to vendor support for updated driver for that kernel version.

http://wireless.murata.com/eng/products/rf-modules-1/wi-fi-bluetooth-for-freescale-i-mx.html

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos