mipi csi-2 port not capturing cvbs video

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

mipi csi-2 port not capturing cvbs video

1,254件の閲覧回数
efecan_icoz
Contributor III

Hi all,

 

I'm using NVP6324 for converting analog video to mipi csi-2. So far i could manage to use it with my imx8mm board with only 1 channel active at 1080p and 720p resolutions. But i couldn't manage to start streaming with neither PAL nor NTSC. Interesting part is when i call gstreamer command nothing happens in screen, and no error messages in console of gstreamer.

 

Is there any ways to debug this issue to find the point of the problem ?

 

As driver I'm using slightly modified version of this post , and for mipi driver I'm using mxc_mipi_csi.

gst command:

 

gst-launch-1.0 v4l2src device="/dev/video0" ! "video/x-raw, format=(string)UYVY, width=(int)720, height=(int)480, framerate=(fraction)30/1" ! imxvideoconvert_g2d ! waylandsink

 

 

 

With GST_DEBUG=4 last messages I get pasted below; looks like v4l2src is streaming

0:00:00.085103883  2293      0xfbc3a00 INFO              GST_STATES gstbin.c:2503:gst_bin_element_set_state:<waylandsink0> current READY pending PAUSED, desired next PLAYING
0:00:00.085132009  2293      0xfbc3a00 INFO              GST_STATES gstbin.c:2957:gst_bin_change_state_func:<pipeline0> child 'waylandsink0' is changing state asynchronously to PLAYING
0:00:00.085132384  2293      0xfc7d940 WARN              video-info video-info.c:521:gst_video_info_from_caps: invalid matrix 3 for RGB format, using RGB
0:00:00.085161384  2293      0xfbc3a00 INFO              GST_STATES gstbin.c:2503:gst_bin_element_set_state:<imxvideoconvert_g2d0> current PAUSED pending VOID_PENDING, desired next PLAYING
0:00:00.085198134  2293      0xfbc3a00 INFO              GST_STATES gstelement.c:2676:gst_element_continue_state:<imxvideoconvert_g2d0> completed state change to PLAYING
0:00:00.085215134  2293      0xfc7d940 INFO               GST_EVENT gstevent.c:820:gst_event_new_caps: creating caps event video/x-raw, width=(int)720, height=(int)576, framerate=(fraction)25/1, pixel-aspect-ratio=(fraction)1/1, colorimetry=(string)bt709, interlace-mode=(string)progressive, format=(string)BGRx
0:00:00.085222759  2293      0xfbc3a00 INFO              GST_STATES gstelement.c:2579:_priv_gst_element_state_changed:<imxvideoconvert_g2d0> notifying about state-changed PAUSED to PLAYING (VOID_PENDING pending)
0:00:00.085337260  2293      0xfbc3a00 INFO              GST_STATES gstbin.c:2951:gst_bin_change_state_func:<pipeline0> child 'imxvideoconvert_g2d0' changed state to 4(PLAYING) successfully
0:00:00.085368760  2293      0xfbc3a00 INFO              GST_STATES gstbin.c:2503:gst_bin_element_set_state:<capsfilter0> current PAUSED pending VOID_PENDING, desired next PLAYING
0:00:00.085394511  2293      0xfbc3a00 INFO              GST_STATES gstelement.c:2676:gst_element_continue_state:<capsfilter0> completed state change to PLAYING
0:00:00.085418261  2293      0xfbc3a00 INFO              GST_STATES gstelement.c:2579:_priv_gst_element_state_changed:<capsfilter0> notifying about state-changed PAUSED to PLAYING (VOID_PENDING pending)
0:00:00.085433261  2293      0xfc7d940 WARN              video-info video-info.c:521:gst_video_info_from_caps: invalid matrix 3 for RGB format, using RGB
0:00:00.085450636  2293      0xfbc3a00 INFO              GST_STATES gstbin.c:2951:gst_bin_change_state_func:<pipeline0> child 'capsfilter0' changed state to 4(PLAYING) successfully
0:00:00.085512761  2293      0xfbc3a00 INFO              GST_STATES gstelement.c:2676:gst_element_continue_state:<v4l2src0> completed state change to PLAYING
0:00:00.085536762  2293      0xfbc3a00 INFO              GST_STATES gstelement.c:2579:_priv_gst_element_state_changed:<v4l2src0> notifying about state-changed PAUSED to PLAYING (VOID_PENDING pending)
0:00:00.085568387  2293      0xfbc3a00 INFO              GST_STATES gstbin.c:2951:gst_bin_change_state_func:<pipeline0> child 'v4l2src0' changed state to 4(PLAYING) successfully
0:00:00.085742138  2293      0xfc7d940 WARN              video-info video-info.c:521:gst_video_info_from_caps: invalid matrix 3 for RGB format, using RGB
New clock: GstSystemClock
0:00:00.086054641  2293      0xfc7d940 WARN              video-info video-info.c:521:gst_video_info_from_caps: invalid matrix 3 for RGB format, using RGB
0:00:00.086338893  2293      0xfc7d940 WARN              video-info video-info.c:521:gst_video_info_from_caps: invalid matrix 3 for RGB format, using RGB
0:00:00.086385393  2293      0xfc7d940 WARN              video-info video-info.c:521:gst_video_info_from_caps: invalid matrix 3 for RGB format, using RGB
0:00:00.086478019  2293      0xfc7d940 WARN              video-info video-info.c:521:gst_video_info_from_caps: invalid matrix 3 for RGB format, using RGB
0:00:00.086603770  2293      0xfc7d940 WARN              video-info video-info.c:521:gst_video_info_from_caps: invalid matrix 3 for RGB format, using RGB
0:00:00.086650770  2293      0xfc7d940 WARN              video-info video-info.c:521:gst_video_info_from_caps: invalid matrix 3 for RGB format, using RGB
0:00:00.086716895  2293      0xfc7d940 WARN              video-info video-info.c:521:gst_video_info_from_caps: invalid matrix 3 for RGB format, using RGB
0:00:00.092291312  2293      0xfc7d940 INFO                    v4l2 gstv4l2object.c:3764:gst_v4l2_object_set_format_full:<v4l2src0:src> Set capture framerate to 25/1
0:00:00.096236091  2293      0xfc7d940 INFO                    v4l2 gstv4l2object.c:3031:gst_v4l2_object_setup_pool:<v4l2src0:src> accessing buffers via mode 4
0:00:00.108593558  2293      0xfc7d940 INFO          v4l2bufferpool gstv4l2bufferpool.c:557:gst_v4l2_buffer_pool_set_config:<v4l2src0:pool:src> increasing minimum buffers to 2
0:00:00.108660059  2293      0xfc7d940 INFO          v4l2bufferpool gstv4l2bufferpool.c:570:gst_v4l2_buffer_pool_set_config:<v4l2src0:pool:src> reducing maximum buffers to 32
0:00:00.108681184  2293      0xfc7d940 INFO          v4l2bufferpool gstv4l2bufferpool.c:581:gst_v4l2_buffer_pool_set_config:<v4l2src0:pool:src> can't allocate, setting maximum to minimum
0:00:00.108872935  2293      0xfc7d940 INFO          v4l2bufferpool gstv4l2bufferpool.c:570:gst_v4l2_buffer_pool_set_config:<v4l2src0:pool:src> reducing maximum buffers to 32
0:00:00.108897185  2293      0xfc7d940 INFO          v4l2bufferpool gstv4l2bufferpool.c:581:gst_v4l2_buffer_pool_set_config:<v4l2src0:pool:src> can't allocate, setting maximum to minimum
0 件の賞賛
返信
3 返答(返信)

922件の閲覧回数
SJZ
Contributor I

did you resolve this?
We have it working for PAL but not NTSC format...

0 件の賞賛
返信

1,240件の閲覧回数
efecan_icoz
Contributor III

Hi @igorpadykov,

Thanks for your help, I have already managed to capture 1080p and 720p streams over nvp6324 with mipi csi2. Now I'm trying to capture cvbs inputs too but as I've mentioned gstreamer doesn't shows anything (not even blackscreen).

That's why I'm thinking maybe the sent or expected pixel counts doesnt match at mipi level or something like that.

 

Edit 1: I'm thinking that what if NVP6324 sends cvbs video data interlaced. Would that broke anything ?

0 件の賞賛
返信

1,243件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi efecan_icoz

 

opposite to i.MX8QM on referenced link i.MX8M Mini

does not have ISI module and not support virtual channels.

In general one can reuse ov5640 driver, as it also uses YUV422 format as Nvp6324:

https://source.codeaurora.org/external/imx/linux-imx/tree/drivers/media/platform/mxc/capture/ov5640_...

 

gst command for 1080p @30 fps:
gst-launch-1.0 v4l2src device=/dev/video0 ! video/x-raw,width=1920,height=1080, framerate=30/1 ! waylandsink

 

camera unit test for debugging:

https://source.codeaurora.org/external/imx/imx-test/tree/test/mxc_v4l2_test/mx6s_v4l2_cap_drm.c?h=im...

 

Best regards
igor

0 件の賞賛
返信