minimum voltage of VDD_SNVS_IN

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

minimum voltage of VDD_SNVS_IN

1,816 次查看
yutaka_ando
NXP Employee
NXP Employee

According to the table 8 of i.MX6Solo/DualLite data sheet (MX6SDLCEC), the minimum of VDD_SNVS_IN is 2.9V

pastedImage_1.jpg

On the other hand, table 11 of this document defines the power consumption of SNVS mode at VDD_SNVS_IN = 2.8V which is 0.1V lower than the minimum voltage defined in table 8.

pastedImage_2.jpg

Does VDD_SNVS_IN support 2.8V?

标签 (1)
0 项奖励
回复
7 回复数

1,631 次查看
b36401
NXP Employee
NXP Employee

For correct operation table 8 is correct, the minimum setting is 2.9V.
This supply also generates the 1.1V on SNVS_CAP which is the logic supply for the 32KHZ OSC and other logic.
The 1.1V is generated from a resistor divider from SNVS_IN, so when it drops to 2.8V the 1.1V will drop below min voltage to operate this logic.

0 项奖励
回复

1,631 次查看
yuji_fuseki
Contributor II

Hi Mrudang,

Ok, I understood.

Power consumption also is increased.

Br,

Yuji

0 项奖励
回复

1,631 次查看
mrudangshelat1
Senior Contributor II

Hi Yuji,

2.8V is in error in the power consumption table. It should be 2.9V like in the operating conditions table.

Regards,

Mrudang

0 项奖励
回复

1,631 次查看
yuji_fuseki
Contributor II

Hi, Mrudang

>I guess you want to say why it is described as 2.9V instead of 2.8V in the datasheet, right?

yes, you're right.

Corrected question:「why minimum operating voltage is NOT described as 2.8V in the datasheet?」

Br,

Yuji

0 项奖励
回复

1,631 次查看
yuji_fuseki
Contributor II

Dear Mrudang

Sorry for jumping in.

>SNVS supply support 2.8V. 

if so, why minimum operating voltage is described as 2.8V in the datasheet?

Br,

Fuseki

0 项奖励
回复

1,631 次查看
mrudangshelat1
Senior Contributor II

Hi Yuji,

I guess you want to say why it is described as 2.9V instead of 2.8V in the datasheet, right?

Mrudang

0 项奖励
回复

1,631 次查看
mrudangshelat1
Senior Contributor II

Hi Yutaka,

Yes, SNVS supply support 2.8V. Please refer the Note#7.

#7: While setting VDD_SNVS_IN voltage with respect to Charging Currents and RTC, refer to Hardware Development Guide for i.MX 6Dual, 6Quad, 6Solo, 6DualLite Families of Applications Processors (IMX6DQ6SDLHDG).

Regards,

Mrudang

0 项奖励
回复