mfgtool2-yocto-mx8-evk-sdcard-sd2.vbs is missing?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

mfgtool2-yocto-mx8-evk-sdcard-sd2.vbs is missing?

1,281 Views
xianju_wang
Contributor I

I followed the instruction below to load linux system on the board. 

https://www.nxp.com/document/guide/get-started-with-the-mcimx8m-evk:GS-MCIMX8M-EVK

In step 2.3.1 Burn NXP Linux BSP image using Manufacturing Tool,  I couldnot find L4.9.88_2.0.0-ga_mfg-tools.tar.gz and I found L4.9.88_2.0.0-mfg-tools.tar.gz instead.  After unzipping it, I could not find mfgtool2-yocto-mx8-evk-sdcard-sd2.vbs .

Thanks.

Xianju 

Labels (2)
0 Kudos
Reply
1 Reply

1,145 Views
igorpadykov
NXP Employee
NXP Employee

Hi xianju

one can look at attached vbs file, note now mfg tool is replaced by uuu tool

https://github.com/NXPmicro/mfgtools

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------