mfg u-boot.imx for imx6q som - Yocto

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

mfg u-boot.imx for imx6q som - Yocto

868件の閲覧回数
tuyennguyen
Contributor I

I have a custom board based on Sabresd. Everything runs smoothly when we boot it from SD card with new firmware.

However we are trying to flash it into NAND using manufacturing tool (MFG), we make a custom recipe called linux-imx-mfgtool_3.14.38.bb  for our board and then bitbake fsl-image-mfgtool-initramfs. The build finished successfully but there is no u-boot.imx which is required by MFG tool. Please advice me how to generate this u-boot.imx. I am sorry I am new in this Yocto project.

Thanks a lot.

ラベル(1)
0 件の賞賛
1 返信

549件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Carrie

please look at attached i.MX6 BSP Porting Guide sect.1.2.1 Preparing the Code

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛