mfg tool failed for android 4.4.3.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

mfg tool failed for android 4.4.3.

1,425件の閲覧回数
thangameenaraje
Contributor II

Hi, everyone,

I am working in sololite platform  custom board.

now i downloaded kitkat 4.4.3  it has kernel 3.10.17. i want to flash  emmc .

first i tried with my sololite evk.

in evk there is no emmc so for sdcard  .

1. downloaded mfg tool for 4.4.3.

2. given list name cfg.ini as  SDCard-Android-IMX6SL-EVK.    , mmc=0,1(tried both)

3. using sd2 slot inserted sd card. changed download mode.

4. added img files under android/evk/<.img>

5. executed exe. found hid device

6. its running but failed at partitioning.

7. error as fdisk not regognized.

i read the android firmware document. in that the given document is same as like for 4.4.2 mfg tool. in this 4.4.3 the kernel is in device tree format. there are more changes in bsp.

there is no file to compile ram uboot and ram kernel

under uboot/ include/configs/< mx6sl_evk_mfg.h>

kernel/arch/arm/configs/ imx6_updater_defconfig

to compile ram uboot and ram kernel

kindly help me in this issue


ラベル(1)
0 件の賞賛
返信
1 返信

1,211件の閲覧回数
saurabh206
Senior Contributor III

Hi

Have you change  the Boot mode switch for firmware update?

You should change "Boot Mode" switch.

Thanks

Saurabh

0 件の賞賛
返信