memtool for i.MX8qm processor

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

memtool for i.MX8qm processor

4,637 Views
威王
Contributor II

Hi,

 

I want memtool for i.MX8QM processor.

How can I get updated memtool code for i.MX8QM processor.

 

Thanks

Wison

0 Kudos
Reply
5 Replies

4,521 Views
威王
Contributor II

mek_8q:/ # uname -r
4.14.98-gfaef852-dirty

0 Kudos
Reply

4,521 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

You can try to refer to thishttps://community.nxp.com/message/628563 

0 Kudos
Reply

4,521 Views
威王
Contributor II

the reference only for imx6 imx7 imx8m,not apply to imx8q;do you have special memtool for imx8q? thanks

0 Kudos
Reply

4,521 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

The method is most the same.

At the following link:  [meta-freescale] [PATCH v2 42/43] imx-test: Add i.MX 8 support 

we see that the imx8 should be added.

-----

this is very vague statement as " imx8" comprises dozen very different family processors

i.MX 8 Series Applications Processors | Arm® Cortex®-A72/A53/A35/M4 cores | NXP 

Based on latest memtool sources only i.MX8MQ family is supported

memtool\test - imx-test - i.MX Driver Test Application Software 

0 Kudos
Reply

4,521 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Which version of BSP are you using?

0 Kudos
Reply