Dear NXP,
There is a compatibility problem with the latest versions of Windows
on MCUXpresso if you debug then
"cannot run program wmic createprocess error=2"
I found the cause is because wmic.exe is missing
"Windows Management Instrumentation Command line (WMIC) tool: The WMIC tool is deprecated in Windows 10, version 21H1 and the 21H1 semi-annual channel release of Windows Server. This tool is superseded by Windows PowerShell for WMI. Note: This deprecation only applies to the command-line management tool. WMI itself is not affected."
Temporary Workaround:
Luckily I still have a "Windows.old" folder
I added this to my PATH
C:\Windows.old\WINDOWS\System32\wbem
Regards.
Lee.
I tried, but i cant. How can i add the path.
thank you
I am having a similar problem MCUXpresso IDE v11.4.1 [Build 6260] [2021-09-15]1050 evbk board
Hi @anthonygarza
Hoping you are excellent.
May you confirm which Windows version are you using too?
Regards.
Pablo Avalos.
I was able to make mine go away by adding the following to my path.
C:\Windows\System32\wbem
Including a copy of the error from mcuxpresso. I just installed it and tried to run the first example.
Hello @neo2
Hoping you are well.
I just wanted to let you know that we forwarded your report and we are checking it internally.
Many thanks for letting us know.
Sincerely,
Pablo Avalos.
Hi
In order to check your issue correctly, please let us know your chip PN and IDE version, thus we can assign right engineer for your issue.
Thanks,
Jun Zhang
I'm the using
- MIMXRT1160-EVK Board
- MCUXpresso IDE v11.4.1 [Build 6260] [2021-09-15]