machine name for imx6 dual wandboard in fsl-release-bsp 3.14 kernel?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

machine name for imx6 dual wandboard in fsl-release-bsp 3.14 kernel?

788件の閲覧回数
gbiradar
Contributor IV

Hi Guy

I'm using wandboard iMX6Dual development board, i have git repository i'm following freescale project user guide, Rev 0, 12/2015.

In section 5.1 Build configurations,

i have build yocto setup against imx6d machine but as i see in meta-fsl-arm/conf/machine i don't see imx6dual but rather solo/duallite/quad.

i need to know which machine configuration i can use for my project.

regards,

Ganesh

ラベル(3)
タグ(2)
0 件の賞賛
1 返信

580件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Ganesh

nxp linux documentation describes nxp reference boards, board

vendors may customize own bsps according to own boards configurations,

please follow wandboard guidelines:

Getting started with Yocto on Wandboard - Wandboard Wiki 

below common description of other vendors board support

difference between Yocto Community BSP and Free... | NXP Community 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛