Hi
While working with custom moard based on imx6s processor and linux-imx rel_imx_3.14.28_1.0.0_ga based kernel, I noticed this in dmesg:
[ 1.331535] galcore: clk_get vg clock failed, disable vg!
This is caused by setting in arch/arm/boot/dts/imx6dl.dtsi:
gpu@00130000 {
...
clocks = <&clks IMX6QDL_CLK_OPENVG_AXI>, <&clks IMX6QDL_CLK_GPU3D_AXI>,
<&clks IMX6QDL_CLK_GPU2D_CORE>, <&clks IMX6QDL_CLK_GPU3D_CORE>,
<&clks IMX6QDL_CLK_DUMMY>;
clock-names = "gpu2d_axi_clk", "gpu3d_axi_clk",
"gpu2d_clk", "gpu3d_clk",
"gpu3d_shader_clk";
...
};
This has two items that look wrong:
- "openvg_axi_clk" is missing in clock-names, thus the error message,
- "gpu2d_axi_clk" in clock-names refers to IMX6QDL_CLK_OPENVG_AXI, not to IMX6QDL_CLK_GPU2D_AXI
Symmetric settng in arch/arm/boot/dts/imx6q.dtsi does not have these issues.
Could someone please comment on this and suggest correct setting for imx6dl.dtsi ?
Hello,
How the system was built ?
For X11, please refer to Chapter 18 (X Windows Acceleration) of
“i.MX_Linux_Reference_Manual.pdf”.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
I'm developing BSP for a custom imx6 based board and thus write recipes myself.
Or - sometimes - build kernel without any recipes, directly from git tree.
I don't see a fix for this mismatch anywhere in linux-imx or linux-fslc or linux-boundary or other kernel trees referenced from recipes in meta-fsl-arm and meta-fsl-arm-extra.
Perhaps this mismatch does not lead to something not working and thus people ignore it.
But it is still incorrect and better to fix it.