lib32-imx-gpu-viv doesn't give 32bit GPU binaries for imx8mq platform

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

lib32-imx-gpu-viv doesn't give 32bit GPU binaries for imx8mq platform

1,304 Views
moorthy_baskara
Contributor I

I tried building 32bit components on 64bit imx8mq platform as it supports imx8 multilib with linux-imx 4.14 beta version (copied manually from imx_4.14.62_1.0.0_beta to meta-freescale master branch). When multilib is enabled and tried to build a component which uses i.mx8 gpu binaries, again it fetches the prebuilt bin file which is used for aarch64 (https://www.nxp.com/lgfiles/NMG/MAD/YOCTO/imx-gpu-viv-6.2.4.p2.1-aarch64.bin) where no 32bit binaries are available (only 64bit binaries present). On this, there is a do_package_qa error I faced. Then I manually edited the SRC_URI to point 32bit recipe (6.2.4.p2.1-aarch32) and I got below error saying that there is no gbm support

install: cannot stat '.../build/tmp-rpb_wayland-glibc/work/armv7at2hf-neon-mx8m-linaromllib32-linux-gnueabi/lib32-imx-gpu-viv/1_6.2.4.p2.1-aarch32-r0/imx-gpu-viv-6.2.4.p2.1-aarch32/gpu-core/usr/lib/pkgconfig/gbm.pc': No such file or directory

ERROR: Task (virtual:multilib:lib32:.../build/conf/../../layers/meta-freescale/recipes-graphics/imx-gpu-viv/imx-gpu-viv_6.2.4.p2.1-aarch32.bb:do_install) failed with exit code '1

Please confirm that multilib support only in linux-imx 4.14 beta and instruct how to use multilib for GPU binaries in imx8m platform.

0 Kudos
3 Replies

452 Views
sklaasboer
Contributor I

Hi,

Is this already solved, or did you found an workaround? I am facing the same problem.

0 Kudos

1,020 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi Moorthy,

You need an entire 32 bit rootfs. Maybe via Professional Services can do that.  Suggest to proceed with Professional Services to develop custom driver for this part

NXP Professional Services|NXP 

 

Regards

0 Kudos

1,020 Views
moorthy_baskara
Contributor I

Hi,

I don't require an entire 32bit rootfs whereas I'm building 32 bit GPU binaries using multilib support on 64bit (i.MX 8MQ EVK) machine. So, I just need to add these 32 bit components on 64 bit rootfs through IMAGE_INSTALL as given below

IMAGE_INSTALL_append = " lib32-imx-gpu-viv"

This is what I tried, but I faced above error.

0 Kudos