Hi All,
I am trying to use the usb modem to my board, i can able to do usb_mode switch to convert from CD-ROM to modem.
LOG for this
I connected modem to usb host :
usb 1-1: new high speed USB device number 2 using fsl-ehci
usb 1-1: New USB device found, idVendor=1bbb, idProduct=f000
usb 1-1: New USB device strings: Mfr=1, Product=2, SerialNumber=3
usb 1-1: Product: MobileBroadBand
usb 1-1: Manufacturer: Alcatel
usb 1-1: SerialNumber: 0123456789ABCDEF
Convertion using usb_modeswicth:
usb_modeswitch -v 0x1bbb -p 0xf000 -V 0x1bbb -P 0x0017 -M "55534243123456788000000080000606f50402527000000000000000000000"
Looking for target devices ...
No devices in target mode or class found
Looking for default dusb 1-1: usbfs: process 2226 (usb_modeswitch) did not claim interface 0 before use
evices ...
Found devices in default mode, class or configuration (1)
Accessing device 002 on bus 001 ...
Getting the current device configuration ...
OK, got current device configuration (1)
Using endpoints 0x01 (out) and 0x81 (in)
Inquiring device details; driver will be detached ...
Looking for active driver ...
No driver found. Either detached before or never attached
SCSI inquiry data (for identification)
-------------------------
Vendor String: ONETOUCH
Model String: KINGFISHER
Revision String: 2.31
-------------------------
USB description data (for identification)
-------------------------
Manufacturer: Alcatel
Product: MobileBroadBand
Serial No.: 0123456789ABCDEF
-------------------------
Setting up communication with interface 0
Using endpoint 0x01 for message sending ...
Trying to send message 1 to endpoint 0x01 ...
OK, message successfully sent
Resetting response endpoint 0x81
Resetting message endpoint 0x01
usb 1-1: USB disconnect, device number 2
Device is gone, skipping any further commands
-> Run lsusb to note any changes. Bye.
root@(none) ~$ usb 1-1: new high speed USB device number 3 using fsl-ehci
usb 1-1: New USB device found, idVendor=1bbb, idProduct=0195
usb 1-1: New USB device strings: Mfr=1, Product=2, SerialNumber=3
usb 1-1: Product: MobileBroadBand
usb 1-1: Manufacturer: Alcatel
usb 1-1: SerialNumber: 0123456789ABCDE
Now i am inserting the modules :
insmod usbnet.ko
insmod usb-storage.ko
insmod cdc_ether.ko
insmod rndis_host.ko
insmod usbserial.ko
Log is here:
insmod usbnet.ko
root@(none) /home$ insmod usb-storage.ko
Initializing USB Mass Storage driver...
scsi0 : usb-storage 1-1:1.2
usbcore: registered new interface driver usb-storage
USB Mass Storage support registered.
root@(none) /home$ scsi 0:0:0:0: Direct-Access ONETOUCH KINGFISHER 2.31 PQ: 0 ANSI: 2
scsi 0:0:0:0: Attached scsi generic sg0 type 0
insmod cdc_ether.ko
usbcore: registered new interface driver cdc_ether
root@(none) /home$ insmod rndis_host.ko
rndis_host 1-1:1.0: eth0: register 'rndis_host' at usb-fsl-ehci.0-1, RNDIS device, 08:2e:5f:29:0e:69
usbcore: registered new interface driver rndis_host
root@(none) /home$ insmod usbserial.ko
usbcore: registered new interface driver usbserial
USB Serial support registered for generic
usbcore: registered new interface driver usbserial_generic
usbserial: USB Serial Driver core
Now if i give ifconfig :
root@(none) /home$ ifconfig -a
eth0 Link encap:Ethernet HWaddr 08:2E:5F:29:0E:69
BROADCAST MULTICAST MTU:1500 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
lo Link encap:Local Loopback
LOOPBACK MTU:16436 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:0
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
How we can establish the connection?
In my PC(kernel version -3.2.0-91-generic-pae ) i tried it by disabling automatic usb_modeswitch in usb_modeswitch.conf file in /etc folder.
i did
sudo usb_modeswitch -v 0x1bbb -p 0xf000 -V 0x1bbb -P 0x0017 -M "55534243123456788000000080000606f50402527000000000000000000000"
after this immediately it is converting to modem and connection is establishing.
Looking for target devices ...
No devices in target mode or class found
Looking for default devices ...
found matching product ID
adding device
Found device in default mode, class or configuration (1)
Accessing device 008 on bus 001 ...
Getting the current device configuration ...
OK, got current device configuration (1)
Using first interface: 0x00
Using endpoints 0x01 (out) and 0x81 (in)
Inquiring device details; driver will be detached ...
Looking for active driver ...
OK, driver found ("usb-storage")
OK, driver "usb-storage" detached
SCSI inquiry data (for identification)
-------------------------
Vendor String: ONETOUCH
Model String: KINGFISHER
Revision String: 2.31
-------------------------
USB description data (for identification)
-------------------------
Manufacturer: Alcatel
Product: MobileBroadBand
Serial No.: 0123456789ABCDEF
-------------------------
Setting up communication with interface 0
Using endpoint 0x01 for message sending ...
Trying to send message 1 to endpoint 0x01 ...
OK, message successfully sent
Resetting response endpoint 0x81
Resetting message endpoint 0x01
Device is gone, skipping any further commands
-> Run lsusb to note any changes. Bye.
Dmesg:
[10449.492021] usb 1-6: new high-speed USB device number 9 using ehci_hcd
[10449.661393] rndis_host 1-6:1.0: eth1: register 'rndis_host' at usb-0000:00:1d.7-6, RNDIS device, 08:2e:5f:29:0e:69
[10449.662012] scsi7 : usb-storage 1-6:1.2
[10450.680042] scsi 7:0:0:0: Direct-Access ONETOUCH KINGFISHER 2.31 PQ: 0 ANSI: 2
[10450.680783] sd 7:0:0:0: Attached scsi generic sg1 type 0
[10450.708634] sd 7:0:0:0: [sdb] Attached SCSI removable disk
[10459.872009] eth1: no IPv6 routers present
and connection is establishing .
similar to this can we get in board also ?
can i get udev/rules.d and supported files for imx6 sabresd board ?
Thanks & Regards,
Lavanya
已解决! 转到解答。
Hi Lavanya,
After creating eth0 node do " ifconfig eth0 proper-IP up " or try with
" udhcpc -i eth0 -b -t 10"
then you will get the IP and then "ping google.com" or global ip like 192.168.1.1
Thanks & Regards,
lavanya
Hi Bandaru
seems driver for this device is not correct or from other linux
distribution/version. It may be suggested to ask from vendor of this
usb modem updated driver for specific linux version which is used in the case.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi igorpadykov,
Actually i am asking about this connection of networking is happening automatically bcz of udev/rules.d in PC that how we can do and what is the exact config file they are using.
For usb_modeswitch they are using "40-usb_modeswitch.rules" similarly which file they are using for setting network connection.
Thanks & Regards,
Lavanya
Hi Lavanya,
After creating eth0 node do " ifconfig eth0 proper-IP up " or try with
" udhcpc -i eth0 -b -t 10"
then you will get the IP and then "ping google.com" or global ip like 192.168.1.1
Thanks & Regards,
lavanya