Hi all,
I built my own rootfs by LTIB using profile 'FSL gnome release package', and started linux on i.MX6Q-SABRESD successfully. But when I pluged a usb hub to OTG port and pluged a usb mouse and a usb keyboard to the hub, the mouse worked well but the keyboard can not.
When I pluged the keyboard,I got some messages as below:
usb 1-1: new low speed USB device number 2 using fsl-ehci
usb 1-1: device v046d pc31c is not supported
input: Logitech USB Keyboard as /devices/platform/fsl-ehci.0/usb1/1-1/1-1:1.0/in
put/input9
generic-usb 0003:046D:C31C.0001: input,hidraw0: USB HID v1.10 Keyboard [Logitech
USB Keyboard] on usb-fsl-ehci.0-1/input0
input: Logitech USB Keyboard as /devices/platform/fsl-ehci.0/usb1/1-1/1-1:1.1/in
put/input10
generic-usb 0003:046D:C31C.0002: input,hidraw1: USB HID v1.10 Device [Logitech U
SB Keyboard] on usb-fsl-ehci.0-1/input1
Besides,I found that when I pressed <ALTF1> the screen became black and <ALTF2> returned to gnome desktop.The NumLOCK and CapsLock indicator lights worked well,but I can't use other function such as typing words in xterm.
Any suggestions? Thanks in advance!
Xiaoqiang
Dear SerchMX
I don't know if Mr. Xiaoquiang Yang is still there, so I'd like to ask you if you know how to solve this problem.
I can see the same issue as him on my iMX53-START board, using the L2.6.35_11.09.01_ER_source + patches and no other change.
Sometimes it happens that pressing some key combination I get the x to crash, and in that case the screen becomes black, with all the keys I pressed written on it. So there's not a hardware problem...
I looked everywhere on the internet without finding any solution. Please help me...
Finally I solved the problem myself!
I had to edit the startx script to load the keyboard.
Now I have to find out how to change the keyboard language layout... I tried editing xorg.conf without success...
I am also having the same problem
usb 1-1: new low speed USB device number 5 using fsl-ehci
usb 1-1: device v047b p00f9 is not supported
input: Silite Generic USB Keyboard as /devices/platform/fsl-ehci.0/usb1/1-1/1-1:1.0/input/input13
generic-usb 0003:047B:00F9.0005: input,hidraw0: USB HID v1.00 Keyboard [Silite Generic USB Keyboard] on usb-fsl-ehci.0-1/input0
input: Silite Generic USB Keyboard as /devices/platform/fsl-ehci.0/usb1/1-1/1-1:1.1/input/input14
generic-usb 0003:047B:00F9.0006: input,hidraw1: USB HID v1.00 Device [Silite Generic USB Keyboard] on usb-fsl-ehci.0-1/input1
Can you please elaborate how you solved the problem. I am new for iMx boards.
Hi Roberto,
These days I was not working,sorry for that.Now I have made my keyboard work by editing the start.x, as you did. And I am finding the way to ahanging the keyboard
layout too,if I have some progress,I will tell you!