We are building Linux image for our custom board based on sabre-sd. Uart 2 is used as debug uart. We are using yocto Fido to build the image , with meta-fsl-arm. The console uart has been changed in the u-boot bootargs and also enabled pin-muxing for uart 2 in the dtb files. Booting stops at "starting kernel". We also enabled CONFIG_DEBUG_LL, after which we are are getting the message "Uncompressing Linux... done, booting the kernel." Please help on the issue. The log file is as below.
U-Boot 2015.07+fslc+g3f0c535 (Oct 16 2015 - 21:09:09 +0530)
CPU: Freescale i.MX6Q rev1.0 at 792MHz
CPU: Commercial temperature grade (0C to 95C)CPU: Thermal invalid data, fuse: 0x0
- invalid sensor device
Reset cause: POR
Board: MX6-SabreSD
I2C: ready
DRAM: 1 GiB
MMC: FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2
*** Warning - bad CRC, using default environment
PCI: pcie phy link never came up
No panel detected: default to Hannstar-XGA
Display: Hannstar-XGA (1024x768)
In: serial
Out: serial
Err: serial
Net: Phy 1 not found
PHY reset timed out
FEC [PRIME]
Hit any key to stop autoboot: 0
switch to partitions #0, OK
mmc1 is current device
reading boot.scr
** Unable to read file boot.scr **
reading zImage
5946592 bytes read in 290 ms (19.6 MiB/s)
Booting from mmc ...
reading imx6q-sabresd-ldo.dtb
42395 bytes read in 19 ms (2.1 MiB/s)
Kernel image @ 0x12000000 [ 0x000000 - 0x5abce0 ]
## Flattened Device Tree blob at 18000000
Booting using the fdt blob at 0x18000000
Using Device Tree in place at 18000000, end 1800d59a
Starting kernel ...
Uncompressing Linux... done, booting the kernel.
=> printenv
baudrate=115200
boot_fdt=try
bootcmd=mmc dev ${mmcdev};if mmc rescan; then if run loadbootscript; then run bootscript; else if run loadimage; then run mmcboot; else run netboot; fi; fi; else run netboot; fi
bootdelay=3
bootscript=echo Running bootscript from mmc ...; source
console=ttymxc1
emmcdev=2
ethact=FEC
ethaddr=00:00:aa:bb:cc:dd
ethprime=FEC
fb=0
fdt_addr=0x18000000
fdt_file=imx6q-sabresd-ldo.dtb
fdt_high=0xffffffff
image=zImage
initrd_high=0xffffffff
ip_dyn=yes
loadaddr=0x12000000
loadbootscript=fatload mmc ${mmcdev}:${mmcpart} ${loadaddr} ${script};
loadfdt=fatload mmc ${mmcdev}:${mmcpart} ${fdt_addr} ${fdt_file}
loadimage=fatload mmc ${mmcdev}:${mmcpart} ${loadaddr} ${image}
mmcargs=setenv bootargs console=${console},${baudrate} root=${mmcroot} ${video_args}
mmcboot=echo Booting from mmc ...; run video_args_script; run mmcargs; if test ${boot_fdt} = yes || test ${boot_fdt} = try; then if run loadfdt; then bootz ${loadaddr} - ${fdt_addr}; else if test ${boot_fdt} = try; then bootz; else echo WARN: Cannot load the DT; fi; fi; else bootz; fi;
mmcdev=1
mmcpart=1
mmcroot=/dev/mmcblk2p2 rootwait rw
netargs=setenv bootargs console=${console},${baudrate} root=/dev/nfs ip=dhcp nfsroot=${serverip}:${nfsroot},v3,tcp
netboot=echo Booting from net ...; run netargs; if test ${ip_dyn} = yes; then setenv get_cmd dhcp; else setenv get_cmd tftp; fi; ${get_cmd} ${image}; if test ${boot_fdt} = yes || test ${boot_fdt} = try; then if ${get_cmd} ${fdt_addr} ${fdt_file}; then bootz ${loadaddr} - ${fdt_addr}; else if test ${boot_fdt} = try; then bootz; else echo WARN: Cannot load the DT; fi; fi; else bootz; fi;
script=boot.scr
update_emmc_firmware=if test ${ip_dyn} = yes; then setenv get_cmd dhcp; else setenv get_cmd tftp; fi; if ${get_cmd} ${update_sd_firmware_filename}; then if mmc dev ${emmcdev} 1; then setexpr fw_sz ${filesize} / 0x200; setexpr fw_sz ${fw_sz} + 1; mmc write ${loadaddr} 0x2 ${fw_sz}; fi; fi
update_sd_firmware=if test ${ip_dyn} = yes; then setenv get_cmd dhcp; else setenv get_cmd tftp; fi; if mmc dev ${mmcdev}; then if ${get_cmd} ${update_sd_firmware_filename}; then setexpr fw_sz ${filesize} / 0x200; setexpr fw_sz ${fw_sz} + 1; mmc write ${loadaddr} 0x2 ${fw_sz}; fi; fi
video_args_hdmi=setenv video_args $video_args video=mxcfb${fb}:dev=hdmi,1280x720M@60,if=RGB24
video_args_lcd=setenv video_args $video_args video=mxcfb${fb}:dev=lcd,CLAA-WVGA,if=RGB666
video_args_lvds=setenv video_args $video_args video=mxcfb${fb}:dev=ldb,LDB-XGA,if=RGB666
video_args_script=for v in ${video_interfaces}; do run video_args_${v}; setexpr fb $fb + 1; done
video_interfaces=hdmi lvds lcd
Environment size: 2687/8188 bytes
thanks,
Sujith Vasudevan
解決済! 解決策の投稿を見る。
Hi
This Issue is solved. There was conflict in pin mux setting of uart 2 in imx6qdl-sabresd.dtsi file. I removed the following line
MX6QDL_PAD_ENET_TXD1__GPIO1_IO29 0x80000000
MX6QDL_PAD_EIM_D22__GPIO3_IO22 0x80000000
MX6QDL_PAD_ENET_CRS_DV__GPIO1_IO25 0x80000000
- MX6QDL_PAD_EIM_D26__GPIO3_IO26 0x80000000 /* conflicts with MX6QDL_PAD_EIM_D26__UART2_TX_DATA*/
+
MX6QDL_PAD_EIM_CS1__GPIO2_IO24 0x80000000
MX6QDL_PAD_ENET_RXD0__GPIO1_IO27 0x80000000
MX6QDL_PAD_EIM_A25__GPIO5_IO02 0x80000000
Thank You Igor and Fabio for all your inputs ...
warm regards,
Sujith Vasudevan
Can you show us in a patch format the changes you did in the dts file?
Hi Fabio,
The changes i made to configure uart is as follows
diff --git a/arch/arm/boot/dts/imx6qdl-sabresd.dtsi b/arch/arm/boot/dts/imx6qdl-sabresd.dtsi
index 9cf7652..2f64a26 100644
--- a/arch/arm/boot/dts/imx6qdl-sabresd.dtsi
+++ b/arch/arm/boot/dts/imx6qdl-sabresd.dtsi
@@ -699,6 +699,13 @@
MX6QDL_PAD_CSI0_DAT11__UART1_RX_DATA 0x1b0b1
>;
};
+
+ pinctrl_uart2: uart2grp {
+ fsl,pins = <
+ MX6QDL_PAD_EIM_D27__UART2_RX_DATA 0x1b0b1
+ MX6QDL_PAD_EIM_D26__UART2_TX_DATA 0x1b0b1
+ >;
+ };
pinctrl_uart5_1: uart5grp-1 {
fsl,pins = <
@@ -899,6 +906,13 @@
status = "okay";
};
+&uart2 {
+ pinctrl-names = "default";
+ pinctrl-0 = <&pinctrl_uart2>;
+ status = "okay";
+};
+
+
&usbh1 {
vbus-supply = <®_usb_h1_vbus>;
status = "okay";
--
regards,
sujith vasudevan
Hi
This Issue is solved. There was conflict in pin mux setting of uart 2 in imx6qdl-sabresd.dtsi file. I removed the following line
MX6QDL_PAD_ENET_TXD1__GPIO1_IO29 0x80000000
MX6QDL_PAD_EIM_D22__GPIO3_IO22 0x80000000
MX6QDL_PAD_ENET_CRS_DV__GPIO1_IO25 0x80000000
- MX6QDL_PAD_EIM_D26__GPIO3_IO26 0x80000000 /* conflicts with MX6QDL_PAD_EIM_D26__UART2_TX_DATA*/
+
MX6QDL_PAD_EIM_CS1__GPIO2_IO24 0x80000000
MX6QDL_PAD_ENET_RXD0__GPIO1_IO27 0x80000000
MX6QDL_PAD_EIM_A25__GPIO5_IO02 0x80000000
Thank You Igor and Fabio for all your inputs ...
warm regards,
Sujith Vasudevan
Hi Sujith
from log: "CPU: Freescale i.MX6Q rev1.0 at 792MHz"
seems this is old preproduction 1.0 version, not supported more.
Please look at attached Release Notes p.11:
Freescale decided to drop the preproduction TO1.1/TO1.0) chip support.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thank You Igor,
I tried to boot the same image in another board. I get the same issue. Here the CPU version is 1.2. Please advice.
U-Boot 2015.07+fslc+g3f0c535 (Oct 16 2015 - 21:09:09 +0530)
CPU: Freescale i.MX6Q rev1.2 996 MHz (running at 792 MHz)
CPU: Automotive temperature grade (-40C to 125C) at 19C
Reset cause: POR
Board: MX6-SabreSD
I2C: ready
DRAM: 1 GiB
MMC: FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2
*** Warning - bad CRC, using default environment
PCI: pcie phy link never came up
No panel detected: default to Hannstar-XGA
Display: Hannstar-XGA (1024x768)
In: serial
Out: serial
Err: serial
Net: Phy 1 not found
PHY reset timed out
FEC [PRIME]
Error: FEC address not set.
Hit any key to stop autoboot: 0
switch to partitions #0, OK
mmc1 is current device
reading boot.scr
** Unable to read file boot.scr **
reading zImage
6235320 bytes read in 313 ms (19 MiB/s)
Booting from mmc ...
reading imx6q-sabresd-ldo.dtb
42395 bytes read in 19 ms (2.1 MiB/s)
Kernel image @ 0x12000000 [ 0x000000 - 0x5f24b8 ]
## Flattened Device Tree blob at 18000000
Booting using the fdt blob at 0x18000000
Using Device Tree in place at 18000000, end 1800d59a
Starting kernel ...
Uncompressing Linux... done, booting the kernel.
Hi Sujith
had you modified uboot dcd header ...board/mx6sabresd/mx6dl_4x_mt41j128.cfg
with new board ddr settings obtained from ddr tester
i.MX6/7 DDR Stress Test Tool V2.20
~igor
Hi Igor,
Thank you. I was able to run DDR stress test successfully. I don't think its some issue with the DDR. Here is the log.
============================================
DDR Stress Test (2.2.0)
Build: Sep 29 2015, 22:20:56
Freescale Semiconductor, Inc.
============================================
============================================
Chip ID
DIGPROG(0x020c8260) = 0x00630002
CHIP ID = i.MX6 Dual/Quad (0x63)
Internal Revision = TO1.2
============================================
============================================
Boot Configuration
SRC_SBMR1(0x020d8004) = 0x08003040
SRC_SBMR2(0x020d801c) = 0x11000001
============================================
============================================
DDR configuration
BOOT_CFG3[5-4]: 0x00, Single DDR channel.
DDR type is DDR3
Data width: 64, bank num: 8
Row size: 14, col size: 10
Chip select CSD0 is used
Density per chip select: 1024MB
============================================
DDR Stress Test Iteration 1
Current Tempareture: 31
============================================
DDR Freq: 396 MHz
t0.1: data is addr test
t0: memcpy10 SSN x64 test
t1: memcpy8 SSN x64 test
t2: byte-wise SSN x64 test
t3: memcpy11 random pattern test
t4: IRAM_to_DDRv2 test
t5: IRAM_to_DDRv1 test
t6: read noise walking ones and zeros test
DDR Freq: 413 MHz
t0.1: data is addr test
t0: memcpy10 SSN x64 test
t1: memcpy8 SSN x64 test
t2: byte-wise SSN x64 test
t3: memcpy11 random pattern test
t4: IRAM_to_DDRv2 test
t5: IRAM_to_DDRv1 test
t6: read noise walking ones and zeros test
DDR Freq: 432 MHz
t0.1: data is addr test
t0: memcpy10 SSN x64 test
t1: memcpy8 SSN x64 test
t2: byte-wise SSN x64 test
t3: memcpy11 random pattern test
t4: IRAM_to_DDRv2 test
t5: IRAM_to_DDRv1 test
t6: read noise walking ones and zeros test
DDR Freq: 452 MHz
t0.1: data is addr test
t0: memcpy10 SSN x64 test
t1: memcpy8 SSN x64 test
t2: byte-wise SSN x64 test
t3: memcpy11 random pattern test
t4: IRAM_to_DDRv2 test
t5: IRAM_to_DDRv1 test
t6: read noise walking ones and zeros test
DDR Freq: 475 MHz
t0.1: data is addr test
t0: memcpy10 SSN x64 test
t1: memcpy8 SSN x64 test
t2: byte-wise SSN x64 test
t3: memcpy11 random pattern test
t4: IRAM_to_DDRv2 test
t5: IRAM_to_DDRv1 test
t6: read noise walking ones and zeros test
DDR Freq: 500 MHz
t0.1: data is addr test
t0: memcpy10 SSN x64 test
t1: memcpy8 SSN x64 test
t2: byte-wise SSN x64 test
t3: memcpy11 random pattern test
t4: IRAM_to_DDRv2 test
t5: IRAM_to_DDRv1 test
t6: read noise walking ones and zeros test
DDR Freq: 528 MHz
t0.1: data is addr test
t0: memcpy10 SSN x64 test
t1: memcpy8 SSN x64 test
t2: byte-wise SSN x64 test
t3: memcpy11 random pattern test
t4: IRAM_to_DDRv2 test
t5: IRAM_to_DDRv1 test
t6: read noise walking ones and zeros test
DDR Freq: 532 MHz
t0.1: data is addr test
t0: memcpy10 SSN x64 test
t1: memcpy8 SSN x64 test
t2: byte-wise SSN x64 test
t3: memcpy11 random pattern test
t4: IRAM_to_DDRv2 test
t5: IRAM_to_DDRv1 test
t6: read noise walking ones and zeros test
Success: DDR Stress test completed!!!
-sujith
Hi Sujith
I see you use community release with U-Boot 2015.07+fslc.
Please try Freescale official BSP from L3.14.28_1.0.0_iMX6QDLS_BUNDLE:
Board Support Packages (27)
L3.14.28_1.0.0_iMX6QDLS_BUNDLE (REV L3.14.28_1.0.0)
It uses v2014.04 as shown in attached Release Notes.
Difference between Freescale official BSP and Community releases and its support rules
is described on
Re: difference between Yocto Community BSP and Freescale BSP Release
~igor
Hi Igor,
I tried uisng Freescale official BSP from L3.14.28_1.0.0_iMX6QDLS_BUNDLE. I still get the same issue.
U-Boot 2014.10+fslc+g5fd0b60 (Oct 28 2015 - 10:27:43)
CPU: Freescale i.MX6Q rev1.0 at 792 MHz
Reset cause: POR
Board: MX6-SabreSD
I2C: ready
DRAM: 1 GiB
MMC: FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2
*** Warning - bad CRC, using default environment
No panel detected: default to Hannstar-XGA
Display: Hannstar-XGA (1024x768)
In: serial
Out: serial
Err: serial
Can't find PMIC:PFUZE100
Net: Phy not found
PHY reset timed out
FEC [PRIME]
Hit any key to stop autoboot: 0
switch to partitions #0, OK
mmc1 is current device
reading boot.scr
** Unable to read file boot.scr **
reading zImage
5287656 bytes read in 246 ms (20.5 MiB/s)
Booting from mmc ...
reading imx6q-sabresd-ldo.dtb
47179 bytes read in 19 ms (2.4 MiB/s)
Kernel image @ 0x12000000 [ 0x000000 - 0x50aee8 ]
## Flattened Device Tree blob at 18000000
Booting using the fdt blob at 0x18000000
Using Device Tree in place at 18000000, end 1800e84a
Starting kernel ...
Hi Sujith
it is not uboot from Freescale official BSP, as
it uses v2014.04 as shown in attached Release Notes.
Best regards
igor
Hi Igor,
Thank you for the reply.
Can you help me with more info on the build.
The steps i followed is as below. Please correct me if i am wrong.
1. Downloaded fsl-L3.14.28_1.0.0_iMX6qdls_Bundle.tar
2. Untared fsl-L3.14.28_1.0.0_iMX6qdls_Bundle.tar which had two files in it fsl-yocto-3.14.28-1.0.0.tar.gz and L3.14.28_1.0.0_ga_images_MX6.tar.gz .
3. Untared fsl-yocto-3.14.28-1.0.0.tar.gz and followed steps in the document Freescale_Yocto_Project_User's_Guide.pdf
repo init -u git://git.freescale.com/imx/fsl-arm-yocto-bsp.git -b imx-3.14.28-1.0.0_ga
repo sync
-sujith
Hi Sujith
as this is new problem please create new thread for it.
Best regards
igor
Thank you Igor,
I have made a seperate post for the build issues.
Can you share more approaches to debug the issue.
-sujith vasudevan