kernel BUG at drivers/crypto/caam/jr.c

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

kernel BUG at drivers/crypto/caam/jr.c

2,737件の閲覧回数
kunsong
Contributor I

hi,

Check log, call trace output "irqstate: 00000103"

Check code: drivers/crypto/caam/jr.c

286 if (irqstate & JRINT_JR_ERROR) {
287 dev_err(dev, "job ring error: irqstate: %08x\n", irqstate);
288 BUG();
289 }

caam_jr_remove function

238 if (atomic_read(&jrpriv->tfm_count)) {
239 dev_err(jrdev, "Device is busy\n");
240 return -EBUSY;
241 }

Judging from the current log, the caam_jr_remove function was called, but the check device is still busy.

I found a similar problem:
https://community.nxp.com/t5/Layerscape/Kernel-panic-with-Layerscape-17-09-kernel-4-9-35/m-p/697467

NXP suggest:
"You are working with the kernel from LSDK 1709 ( 4.9.35), but your u-Boot seem to be taken from an earlier release (1709 u-Boot is 2017.07, your one is 2017.03).
Can you update your u-Boot and try again?"

Check our version:

nxp-ls1028 kernel: Linux version 5.10.154*
nxp-ls1028 kernel: efi: EFI v2.80 by Das U-Boot

U-Boot 2019.10+fsl+g3d542a3d22 (Dec 21 2021 - 20:21:21 +0000)

our uboot version is Higher, do you know the possible cause of this problem?

Thanks!

BR/SK

 

 


caam_jr 8030000.jr: Device is busy caam_jr 8020000.jr: Device is busy caam_jr 8010000.jr: Device is busy arm-smmu 5000000.iommu: disabling translation caam_jr 8010000.jr: job ring error: irqstate: 00000103 ------------[ cut here ]------------ kernel BUG at drivers/crypto/caam/jr.c:288! Internal error: Oops - BUG: 0 [#1] PREEMPT SMP Modules linked in: lttng_ring_buffer_client_discard(O) lttng_ring_buffer_client_overwrite(O) lttng_ring_buffer_metadata_client(O) lttng_ring_buffer_client_mmap_discard(O) lttng_ring_buffer_client_mmap_overwrite(O) lttng_ring_buffer_metadata_mmap_client(O) lttng_probe_printk(O) lttng_probe_signal(O) lttng_probe_irq(O) lttng_probe_sched(O) lttng_tracer(O) lttng_statedump(O) lttng_wrapper(O) lttng_uprobes(O) lttng_clock(O) lttng_kprobes(O) lttng_lib_ring_buffer(O) lttng_kretprobes(O) binfmt_misc [last unloaded: tpm_ftpm_tee] CPU: 0 PID: 163 Comm: hwrng Tainted: G W O 5.10.154-wrl21.15-wrprime-1-yocto-standard-custom-rcs #1 Hardware name: freescale ls1028a/ls1028a, BIOS 2019.10+fsl+g3d542a3d22 12/21/2021 pstate: 60000085 (nZCv daIf -PAN -UAO -TCO BTYPE=--) pc : caam_jr_interrupt+0x128/0x130 lr : caam_jr_interrupt+0x128/0x130 sp : ffff80001144be50 x29: ffff80001144be50 x28: ffff800010f61008 x27: ffff800011228000 x26: ffff800010f61008 x25: ffff000027904800 x24: 0000000000000072 x23: ffff8000113ba140 x22: 0000000000000001 x21: ffff800011433000 x20: ffff000027904e80 x19: 0000000000000103 x18: 0000000000000030 x17: 0000000000000000 x16: 0000000000000000 x15: ffffffffffffffff x14: ffff8000113ebcb8 x13: 0000000000000008 x12: fffffffffffcac8f x11: ffff00000038bb00 x10: ffff8000112a1e90 x9 : ffff8000100a99c0 x8 : ffff800011249e90 x7 : ffff8000112a1e90 x6 : 0000000000000000 x5 : 0000000000000000 x4 : 0000000000000000 x3 : 0000000000000000 x2 : 0000000000000000 x1 : 0000000000000000 x0 : ffff0000279ac600 Call trace: caam_jr_interrupt+0x128/0x130 __handle_irq_event_percpu+0x84/0x2b0 handle_irq_event+0x6c/0xfc handle_fasteoi_irq+0xc8/0x230 __handle_domain_irq+0xb8/0x130 gic_handle_irq+0x90/0x158 el1_irq+0xcc/0x180 _raw_spin_lock_irq+0x0/0x90 caam_rng_read_one.constprop.0+0x248/0x370 caam_read+0x8c/0xb0 hwrng_fillfn+0xfc/0x1cc kthread+0x14c/0x160 ret_from_fork+0x10/0x30 Code: 2a1303e2 d00029a1 910ee021 940b2b1d (d4210000) ---[ end trace f04d90f3ad0da5f4 ]--- Kernel panic - not syncing: Oops - BUG: Fatal exception in interrupt Kernel Offset: disabled CPU features: 0x28040022,21002008 Memory Limit: none

 

 

0 件の賞賛
返信
3 返答(返信)

2,671件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

I suspect there is problem with your Linux Kernel source code.

Please refer to Linux SDK release from the following link 

https://github.com/nxp-qoriq/yocto-sdk

Yocto branch and version
========================
| Branch      | Version          |
|-------------|------------------|
| mickledore  | YP 4.2–lf-6.1.36 |
| langdale    | YP 4.1–lf-6.1.1  |
| kirkstone   | YP 4.0–lf-5.15.71|
| honister    | YP 3.4–lf-5.15.5 |
| hardknott   | YP 3.3–lf-5.10.72|

We didn't release Linux Kernel 5.10.154* to customer.

Please download one formal release LSDK to do verification on your target board.

0 件の賞賛
返信

2,644件の閲覧回数
kunsong
Contributor I

yes, We have a customized kernel system, and this problem is difficult to reproduce.

Do you know what "irqstate: 00000103 " means ?

I didn't find any definition in the manual

 

0 件の賞賛
返信

2,713件の閲覧回数
kunsong
Contributor I

hi, @bpe 

Can you give some advice?

Do you know what this value means?  irqstate: 00000103 

Thanks!

BR/SK

0 件の賞賛
返信