Hi jesse
for flexcan configuaration one can look at i.MX6 Sabre AI dts:
arch/arm/boot/dts/imx6qdl-sabreauto.dtsi
and check sect.5.1 Build configurations attached Yocto Guide.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
in myandroid/kernel_imx/drivers/net/can/dev.c
static int can_validate(struct nlattr *tb[], struct nlattr *data[])
{
bool is_can_fd = false;
/* begin: issue #: prevent crash */
if( data != NULL ) //add this can prevent from crash
{
if (data[IFLA_CAN_CTRLMODE]) {
struct can_ctrlmode *cm = nla_data(data[IFLA_CAN_CTRLMODE]);
is_can_fd = cm->flags & cm->mask & CAN_CTRLMODE_FD;
}
if (is_can_fd) {
if (!data[IFLA_CAN_BITTIMING] || !data[IFLA_CAN_DATA_BITTIMING])
return -EOPNOTSUPP;
}
if (data[IFLA_CAN_DATA_BITTIMING]) {
if (!is_can_fd || !data[IFLA_CAN_BITTIMING])
return -EOPNOTSUPP;
}
return 0;
}
return -ENODATA;
/* end: issue #: prevent crash */
}