'imxv4l2videosrc' shows no capabilities

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

'imxv4l2videosrc' shows no capabilities

608件の閲覧回数
dh29
Contributor IV

i.MX7D, gstreamer-1.0, imx gstreamer plugin v0.12.3

========================================

In my on-going battle to get an AD7280M (csi-mipi) working on an i.MX7 I have reached the point whereby occasionally I can capture an image (albeit wrong colors), but only if I use the v4l2src. I cannot get the 'imxv4l2videosrc' to work.

I have inspected the 'imxv4l2videosrc' using, 

gst-inspect-1.0 imxv4l2videosrc

and it shows the following:

Factory Details:
   Rank primary (256)
   Long-name V4L2 CSI Video Source
   Klass Source/Video
   Description Capture video streams using V4L2 CSI interface
   Author Philip Craig <phil@blackmoth.com.au>

Plugin Details:
   Name imxv4l2videosrc
   Description GStreamer i.MX V4L2 CSI video source
   Filename /usr/lib/gstreamer-1.0/libgstimxv4l2videosrc.so
   Version 0.12.3
   License LGPL
   Source module gstreamer-imx
   Binary package Unknown package release
   Origin URL Unknown package origin

GObject
   +----GInitiallyUnowned
      +----GstObject
         +----GstElement
            +----GstBaseSrc
               +----GstPushSrc
                  +----GstImxV4l2VideoSrc

Implemented Interfaces:
   GstURIHandler
   GstPhotography

Pad Templates:
   SRC template: 'src'
      Availability: Always
   Capabilities:
      video/x-raw


   Element Flags:
      no flags set

So there are no capabilities listed with the 'video/x-raw' ??? Anybody any ideas why???

ラベル(3)
0 件の賞賛
2 返答(返信)

391件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi dh29,

The i.MX7D has no VPU.

Regards

0 件の賞賛

391件の閲覧回数
dh29
Contributor IV

Hi Bio_TICFSL ,

I have managed to get gstreamer to capture using v4l2src , albeit with 2 images; one on top of the other (I'm struggling to get the iMX7 to capture anything CCIR / BT 656 Interlaced mode).

So because the i.MX7D has no VPU, this means that the gstreamer i.MX plugins are not applicable?

0 件の賞賛