imxv4l2src 1280x720 csi camera error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imxv4l2src 1280x720 csi camera error

1,054件の閲覧回数
m_c
Senior Contributor I

We use below command to test CSI camera in 1280x720 4.1.15 on and get error as below.

root@imx6qsabresd:~# gst-launch-1.0 imxv4l2src device=/dev/video0 ! 'video/x-raw,width=1280,height=720,framerate=(fraction)30/1' ! imxv4l2sink

ERROR: v4l2 capture: slave not found!

====== IMXV4L2SRC: 4.0.9 build on Aug  2 2016 15:43:47. ======

====== IMXV4L2SINK: 4.0.9 build on Aug  2 2016 15:43:47. ======

Setting pipeline to PAUSED ...

display(/dev/fb0) resolution is (1920x1080).

Pipeline is live and does not need PREROLL ...

Setting pipeline to PLAYING ...

New clock: GstSystemClock

v4l2sink need allocate 3 buffers.

imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_5 = 0x08000000

imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_5 = 0x08000000

mxc_sdc_fb fb@0: timeout when waiting for flip irq

imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_5 = 0x08000000

imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_5 = 0x08000000

ERROR: from element /GstPipeline:pipeline0/GstImxV4l2Src:imxv4l2src0: Internal data flow error.

Additional debug info:

/home/mimxc_sdc_fb fb@0: timeout when waiting for flip irq

ke/yocto/imx6qsabresd/tmp/work/coimx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_5 = 0x08000000

rtexa9hf-vfp-neon-poky-linux-gnueabi/gstreamer1.0/1.6.0-r0/gstreamer-1.6.0/libs/gst/base/gstbasesrc.c(2943): gst_base_src_loop (): /GstPipeline:pipeline0/GstImxV4l2Src:imxv4l2src0:

streaming task paused, reason error (-5)

Execution ended after 0:00:01.675626667

Setting pipeline to PAUSED ...

Setting pipeline to READY ...

mxc_sdc_fb fb@0: timeout when waiting for flip irq

imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_5 = 0x08000000

(gst-launch-1.0:908): GStreamer-CRITICAL **: gst_mini_object_unref: assertion 'mini_object->refcount > 0' failed

Setting pipeline to NULL ...

Total showed frames (5), playing for (0:00:01.676514667), fps (2.982).

Freeing pipeline ...

ラベル(3)
0 件の賞賛
返信
1 返信

627件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  The messages about IPU_INT_STAT_5 are used to indicate “about errors that are
result of data rate problems. Such problems may be a result of the IPU running in
slower clock then required by the use case. This signal can be used in order to indicate
the system that the IPU can't handle the desired data rate. In that case the system

may need to increase the clock to the IPU or simplify the use case.”

So, we have here performance problem.

To improve situation one can apply overlaysink gstreamer element. Please refer to

sections 7.5 (Overlaysink usage) and 7.3.1.6.3 (Multiple videos overlay) of “i.MX_Linux_User's_Guide.pdf”.

Also, please try to increase DMFC FIFO size (dmfc=3 in boot parameter)

http://www.nxp.com/webapp/Download?colCode=L4.1.15_1.2.0_LINUX_DOCS&Parent_nodeId=133769948107170617...

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信