imx93evk Yocto image(imx-image-multimedia) build fails

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx93evk Yocto image(imx-image-multimedia) build fails

175 Views
osihgnes
Contributor I

Dear all
I am a novice at building the Yocto Project. Therefore, I carefully followed the instructions in the i.MX Yocto Project User's Guide (Rev. LF6.6.3_1.0.0 — 29 March 2024) for setting up the environment, using the correct distribution and machine configuration for the imx93 EVK.
DISTRO="fsl-imx-wayland"
MACHINE="imx93evk"

Additionally, I added the following line to local.conf to use Chromium.
CORE_IMAGE_EXTRA_INSTALL += "chromium-ozone-wayland"

However, when I tried to bitbake imx-image-multimedia, I encountered the following errors:

ERROR: Task (/home/user/imx-yocto-bsp/sources/poky/meta/recipies-devtools/gcc/gcc_13.2.bb:do_compile) failed with exit code '1'

ERROR: Task (virtual:native/home/user/imx-yocto-bsp/sources/poky/meta/recipies-devtools/rust/rust_1.70.0.bb:do_install) failed with exit code '1'

ERROR: Task (virtual:native/home/user/imx-yocto-bsp/sources/meta-openembedded/meta-oe/recipies-devtools/doxygen/doxygen_1.9.3.bb:do_compile) failed with exit code '1'

If you have any suggestions or workarounds for these errors, please let me know.

Thank you in advance

0 Kudos
Reply
3 Replies

142 Views
joanxie
NXP TechSupport
NXP TechSupport

I have built it successfully, this is my steps:

1) repo init -u https://github.com/nxp-imx/imx-manifest -b imx-linux-nanbield -m imx-6.6.3-1.0.0.xml
2) repo sync
3)DISTRO=fsl-imx-wayland MACHINE=imx93-11x11-lpddr4x-evk source imx-setup-release.sh -b imx93-wayland

4)change the local.conf

5) bitbake imx-image-multimedia

joanxie_0-1719024311601.png

so pls check if you install all of packages for the ubuntu environment setup, you can refer to the chapter 3 Host Setup, and I use the imx93-11x11-lpddr4x-evk, but yours should be ok, maybe you can try mine again

 

0 Kudos
Reply

87 Views
osihgnes
Contributor I

Hi, Joan,

I have already followed the steps you suggested. I successfully built it by adding the following elements to local.conf:

BB_TIMEOUT = "1800"
BB_NUMBER_THREADS = '2'
PARALLEL_MAKE = '-j 2'
SSTATE_DIR = "${TOPDIR}/sstate-cache"

However, I don't have information on how to run Chromium. I tried running Chromium in the usual way, but I encountered errors. Could you provide information on how to run Chromium or the possible causes of the errors?

Thank you in advance

0 Kudos
Reply

54 Views
joanxie
NXP TechSupport
NXP TechSupport

pls create a new case for this new topic, we need spend time on reproducing this on inx93 board

0 Kudos
Reply